Time
This contains all time functionality. More...
Modules | |
Types | |
Time specific types. | |
Detailed Description
This contains all time functionality.
Function Documentation
◆ gos_time_get_current_utc_as_iso8601()
gos_result_t gos_time_get_current_utc_as_iso8601 | ( | gos_iso8601_t * | iso8601_struct, |
bool | add_timezone |
||
) |
Returns the current time as a gos_iso8601_t struct.
This has similar functionality to gos_time_get_current_utc_ms() except the current time is returned as a gos_iso8601_t
- Parameters
-
[out] iso8601_struct
Buffer to hold the current time as a gos_iso8601_t [in] add_timezone
If true then include the timezone offset in the returned value, if false then return UTC time with 0 timezone offset
- Returns
- gos_result_t result of api call
◆ gos_time_get_current_utc_as_iso8601_str()
gos_result_t gos_time_get_current_utc_as_iso8601_str | ( | gos_iso8601_str_t * | iso8601_str, |
bool | add_timezone |
||
) |
Returns the current time as a gos_iso8601_str_t.
This has similar functionality to gos_time_get_current_utc_ms() except the current time is returned as a gos_iso8601_str_t
- Note
- The returned
iso8601_str
is null-terminated and can be directly printed as a string
- Parameters
-
[out] iso8601_str
Buffer to hold the current time as a gos_iso8601_str_t [in] add_timezone
If true then include the timezone offset in the returned value, if false then return UTC time with 0 timezone offset
- Returns
- gos_result_t result of api call
- Examples:
- dms/messages/main.c, dms/telemetry/main.c, hurricane/weatherstation/main.c, network/http_server/requests/root_page.c, network/http_server_stream/main.c, network/tcp_client/main.c, network/udp_client/main.c, network/websocket_client/main.c, utility/msgpack/read_write_buffer.c, and utility/msgpack/read_write_stream.c.
◆ gos_time_get_current_utc_ms()
gos_result_t gos_time_get_current_utc_ms | ( | gos_utc_ms_t * | utc_time_ms, |
bool | add_timezone |
||
) |
Returns the current UTC time in milliseconds.
This returns the current time as the number of milliseconds since the Epoch. i.e. This returns UNIX time.
- Note
- If the time.zone variable is set and
add_timezone
is true then the timezone will be included in the returned value.
The current time may be set with gos_time_set_current_utc_ms(). However, the recommended approach is to use Network Time Protocol (NTP) to retrieve the time from the network, see ntp.enabled. Additionally, see gos_ntp_update() for more details about obtaining the current UTC time via NTP.
This API will return GOS_NEVER_SET if the time was never set.
- Note
- The value returned by this API is maintained by Real-Time Clock (RTC) hardware. The time will persist through reboots and resets as long as the device is powered.
See time.rtc for more details.
- Parameters
-
[out] utc_time_ms
Buffer to hold the current time [in] add_timezone
If true then include the timezone offset in the returned value, if false then return UTC time with 0 timezone offset
- Returns
- gos_result_t result of api call
◆ gos_time_get_current_utc_seconds()
gos_result_t gos_time_get_current_utc_seconds | ( | gos_utc_seconds_t * | utc_time_seconds_ptr, |
bool | add_timezone |
||
) |
Returns the current time in seconds.
This has similar functionality to gos_time_get_current_utc_ms() except the current time is returned as a gos_utc_seconds_t
- Parameters
-
[out] utc_time_seconds_ptr
Buffer to hold the current time in seconds [in] add_timezone
If true then include the timezone offset in the returned value, if false then return UTC time with 0 timezone offset
- Returns
- gos_result_t result of api call
- Examples:
- hurricane/security_camera/camera.c.
◆ gos_time_get_ms_since_time_set()
gos_result_t gos_time_get_ms_since_time_set | ( | uint64_t * | ms_since_last_set_ptr | ) |
Return the number of milliseconds since the time was last set.
This returns the number of millseconds since the UTC time was last set.
- Parameters
-
[out] ms_since_last_set_ptr
Buffer to hold the number of milliseconds since the UTC time was last set
- Returns
- gos_result_t result of api call
◆ gos_time_get_timezone_offset()
gos_result_t gos_time_get_timezone_offset | ( | gos_timezone_offset_t * | offset_ptr | ) |
Get the current timezone offset.
This returns the current timezone offset in seconds.
- Parameters
-
[out] offset_ptr
Point to hold the current timezone offset, see gos_timezone_offset_t
- Returns
- gos_result_t result of api call
◆ gos_time_get_uptime()
gos_result_t gos_time_get_uptime | ( | uint64_t * | uptime_ms_ptr | ) |
Returns the system's uptime.
The returns the number of milliseconds since the system was started.
- Parameters
-
[out] uptime_ms_ptr
Buffer to hold current up time in milliseconds
- Returns
- gos_result_t result of api call
◆ gos_time_iso8601_to_str()
gos_result_t gos_time_iso8601_to_str | ( | const gos_iso8601_t * | iso8601_struct, |
gos_iso8601_str_t * | iso8601_str |
||
) |
Convert from gos_iso8601_t to gos_iso8601_str_t.
This is a helper function to convert from a gos_iso8601_t to an gos_iso8601_str_t The returned gos_iso8601_str_t is null-terminated and can be directly printed as a string.
- Parameters
-
[in] iso8601_struct
UTC time as a gos_iso8601_t object [out] iso8601_str
converted, printable ISO8601 string
- Returns
- gos_result_t result of api call
◆ gos_time_iso8601_to_utc_ms()
gos_result_t gos_time_iso8601_to_utc_ms | ( | const gos_iso8601_t * | iso8601_struct, |
gos_utc_ms_t * | utc_ms_ptr |
||
) |
Convert from gos_iso8601_t to UTC time in milliseconds.
This is a helper function to convert from a gos_iso8601_t to UTC time in milliseconds
- Note
- The returned
utc_ms_ptr
will contain the timezone offset if the suppliediso8601_struct
contains a timezone offset.
- Parameters
-
[in] iso8601_struct
UTC time as a gos_iso8601_t object [out] utc_ms_ptr
Current UTC time in milliseconds
- Returns
- gos_result_t result of api call
◆ gos_time_set_current_utc_ms()
gos_result_t gos_time_set_current_utc_ms | ( | gos_utc_ms_t | time | ) |
Sets the current time in milliseconds.
This updates the current Real-Time Clock value (RTC). The value set will persist through reboots as long as the device is powered.
- Note
- This API is not needed if Network Time Protocol (NTP) is used. See gos_ntp_update() for more details
-
On some platforms the time can only be set to the nearest second. On these platforms, the millisecond part of the supplied
time
is dropped -
The specified
time
should NOT contain a timezone offset
- Parameters
-
[in] time
New UTC time, i.e. the current number of milliseconds since the Epoch
- Returns
- gos_result_t result of api call
◆ gos_time_set_timezone_offset()
gos_result_t gos_time_set_timezone_offset | ( | gos_timezone_offset_t | offset | ) |
Set the current timezone offset.
This updates the current timezone offset. The supplied offset
should be the a positive or negative integer in seconds from the UTC base time.
See time.zone for more details on setting the timezone via Gecko OS setting.
- Note
- You must invoke gos_settings_save() for the value to persist through reboots.
- Parameters
-
[in] offset
Timezone offset in seconds, see gos_timezone_offset_t
- Returns
- gos_result_t result of api call
◆ gos_time_utc_ms_to_iso8601()
gos_result_t gos_time_utc_ms_to_iso8601 | ( | gos_utc_ms_t | utc_ms, |
gos_timezone_offset_t | timezone_offset, |
||
gos_iso8601_t * | iso8601_struct |
||
) |
Convert from UTC time in milliseconds to gos_iso8601_t struct.
This is a helper function to convert from UTC time in milliseconds to a gos_iso8601_t struct
- Parameters
-
[in] utc_ms
Current UTC time in milliseconds WITHOUT a timezone offset [in] timezone_offset
Timezone offset in seconds, leave a 0 if not used [out] iso8601_struct
Pointer to gos_iso8601_t to hold converted time
- Returns
- gos_result_t result of api call
◆ gos_time_utc_ms_to_iso8601_str()
gos_result_t gos_time_utc_ms_to_iso8601_str | ( | gos_utc_ms_t | utc_ms, |
gos_timezone_offset_t | timezone_offset, |
||
gos_iso8601_str_t * | iso8601_str |
||
) |
Convert from UTC time in milliseconds to gos_iso8601_str_t struct.
This is a helper function to convert from UTC time in milliseconds to a gos_iso8601_str_t struct The gos_iso8601_str_t is null-terminated and can be directly printed as a string.
- Parameters
-
[in] utc_ms
Current UTC time in milliseconds WITHOUT a timezone offset [in] timezone_offset
Timezone offset in seconds, leave a 0 if not used [out] iso8601_str
Pointer to gos_iso8601_str_t to hold converted time as a string
- Returns
- gos_result_t result of api call
- Examples:
- file/log_file/main.c, and file/log_file_encrypted/main.c.