Api_system_shutdown
Data Structures |
|
struct | gos_shutdown_options_t |
Functions |
|
gos_result_t | gos_shutdown (const gos_shutdown_options_t *options) |
Put module into shutdown mode.
More...
|
|
Detailed Description
Function Documentation
◆ gos_shutdown()
gos_result_t gos_shutdown | ( | const gos_shutdown_options_t * |
options
|
) |
Put module into shutdown mode.
In shutdown mode there is no RAM retention. Upon wakeup the device reboots into its reset state.
See Gecko OS Command API documentation: shutdown .
- Note
-
Leave the
options
argument NULL to use the configured Gecko OS settings
- Parameters
-
[in] options
Options for how the device should wakeup, see gos_shutdown_options_t , leave NULL to use configured Gecko OS settings
- Returns
- gos_result_t result of API