App Execution Contexts #
Gecko OS app code can execute in several different contexts.
A context refers either to a thread, an IRQ, or an RTOS timer execution context.
A context essentially describes a processor's registers. When one context is swapped for another context, the current context's state (i.e. the processor's registers) is saved and the processor's registers are updated with the new context's previously saved state. Once the processor registers are updated with the new context's state the processor continues executing as if the new context were executing the whole time. In this way multiple independent contexts can exist in Gecko OS.
When in a context, all called functions execute within that context.
However, in one context you can set up an event that is handled in another context when the event takes place.
So, for example, if X is the current context, and functions A thru Z are called, every one of those functions execute in context X.
It's important to note that while executing functions A thru Z, context X could be temporarily suspended, and context Y could begin executing other functions. When context X resumes it continues executing its functions.
Note : By default all app code executes in the App thread context.
To execute in a different context, specific APIs or flags are required.
For each context below, there are details of the APIs and flags that determine execution in that context.
Context Attributes #
A context can be described by the following attributes.
Stack Space #
Stack space is the local memory available within the current context. Variables and buffers declared inside a function are considered local and reside 'on the stack'. When a function calls another function, the calling function's local variables are placed on the stack before going into the called function. In this way the stack is implemented as last-in-first-out (LIFO). A context has limited amount of stack space. If a context's stack overflows then hardfaults will likely occur.
Priority #
A context has a certain priority in the system. By priority, it is meant the algorithm used to determine which context to execute next. A given context can be 'preempted' by another context with higher priority.
Non-Blocking #
Certain contexts must never block. That is, code that executes in a non-blocking context must quickly execute then return. If a context allows for blocking then when a blocking section of code is executed, the blocked context is suspended and another non-blocked context resumes execution.
Initialized #
Some contexts are initialized on Gecko OS startup while others are initialized when needed.
Invoked #
Contexts are invoked in different ways. Some are event driven while others depend on hardware.
Summary of Context Attributes #
The execution contexts in the table below are listed in priority order, with highest priority at the top.
Execution Context | Stack Space | Priority | Non-blocking | Initialized | Invoked |
---|---|---|---|---|---|
Hardware IRQ 1 | 512 | IRQ (higher than RTOS scheduler) | N/A | When hardware IRQ triggered | |
RTOS Timer 1 | 512 | RTOS Scheduler (higher than Real time) | N/A | On RTOS timer time-out | |
System Event Thread 1 | 1K | Real time | On Gecko OS startup | When system event issued | |
Network Thread | 6K | Higher | On Gecko OS startup | When network event issued | |
HTTP Server Thread 2 | 5K | Higher / Medium (between these two values) | When HTTP Server starts | When HTTP request issued | |
App Thread | 6K | Medium | When App is loaded | When App has event to execute | |
Command Thread 2 | 6K | Medium | On Gecko OS startup | When external command received |
Notes
1 . Resources for these execution contexts are extremely limited. Defer complex processing to a context with more resources.
2 . These execution contexts have a system monitor to prevent lock-ups. Limit callback blocking time as specified in context description.
Available Contexts #
The following contexts are available to a Gecko OS App.
App Thread #
- Stack space: 6K (configurable)
- Priority: Medium (configurable)
- Non-blocking : False
- Initialized: When App is loaded
- Invoked: when App has event to execute
This is the default Gecko OS Application context. Unless otherwise specified, all App code executes within this context.
The following Gecko OS APIs issue events that are added to the App thread event queue, or register event handlers to be executed when an event is encountered in the event queue:
- Issue Event
-
Register Event Handler
- gos_network_register_event_handler()
- gos_network_register_softap_event_handler()
- gos_setup_register_client_event_handler()
- gos_setup_register_finished_event_handler()
- gos_tcp_register_client_event_handlers()
- gos_tcp_register_server_event_handlers()
- gos_udp_register_receive_event_handler()
- gos_websocket_register_server_event_handlers()
- gos_websocket_register_client_event_handlers()
Network Thread #
- Stack space: 6K
- Priority: High
- Non-blocking : False
- Initialized: On Gecko OS startup
- Invoked: when network event issued
This is where Gecko OS network related tasks execute. App code will execute in this context using the Event API and the GOS_EVENT_FLAG_IN_NETWORK_WORKER flag.
App code executes in the network thread with the following APIs:
Events execute in the network thread if issued or registered with the GOS_EVENT_FLAG_IN_NETWORK_WORKER flag using the following APIs:
System Event Thread #
- Stack space: 1K
- Priority: Medium-High
- Non-blocking : True
- Initialized: On Gecko OS startup
- Invoked: when system event issued
This is where simple Gecko OS tasks execute. For instance, this context is where the LEDs are updated.
Events that execute in the system event thread should be very simple and non-blocking.
Events execute in the system event thread if issued or registered with the GOS_EVENT_FLAG_IN_EVENT_THREAD flag using the following APIs:
HTTP Server Thread #
- Stack space: 5K
- Priority: Medium-High
- Non-blocking : False
- Initialized: When HTTP server starts
- Invoked: when HTTP request received
This is where HTTP server callbacks are executed. Code in this context may block, but no other HTTP server callbacks can execute until the current callback returns.
App code executes in the HTTP Server context with the following APIs:
-
Register URI and associated callback
- gos_hs_register_dynamic_page() , called by macro GOS_HTTP_SERVER_REGISTER_DYNAMIC_PAGES()
- Other HTTP server callbacks
The HTTP Server thread has a system monitor which ensures the serial command processor does not lock up.
HTTP request callbacks, e.g. gos_hs_register_dynamic_page() , must not block for more than 25s.
Command Thread #
- Stack space: 6K
- Priority: Medium
- Non-blocking : False
- Initialized: On Gecko OS startup
- Invoked: When external command received
This is where external commands are executed. While this context may block, no other external commands may execute until the current command completes.
External commands are received from:
- Serial console
- HTTP server REST API
- Remote terminal
- Command API
App code executes in the Command Thread context in response to the following APIs:
- Issue commands
The Command Thread has a system monitor which ensures the serial command processor does not lock up.
Custom command callbacks must NOT block for more than 30s. If a custom command does need to run longer then gos_cmd_update_system_monitor should periodically be called to update the system monitor before the 30s timeout.
Hardware IRQ #
- Stack space: 512
- Priority: IRQ (above 'Highest')
- Non-blocking : True
- Initialized: N/A
- Invoked: When hardware IRQ triggered
This is where an MCU interrupt vector executes. This has extremely high priority. Code in an IRQ must be extremely simple. Furthermore, an IRQ must never block.
When using an IRQ callback, defer heavy processing to the App Thread by using an RTOS object such as:
The App Thread should block on the RTOS object and begin executing when the object's state changes.
App code executes in a hardware IRQ context using the following APIs:
RTOS Timer #
- Stack space: 512
- Priority: Highest
- Non-blocking : True
- Initialized: N/A
- Invoked: On RTOS timer time-out
This is where an RTOS timer callback executes. An RTOS timer callback is very similar to a hardware IRQ callback .
The callback should be extremely simple and never block.
WARNING : An RTOS timer callback runs at a very high priority and has limited stack. RTOS timer callback processing must be very limited. Heavier processing should be done other threads, such as the App or network threads. Running the timer frequently, for example every 1ms, is strongly discouraged as it can lead to instabilities elsewhere in the system.
When using an RTOS timer callback, defer heavy processing to the App Thread by using an RTOS object such as:
App code executes in a RTOS timer context with the following API:
Comprehensive Execution Context Diagram #
Click diagram to zoom.