Bitstring
Bitstring utility. More...
Modules | |
Types | |
Bitstring data types. | |
Detailed Description
Bitstring utility.
Function Documentation
◆ gos_bitstring_alloc()
gos_result_t gos_bitstring_alloc | ( | gos_bitstring_t ** | bitstring_ptr, |
uint32_t | bit_count |
||
) |
Allocate a gos_bitstring_t object
- Note
- Use gos_free() to cleanup the allocated object
- Parameters
-
bitstring_ptr
Pointer to hold allocated object bit_count
Number of bits this string can hold
- Returns
- gos_result_t, result of API call
◆ gos_bitstring_bit_is_set()
bool gos_bitstring_bit_is_set | ( | const gos_bitstring_t * | bitstring, |
uint32_t | bit_index |
||
) |
Return if bit at index is set to 1
- Parameters
-
bitstring
gos_bitstring_t to check bit bit_index
Index of bit to return if it is set to 1
- Returns
- true if bit a
bit_index
is 1, false else
◆ gos_bitstring_clear_bit()
gos_result_t gos_bitstring_clear_bit | ( | gos_bitstring_t * | bitstring, |
uint32_t | bit_index |
||
) |
Clear bit to 0 at specified index
- Parameters
-
bitstring
gos_bitstring_t to clear bit in bit_index
Index of bit in string to clear to 0
- Returns
- gos_result_t, result of API call
◆ gos_bitstring_get_count()
uint32_t gos_bitstring_get_count | ( | const gos_bitstring_t * | bitstring | ) |
Return the number of bits set to 1 in the bitstring
- Parameters
-
bitstring
gos_bitstring_t to get count
- Returns
- Number of bits set to 1 in provided gos_bitstring_t
◆ gos_bitstring_get_index()
uint32_t gos_bitstring_get_index | ( | const gos_bitstring_t * | bitstring, |
uint32_t | nth_set_bit |
||
) |
Return index of nth set bit in string
This returns the index of the nth set it in the given gos_bitstring_t
- Parameters
-
bitstring
gos_bitstring_t to iterate nth_set_bit
Number of set bits to count
- Returns
- The index of the
nth_set_bit
in the given bitstring
◆ gos_bitstring_init()
gos_result_t gos_bitstring_init | ( | gos_bitstring_t * | bitstring, |
uint32_t | bit_count |
||
) |
Initialize a pre-allocated gos_bitstring_t object
- Parameters
-
bitstring
Pointer to pre-allocated gos_bitstring_t object bit_count
Number of bits this string can hold
- Returns
- gos_result_t, result of API call
◆ gos_bitstring_iterator_current()
uint32_t gos_bitstring_iterator_current | ( | const gos_bitstring_iterator_t * | iterator | ) |
Get the current index of the iterator
This returns the current index of the given iterator
. If the iterator has gone past all the SET bits in the bitstring then this will return UINT16_MAX.
- Note
- gos_bitstring_iterator_init() but be called first.
- Parameters
-
iterator
Iterator to get current index
- Returns
- Current index of iterator
◆ gos_bitstring_iterator_init()
gos_result_t gos_bitstring_iterator_init | ( | gos_bitstring_iterator_t * | iterator, |
const gos_bitstring_t * | bitstring |
||
) |
Initialize a gos_bitstring_iterator_t
This initializes a gos_bitstring_iterator_t which is used to iterate over the set bits in the specified bitstring.
- Parameters
-
iterator
gos_bitstring_iterator_t to initialize bitstring
gos_bitstring_t to iterate
- Returns
- gos_result_t, result of API call
◆ gos_bitstring_iterator_next()
uint32_t gos_bitstring_iterator_next | ( | gos_bitstring_iterator_t * | iterator | ) |
Get index of next SET bit of bitstring
This finds the next SET bit of the corresponding bitstring and returns its index in the string. If no more SET bits are found then this return UINT16_MAX.
- Note
- gos_bitstring_iterator_init() but be called first.
- Parameters
-
iterator
Iterator to find next SET bit in bitstring
- Returns
- Index of next SET bit in bitstring
◆ gos_bitstring_merge()
void gos_bitstring_merge | ( | gos_bitstring_t * | dest_bitstring, |
const gos_bitstring_t * | src_bitstring, |
||
bool | set_bits |
||
) |
Merge bitstrings
Merge the bits in src_bitstring
into dest_bitstring
. If set_bits
= true, then all the set bits in src_bitstring
while be set in dest_bitstring
. If set_bits
= false, then all the cleared bits in src_bitstring
while be cleared in dest_bitstring
.
- Note
- The given src_bitstring
and
dest_bitstring` do NOT need to be the same length.
- Parameters
-
dest_bitstring
String to update src_bitstring
String to merge into dest_bitstring
set_bits
If true then set corresponding bits in dest_bitstring
(e.g. OR operation), if false then clear corresponding bits indest_bitstring
(e.g. AND operation)
◆ gos_bitstring_reset()
gos_result_t gos_bitstring_reset | ( | gos_bitstring_t * | bitstring | ) |
Clear all bits to zero
This clears all bits in the given gos_bitstring_t to zero.
- Parameters
-
bitstring
gos_bitstring_t to clear to zero
- Returns
- gos_result_t, result of API call
◆ gos_bitstring_set_bit()
gos_result_t gos_bitstring_set_bit | ( | gos_bitstring_t * | bitstring, |
uint32_t | bit_index |
||
) |
Set bit to 1 at specified index
- Parameters
-
bitstring
gos_bitstring_t to set bit in bit_index
Index of bit in string to set to 1
- Returns
- gos_result_t, result of API call