Types
Log file types. More...
Data Structures | |
struct | gos_log_file_stats_t |
Information about a log file. More... | |
Typedefs | |
typedef uint16_t | gos_log_file_header_t |
Header prepended to each log record. More... | |
Detailed Description
Log file types.
Typedef Documentation
◆ gos_log_file_header_t
typedef uint16_t gos_log_file_header_t |
Header prepended to each log record.
- Note
- If the most-significant bit is cleared (i.e. 0) then the record is valid else the record is invalid (i.e. the log record data may not have been successfully written)