General API
HTTP server stream general API for both REST and Websocket clients. More...
Functions |
|
| gos_result_t | gos_hs_stream_register (const char *stream_name, gos_hs_stream_handler_t handler, gos_hs_stream_permissions_t permissions, void *arg) |
| gos_result_t | gos_hs_stream_unregister (const char *stream_name) |
| gos_result_t | gos_hs_stream_flush ( gos_msgpack_context_t *msgpack, uint32_t timeout_ms) |
| gos_result_t | gos_hs_stream_write_direct ( gos_msgpack_context_t *msgpack, const void *buffer, uint32_t length) |
Detailed Description
HTTP server stream general API for both REST and Websocket clients.
Function Documentation
◆ gos_hs_stream_flush()
| gos_result_t gos_hs_stream_flush | ( | gos_msgpack_context_t * |
msgpack,
|
| uint32_t |
timeout_ms
|
||
| ) |
Flush data to client
This is used to flush data back to a client.
Data should be flushed in two instances:
- Responding to a client read request
- Asynchronously writing to a websocket client
Responding to a client read request: When a client issues a read request, the corresponding stream handle
gos_hs_stream_handler_t
is invoked in the application thread context. In the handler, the application should use the msgpack APIs to populate the given
gos_msgpack_context_t
. Once the data is written to the
gos_msgpack_context_t
, it should be flushed using this API.
- Note
-
When responding to a client read request, the
timeout_msargument is the amount of time to wait for the response to be transferred.
Asynchronously writing to a websocket client: The application can asynchronously write data to a websocket client. This is done by first creating a write request with the gos_hs_stream_ws_write() API. The gos_hs_stream_ws_write() API creates a gos_msgpack_context_t that the application should populate with the msgpack APIs. Once the message is populated, this flush API is used to send the data to the websocket client.
- Note
-
When asynchronously writing a websocket client, the
timeout_msargument is the amount of time to wait for the client to respond with an acknowledgment that the packet was received. Iftimeout_msis 0 then the client will NOT return an acknowledgment. This allows for faster data transfer as the device does not need to wait for a response for each transmitted data packet.
- Parameters
-
[in] msgpackgos_msgpack_context_t to populate with data to send to remote client [in] timeout_msAmount of time in milliseconds to wait for either the data to be sent or the amount of time to wait for a response
- Returns
- gos_result_t result of api call
◆ gos_hs_stream_register()
| gos_result_t gos_hs_stream_register | ( | const char * |
stream_name,
|
| gos_hs_stream_handler_t |
handler,
|
||
| gos_hs_stream_permissions_t |
permissions,
|
||
| void * |
arg
|
||
| ) |
Register a stream handler
This registers a stream handler. Once a stream is registered, remote clients can issue read or write requests for the stream. When the client issues a request, the handler is invoked in the application thread context. See gos_hs_stream_handler_t for more details about how the handler works.
- Parameters
-
[in] stream_nameName of stream to listen [in] handlerHandler to be invoked when remote client issues a read/write request for stream [in] permissionsPermissions clients are allowed for this stream [in] argOptional argument to be supplied to stream handler. Leave NULL if unused.
- Returns
- gos_result_t result of api call
◆ gos_hs_stream_unregister()
| gos_result_t gos_hs_stream_unregister | ( | const char * |
stream_name
|
) |
Unregister a stream handler
Unregister a stream handler that was previously registered with gos_hs_stream_register() .
- Parameters
-
[in] stream_nameName of previously registered stream
- Returns
- gos_result_t result of api call
◆ gos_hs_stream_write_direct()
| gos_result_t gos_hs_stream_write_direct | ( | gos_msgpack_context_t * |
msgpack,
|
| const void * |
buffer,
|
||
| uint32_t |
length
|
||
| ) |
Directly write the msgpack context
Typically the msgpack APIs are used to populate the msgpack context. This API allows for directly writing msgpack-formatted data to the internal buffer.
- Parameters
-
[in] msgpackgos_msgpack_context_t to populate with data to send to remote client [in] bufferMsgpack-formatted data to write to context [in] lengthLength of given buffer in bytes
- Returns
- gos_result_t result of api call
- Examples:
- hurricane/arducam/camera.c .