gos_http_request_t Struct Reference
HTTP request context. More...
Data Fields | |
const char * | url |
The HTTP request URL, if no schema is included http:// is used. | |
gos_tls_certificates_t | certs |
For HTTPS (secure) request, the TLS cert filenames, gos_tls_certificates_t. | |
const char * | content_type |
int32_t | content_length |
gos_interface_t | interface |
Network interface, gos_interface_t. | |
gos_http_method_t | method |
bool | use_secure_element |
If true, the secure element will be used for all registered TLS operations. | |
Detailed Description
HTTP request context.
Field Documentation
◆ content_length
int32_t gos_http_request_t::content_length |
Specifies the content length that will be sent. If greater/equal to zero then specifies the 'content-length' header If equal -1, then specifies 'transfer-encoding: chunked' and writes are chunked encoded
- Note
- this only used for a POST request.
◆ content_type
const char* gos_http_request_t::content_type |
The 'content-type' header
- Note
- this only used for a POST request.
◆ method
gos_http_method_t gos_http_request_t::method |
HTTP request method, gos_http_method_t
- Note
- This is only used for gos_http_open_request()