gos_dynamic_buffer_t Struct Reference
Data Fields | |
uint8_t * | buffer |
Pointer to allocated buffer. | |
const uint8_t * | buffer_end |
Pointer to end of allocated buffer. | |
uint8_t * | append |
Pointer to where data should be appended to the buffer. | |
uint8_t * | prepend |
Pointer to where data should be prepended to the buffer. | |
Detailed Description
Dynamic buffer context
- Examples:
- cloud/dps_demo/main.c.