Telemetry
DMS Telemetry. More...
Functions |
|
void | gos_dms_set_telemetry_callback ( gos_dms_telemetry_callback_t callback) |
Set callback to allow for posting custom telemetry information to the DMS.
More...
|
|
gos_result_t | gos_dms_post_telemetry (void) |
Force the device to immediately post telemetry to the DMS.
More...
|
|
Detailed Description
DMS Telemetry.
Function Documentation
◆ gos_dms_post_telemetry()
gos_result_t gos_dms_post_telemetry | ( | void |
|
) |
Force the device to immediately post telemetry to the DMS.
This force the device to immediately post telemetry information to the DMS.
- Returns
- Result of API, see gos_result_t
◆ gos_dms_set_telemetry_callback()
void gos_dms_set_telemetry_callback | ( | gos_dms_telemetry_callback_t |
callback
|
) |
Set callback to allow for posting custom telemetry information to the DMS.
This sets a callback which is invoked when the device posts telemetry information to the DMS.
The callback executes in the Network Thread context. It is invoked when gos_dms_post_telemetry() is called and/or every dms.telemetry.interval milliseconds.
Refer to gos_dms_telemetry_callback_t for more information about the callback.
- Parameters
-
callback
Callback which enables posting custom telemetry to DMS. See gos_dms_telemetry_callback_t
- Examples:
- dms/telemetry/main.c .