Contains information about a SoftAP client. More...
Data Fields | |
gos_mac_t | mac |
Mac address. | |
bool | valid |
Connection status. | |
uint8_t | reserved |
Addtional client information (specific to the softap type) | |
uint32_t | ipv4_address |
IPv4 address of client. | |
Detailed Description
Contains information about a SoftAP client.
- Examples:
- network/softap_tcp_server/main.c, and wifi/web_setup/main.c.