gos_file_system_stats_t Struct Reference
Statistics about the file system. More...
Data Fields | |
uint32_t | file_count |
Number of files on the file system (based on the memory type, e.g. extended or bulk) | |
uint32_t | bytes_available |
Number of bytes available for files. | |
uint32_t | bytes_used |
Number of bytes used by current files. | |
uint32_t | total_size |
Total size (in bytes) of the flash memory type, e.g. extended or bulk) | |
Detailed Description
Statistics about the file system.