Miscellaneous
RTOS miscellaneous functions. More...
Functions | |
uint32_t | gos_rtos_get_time (void) |
Get the current system tick count. More... | |
gos_result_t | gos_rtos_delay_milliseconds (uint32_t milliseconds) |
Sleep for a given period. More... | |
Detailed Description
RTOS miscellaneous functions.
Function Documentation
◆ gos_rtos_delay_milliseconds()
gos_result_t gos_rtos_delay_milliseconds | ( | uint32_t | milliseconds | ) |
Sleep for a given period.
Causes the current thread to sleep for AT LEAST the specified number of milliseconds. If the processor is heavily loaded with higher priority tasks, the delay may be longer than requested.
- Parameters
-
[in] milliseconds
: Time to sleep in milliseconds
- Returns
- Result of API call, gos_result_t
◆ gos_rtos_get_time()
uint32_t gos_rtos_get_time | ( | void |
| ) |
Get the current system tick count.
The system tick counter increments every millisecond. The value wraps back to zero after 2^32 milliseconds have passed since startup.
- Returns
- Number of milliseconds since system was started