gos_http_response_t Struct Reference
HTTP response struct used by gos_http_receive_response() More...
Data Fields | |
int | version |
int | code |
HTTP response code. | |
int | content_length |
char * | headers [GOS_HTTP_BASIC_HEADER_COUNT] |
'Basic' HTTP response headers, see gos_http_basic_header_t | |
gos_http_response_header_t * | header_list |
uint8_t * | buffer |
Allocated HTTP response headers buffer (system use only) | |
Detailed Description
HTTP response struct used by gos_http_receive_response()
- Note
- This does NOT include the response body
Field Documentation
◆ content_length
int gos_http_response_t::content_length |
The response body length
- Note
- -1 means the response body is chunked
◆ header_list
gos_http_response_header_t* gos_http_response_t::header_list |
Linked list of additional response headers
- Note
- Must set GOS_HTTP_RESPONSE_ALL_HEADERS flag to return additional headers
◆ version
int gos_http_response_t::version |
The version of the HTTP response,
- 0 = HTTP/1.0
- 1 = HTTP/1.1