GPIO
Functions for using General Purpose Input/Output (GPIO) peripheral. More...
Modules |
|
| Types | |
|
Hardware GPIO data types.
|
|
Functions |
|
| gos_result_t | gos_gpio_init ( gos_gpio_t gpio, gos_gpio_config_t direction, bool init_val) |
|
Initialize GPIO as input or output.
More...
|
|
| gos_result_t | gos_gpio_direct_init ( gos_gpio_t gpio, gos_gpio_config_t direction) |
|
Initialize GPIO as input or output.
More...
|
|
| gos_result_t | gos_gpio_deinit ( gos_gpio_t gpio) |
De-initialize a GPIO. This is the equivalent of using the Command API function
gpio_dir
with argument
none
More...
|
|
| gos_result_t | gos_gpio_set ( gos_gpio_t gpio, bool value) |
|
Set value of output GPIO (HIGH or LOW)
More...
|
|
| gos_result_t | gos_gpio_direct_set ( gos_gpio_t gpio, bool value) |
|
Set value of output GPIO (HIGH or LOW)
More...
|
|
| bool | gos_gpio_get ( gos_gpio_t gpio) |
|
Get value of GPIO.
More...
|
|
| gos_result_t | gos_gpio_irq_enable ( gos_gpio_t gpio, gos_gpio_irq_trigger_t edge, gos_handler_t callback, void *arg) |
|
Execute the given callback when the specified edge event is detected on the GPIO.
More...
|
|
| gos_result_t | gos_gpio_irq_disable ( gos_gpio_t gpio) |
|
Disables an interrupt trigger for an input GPIO pin.
More...
|
|
| gos_result_t | gos_gpio_mask_set (uint32_t gpio_mask) |
|
Set output GPIOs HIGH.
More...
|
|
| gos_result_t | gos_gpio_mask_clear (uint32_t gpio_mask) |
|
Set output GPIOs LOW.
More...
|
|
| uint32_t | gos_gpio_mask_get (uint32_t gpio_mask) |
|
Return value of GPIOs.
More...
|
|
Detailed Description
Functions for using General Purpose Input/Output (GPIO) peripheral.
Function Documentation
◆ gos_gpio_deinit()
| gos_result_t gos_gpio_deinit | ( | gos_gpio_t |
gpio
|
) |
De-initialize a GPIO. This is the equivalent of using the Command API function
gpio_dir
with argument
none
See Gecko OS Command API documentation: gpio_dir .
- Note
- The GPIO must be initialized with gos_gpio_init() first.
◆ gos_gpio_direct_init()
| gos_result_t gos_gpio_direct_init | ( | gos_gpio_t |
gpio,
|
| gos_gpio_config_t |
direction
|
||
| ) |
Initialize GPIO as input or output.
- Note
- This only initializes the GPIO at the hardware level. Use gos_gpio_init() for Gecko OS to be aware of this GPIO.
◆ gos_gpio_direct_set()
| gos_result_t gos_gpio_direct_set | ( | gos_gpio_t |
gpio,
|
| bool |
value
|
||
| ) |
Set value of output GPIO (HIGH or LOW)
- Note
- This bypass Gecko OS and directly accesses the GPIO driver.
◆ gos_gpio_get()
| bool gos_gpio_get | ( | gos_gpio_t |
gpio
|
) |
Get value of GPIO.
See Gecko OS Command API documentation: gpio_set .
- Note
- The gpio need NOT be initialized as an input first.
◆ gos_gpio_init()
| gos_result_t gos_gpio_init | ( | gos_gpio_t |
gpio,
|
| gos_gpio_config_t |
direction,
|
||
| bool |
init_val
|
||
| ) |
Initialize GPIO as input or output.
See Gecko OS Command API documentation: gpio_dir .
◆ gos_gpio_irq_disable()
| gos_result_t gos_gpio_irq_disable | ( | gos_gpio_t |
gpio
|
) |
Disables an interrupt trigger for an input GPIO pin.
Disables an interrupt trigger for an input GPIO pin. Using this function on a gpio pin which has not been set up using gos_gpio_irq_enable() is undefined.
- Parameters
-
gpio: the gpio pin which provided the interrupt trigger
◆ gos_gpio_irq_enable()
| gos_result_t gos_gpio_irq_enable | ( | gos_gpio_t |
gpio,
|
| gos_gpio_irq_trigger_t |
edge,
|
||
| gos_handler_t |
callback,
|
||
| void * |
arg
|
||
| ) |
Execute the given callback when the specified edge event is detected on the GPIO.
The callback is executed in the IRQ context and MUST be very light-weight. All heavy processing should be deferred to the app thread.
- Note
- The corresponding GPIO need MUST be configured as an input first.
- Examples:
- peripheral/gpio_irq/main.c .
◆ gos_gpio_mask_clear()
| gos_result_t gos_gpio_mask_clear | ( | uint32_t |
gpio_mask
|
) |
Set output GPIOs LOW.
For any bit in the mask that's '1', the corresponding GPIO's value is driven LOW ('0' valued bits are ignored)
- Note
- The corresponding GPIO must be configured as an OUTPUT first.
◆ gos_gpio_mask_get()
| uint32_t gos_gpio_mask_get | ( | uint32_t |
gpio_mask
|
) |
Return value of GPIOs.
For any bit in the mask that's '1', the corresponding GPIO's value is read and returned in the value mask.
- Note
- The corresponding GPIO need NOT be configured as an input first.
◆ gos_gpio_mask_set()
| gos_result_t gos_gpio_mask_set | ( | uint32_t |
gpio_mask
|
) |
Set output GPIOs HIGH.
For any bit in the mask that's '1', the corresponding GPIO's value is driven HIGH ('0' valued bits are ignored)
- Note
- The corresponding GPIO must be configured as an OUTPUT first.
◆ gos_gpio_set()
| gos_result_t gos_gpio_set | ( | gos_gpio_t |
gpio,
|
| bool |
value
|
||
| ) |
Set value of output GPIO (HIGH or LOW)
- Note
- The GPIO must be initialized as an output with gos_gpio_init() first.
- Examples:
- intro/blinky/main.c , network/http_server/requests/get_params.c , network/http_server/requests/json_parser.c , network/http_server/requests/set_light.c , network/http_server/requests/toggle_light.c , network/http_server_stream/main.c , peripheral/gpio_irq/main.c , and system/indicator/main.c .