Key Pair
Elliptic Curve keypair APIs. More...
Functions |
|
| gos_result_t | gos_atca_calculate_public_key (uint16_t slot_id, uint8_t *public_key) |
| gos_result_t | gos_atca_write_public_key (uint16_t slot_id, uint8_t *public_key) |
| gos_result_t | gos_atca_generate_keypair (uint16_t slot_id, uint8_t *public_key) |
| gos_result_t | gos_atca_get_public_key (uint16_t slot_id, uint8_t *public_key) |
Detailed Description
Elliptic Curve keypair APIs.
Function Documentation
◆ gos_atca_calculate_public_key()
| gos_result_t gos_atca_calculate_public_key | ( | uint16_t |
slot_id,
|
| uint8_t * |
public_key
|
||
| ) |
Calculate the EC public key based on the private key at the specified slot
- Parameters
-
[in] slot_idSlot with existing private key [out] public_keyCalculated public key. Format will be the X and Y integers in big-endian format. 64 bytes for P256 curve.
- Returns
- gos_result_t result of API
- Examples:
- demo/secure_element/commands.c .
◆ gos_atca_generate_keypair()
| gos_result_t gos_atca_generate_keypair | ( | uint16_t |
slot_id,
|
| uint8_t * |
public_key
|
||
| ) |
Issues GenKey command, which generates a new random private key in slot and returns the public key.
- Parameters
-
[in] slot_idSlot number where an ECC private key is configured. Can also be ATCA_TEMPKEY_KEYID to generate a private key in TempKey. [out] public_keyPublic key will be returned here. Format will be the X and Y integers in big-endian format. 64 bytes for P256 curve. Set to NULL if public key isn't required.
- Returns
- gos_result_t result of API
- Examples:
- demo/secure_element/se_utils.c .
◆ gos_atca_get_public_key()
| gos_result_t gos_atca_get_public_key | ( | uint16_t |
slot_id,
|
| uint8_t * |
public_key
|
||
| ) |
Executes Read command to read an ECC P256 public key from a slot configured for clear reads.
This function assumes the public key is stored using the ECC public key format specified in the datasheet.
- Parameters
-
[in] slot_idSlot number to read from. Only slots 8 to 15 are large enough for a public key. [out] public_keyPublic key is returned here (64 bytes). Format will be the 32 byte X and Y big-endian integers concatenated.
- Returns
- gos_result_t result of API
- Examples:
- demo/secure_element/commands.c .
◆ gos_atca_write_public_key()
| gos_result_t gos_atca_write_public_key | ( | uint16_t |
slot_id,
|
| uint8_t * |
public_key
|
||
| ) |
Executes the Write command, which writes a public key to a data slot in the SE format
- Parameters
-
[in] slot_idSlot number to write. Only slots 8 to 15 are large enough to store a public key. [in] public_keyPublic key to write into the slot specified. X and Y integers in big-endian format. 64 bytes for P256 curve.
- Returns
- gos_result_t result of API
- Examples:
- demo/secure_element/commands.c .