Types
Command types. More...
Typedefs | |
typedef gos_result_t(* | gos_cmd_writer_t) (void *user, const void *data, uint32_t length) |
Command writer prototype. More... | |
typedef gos_result_t(* | gos_cmd_write_poller_t) (void *user, uint32_t *bytes_available) |
Command write poller prototype. More... | |
Enumerations | |
enum | gos_cmd_result_t { GOS_CMD_SUCCESS = 0, GOS_CMD_FAILED = 1, GOS_CMD_PARSE_ERROR = 2, GOS_CMD_UNKNOWN = 3, GOS_CMD_TOO_FEW_ARGS = 4, GOS_CMD_TOO_MANY_ARGS = 5, GOS_CMD_UNKNOWN_OPTION = 6, GOS_CMD_BAD_ARGS = 7, GOS_CMD_BUFFER_OVERFLOW = 8, GOS_CMD_BOUNDS_ERROR = 9, GOS_CMD_SET_OK = 10, GOS_CMD_EXECUTE_AOK = 11, GOS_CMD_STOPPED = 12, GOS_CMD_IN_PROGRESS = 13, GOS_CMD_TIMEOUT = 14, GOS_CMD_INVALID_RESPONSE = 15 } |
Gecko OS command response codes. More... | |
Detailed Description
Command types.
Typedef Documentation
◆ gos_cmd_write_poller_t
typedef gos_result_t(* gos_cmd_write_poller_t) (void *user, uint32_t *bytes_available) |
Command write poller prototype.
This is used with gos_cmd_read_write_data()
- Parameters
-
user
User argument supplied to gos_cmd_read_write_data() bytes_available_ptr
Pointer to hold number of bytes available
- Returns
- Result of writing, if success should return GOS_SUCCESS, else appropriate error code, see gos_result_t
◆ gos_cmd_writer_t
typedef gos_result_t(* gos_cmd_writer_t) (void *user, const void *data, uint32_t length) |
Command writer prototype.
This is used with gos_cmd_read_write_data()
- Parameters
-
user
User argument supplied to gos_cmd_read_write_data() data
Data to write length
Length of data to write
- Returns
- Result of writing, if success should return GOS_SUCCESS, else appropriate error code, see gos_result_t
Enumeration Type Documentation
◆ gos_cmd_result_t
enum gos_cmd_result_t |
Gecko OS command response codes.