Circular Queue
Circular Queue. More...
Modules |
|
| Types | |
|
Circular Queue data types.
|
|
Detailed Description
Circular Queue.
A circular queue is a First In, First Out (FIFO) data structure that will 'wrap' to the beginning once the end of the list is reached.
This circular queue implementation stores the contents of each entry internally. This means an entry's memory does NOT need to persist after the entry is added to the queue.
Function Documentation
◆ gos_safe_circular_queue_flush()
| void gos_safe_circular_queue_flush | ( | gos_safe_circular_queue_t * |
queue,
|
| gos_safe_circular_queue_flush_callback_t |
callback
|
||
| ) |
Remove all entries from queue
This removes all entries from the queue, optionally calling the given
callback
for each entry.
- Parameters
-
[in] queueThread-safe, circular queue [in] callbackCallback to be invoked for each entry in queue, leave NULL if unused
- Returns
- gos_result_t , result of API
◆ gos_safe_circular_queue_get_count()
| uint16_t gos_safe_circular_queue_get_count | ( | const gos_safe_circular_queue_t * |
queue
|
) |
Return number of entries in queue
- Parameters
-
[in] queueThread-safe, circular queue
- Returns
- Number of entries in queue
◆ gos_safe_circular_queue_get_free_space_count()
| uint16_t gos_safe_circular_queue_get_free_space_count | ( | const gos_safe_circular_queue_t * |
queue
|
) |
Return available slots in queue
- Parameters
-
[in] queueThread-safe, circular queue
- Returns
- Number of unused/free slots in queue (i.e. free space)
◆ gos_safe_circular_queue_get_head()
| void* gos_safe_circular_queue_get_head | ( | gos_safe_circular_queue_t * |
queue
|
) |
Return pointer to head (i.e. oldest entry) of queue
- Note
- WARN: The returned pointer is NOT thread-safe!
- Parameters
-
[in] queueThread-safe, circular queue
- Returns
- Pointer to head of queue
◆ gos_safe_circular_queue_get_tail()
| void* gos_safe_circular_queue_get_tail | ( | gos_safe_circular_queue_t * |
queue
|
) |
Return pointer to tail (i.e. next available slot) of queue
- Note
- WARN: The returned pointer is NOT thread-safe!
- Parameters
-
[in] queueThread-safe, circular queue
- Returns
- Pointer to tail of queue
◆ gos_safe_circular_queue_init()
| gos_result_t gos_safe_circular_queue_init | ( | gos_safe_circular_queue_t * |
queue,
|
| void * |
buffer,
|
||
| uint16_t |
entry_size,
|
||
| uint16_t |
max_entry_count
|
||
| ) |
Initialize a thread-safe circular queue (aka FIFO)
This initialize a gos_safe_circular_queue_t context.
- Note
-
The given
buffermust be pre-allocated and large enough to holdentry_size X max_entry_countbytes of data.
- Parameters
-
[in] queueThread-safe, circular queue to initialize [in] bufferPre-allocated buffer to hold queue entries [in] entry_sizeSize in bytes of each queue entry [in] max_entry_countMaximum number of entries the queue can hold
- Returns
- gos_result_t , result of API
◆ gos_safe_circular_queue_is_empty()
| bool gos_safe_circular_queue_is_empty | ( | const gos_safe_circular_queue_t * |
queue
|
) |
Return if queue is empty
- Parameters
-
[in] queueThread-safe, circular queue
- Returns
- true if empty, false else
◆ gos_safe_circular_queue_is_full()
| bool gos_safe_circular_queue_is_full | ( | const gos_safe_circular_queue_t * |
queue
|
) |
Return if queue is full
- Parameters
-
[in] queueThread-safe, circular queue
- Returns
- true if full, false else
◆ gos_safe_circular_queue_pop()
| gos_result_t gos_safe_circular_queue_pop | ( | gos_safe_circular_queue_t * |
queue,
|
| void * |
entry
|
||
| ) |
Remove oldest entry from queue
This removes the oldest entry from the beginning of the queue (aka FIFO).
- Note
- This API does NOT block, if the queue is empty then this fails immediately.
- Parameters
-
[in] queueThread-safe, circular queue [out] entryBuffer to hold removed entry, leave NULL if unused
- Returns
- gos_result_t , result of API
◆ gos_safe_circular_queue_push()
| gos_result_t gos_safe_circular_queue_push | ( | gos_safe_circular_queue_t * |
queue,
|
| void * |
entry
|
||
| ) |
Add an entry to the end of the queue
This pushes an entry to the end of the queue (aka FIFO).
- Note
-
After calling this API, the given
entrymay be discarded as the entry's data is memcpy'd into the queue buffer. - This API does NOT block, if there is no room in the queue then it fails immediately.
- Parameters
-
[in] queueThread-safe, circular queue [in] entryEntry to memcpy to end of FIFO
- Returns
- gos_result_t , result of API
◆ gos_safe_circular_queue_tail_is_last_entry()
| bool gos_safe_circular_queue_tail_is_last_entry | ( | gos_safe_circular_queue_t * |
queue
|
) |
Return if the tail is at end of buffer
This returns if the tail entry is also the last slot of the queue buffer. This is useful to determine if the queue is about to wrap to the beginning of the buffer.
- Parameters
-
[in] queueThread-safe, circular queue
- Returns
- true if tail is at end of buffer, false else