Macros
MessagePack macros. More...
Macros |
|
| #define | MSGPACK_BOOL (obj) _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object8_t , boolean) |
| #define | MSGPACK_INT8 (obj) _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object8_t , s) |
| #define | MSGPACK_UINT8 (obj) _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object8_t , u) |
| #define | MSGPACK_INT16 (obj) _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object16_t , s) |
| #define | MSGPACK_UINT16 (obj) _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object16_t , u) |
| #define | MSGPACK_INT32 (obj) _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object32_t , s) |
| #define | MSGPACK_UINT32 (obj) _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object32_t , u) |
| #define | MSGPACK_FLOAT (obj) _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object32_t , flt) |
| #define | MSGPACK_INT64 (obj) _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object64_t , s) |
| #define | MSGPACK_UINT64 (obj) _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object64_t , u) |
| #define | MSGPACK_DOUBLE (obj) _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object64_t , dbl) |
| #define | MSGPACK_DICT (obj, key) gos_msgpack_get_dict_object (( gos_msgpack_object_dict_t *)obj, key, MSGPACK_TYPE_ANY ) |
| #define | MSGPACK_DICT_TYPE (obj, key, type) gos_msgpack_get_dict_object (( gos_msgpack_object_dict_t *)obj, key, MSGPACK_TYPE_ ## type) |
| #define | MSGPACK_DICT_STR (obj, key) ( gos_msgpack_object_str_t *) MSGPACK_DICT_TYPE (obj, key, STR) |
| #define | MSGPACK_DICT_BIN (obj, key) ( gos_msgpack_object_bin_t *) MSGPACK_DICT_TYPE (obj, key, BIN) |
| #define | MSGPACK_DICT_DICT (obj, key) ( gos_msgpack_object_dict_t *) MSGPACK_DICT_TYPE (obj, key, DICT) |
| #define | MSGPACK_DICT_ARRAY (obj, key) ( gos_msgpack_object_array_t *) MSGPACK_DICT_TYPE (obj, key, ARRAY) |
| #define | MSGPACK_DICT_INT (obj, key) MSGPACK_DICT_TYPE (obj, key, INT_OR_UINT) |
| #define | MSGPACK_DICT_UINT (obj, key) MSGPACK_DICT_TYPE (obj, key, INT_OR_UINT) |
| #define | MSGPACK_ARRAY (obj, index) gos_msgpack_get_array_object (( gos_msgpack_object_array_t *)obj, index, MSGPACK_TYPE_ANY ) |
| #define | MSGPACK_ARRAY_TYPE (obj, index, type) gos_msgpack_get_array_object (( gos_msgpack_object_array_t *)obj, index, MSGPACK_TYPE_ ## type) |
| #define | MSGPACK_ARRAY_DICT (obj, index) ( gos_msgpack_object_dict_t *) MSGPACK_ARRAY_TYPE (obj, index, DICT) |
| #define | MSGPACK_ARRAY_ARRAY (obj, index) ( gos_msgpack_object_array_t *) MSGPACK_ARRAY_TYPE (obj, index, ARRAY) |
| #define | MSGPACK_ARRAY_LENGTH (obj) ((( gos_msgpack_object_array_t *)obj)->count) |
| #define | MSGPACK_ARRAY_STR (obj, index) ( gos_msgpack_object_str_t *) MSGPACK_ARRAY_TYPE (obj, index, STR) |
| #define | MSGPACK_ARRAY_BIN (obj, index) ( gos_msgpack_object_bin_t *) MSGPACK_ARRAY_TYPE (obj, index, BIN) |
| #define | MSGPACK_ARRAY_INT (obj, index) MSGPACK_ARRAY_TYPE (obj, index, INT) |
| #define | MSGPACK_ARRAY_UINT (obj, index) MSGPACK_ARRAY_TYPE (obj, index, UINT) |
| #define | MSGPACK_STR_VALUE (obj) ((const gos_msgpack_object_str_t *)(obj))->data |
| #define | MSGPACK_STR_LENGTH (obj) ((const gos_msgpack_object_str_t *)(obj))->length |
| #define | MSGPACK_STR_CMP (obj, str) gos_msgpack_str_cmp (( gos_msgpack_object_t *)obj, str) |
| #define | MSGPACK_BIN_VALUE (obj) ((const gos_msgpack_object_bin_t *)(obj))->data |
| #define | MSGPACK_BIN_LENGTH (obj) ((const gos_msgpack_object_bin_t *)(obj))->length |
| #define | MSGPACK_BIN_CMP (obj, mem) memcmp( MSGPACK_BIN_VALUE (obj), mem, MSGPACK_BIN_LENGTH (obj)) |
| #define | MSGPACK_INT (obj) gos_msgpack_get_int (obj) |
| #define | MSGPACK_UINT (obj) gos_msgpack_get_uint (obj) |
| #define | MSGPACK_LONG (obj, buffer) gos_msgpack_get_long (obj, buffer) |
| #define | MSGPACK_ULONG (obj, buffer) gos_msgpack_get_ulong (obj, buffer) |
| #define | MSGPACK_STR (obj, buffer, max_length) gos_msgpack_get_str (( gos_msgpack_object_t *)obj, buffer, max_length) |
| #define | MSGPACK_BIN (obj, mem, max_length) memcpy(mem, MSGPACK_BIN_VALUE (obj), MIN (max_length, MSGPACK_BIN_LENGTH (obj))) |
| #define | MSGPACK_TO_STR (obj, buffer, max_length) gos_msgpack_to_str (( gos_msgpack_object_t *)obj, buffer, max_length) |
| #define | MSGPACK_IS_NIL (obj) _MSGPACK_IS_(obj, NIL) |
| #define | MSGPACK_IS_BOOL (obj) _MSGPACK_IS_(obj, BOOL) |
| #define | MSGPACK_IS_INT8 (obj) _MSGPACK_IS_(obj, INT8) |
| #define | MSGPACK_IS_UINT8 (obj) _MSGPACK_IS_(obj, UINT8) |
| #define | MSGPACK_IS_INT16 (obj) _MSGPACK_IS_(obj, INT16) |
| #define | MSGPACK_IS_UINT16 (obj) _MSGPACK_IS_(obj, UINT16) |
| #define | MSGPACK_IS_INT32 (obj) _MSGPACK_IS_(obj, INT32) |
| #define | MSGPACK_IS_UINT32 (obj) _MSGPACK_IS_(obj, UINT32) |
| #define | MSGPACK_IS_INT64 (obj) _MSGPACK_IS_(obj, INT64) |
| #define | MSGPACK_IS_UINT64 (obj) _MSGPACK_IS_(obj, UINT64) |
| #define | MSGPACK_IS_UINT (obj) gos_msgpack_object_is_type (( gos_msgpack_object_t *)obj, MSGPACK_TYPE_UINT ) |
| #define | MSGPACK_IS_INT (obj) gos_msgpack_object_is_type (( gos_msgpack_object_t *)obj, MSGPACK_TYPE_INT ) |
| #define | MSGPACK_IS_FLOAT (obj) _MSGPACK_IS_(obj, FLOAT) |
| #define | MSGPACK_IS_DOUBLE (obj) _MSGPACK_IS_(obj, DOUBLE) |
| #define | MSGPACK_IS_STR (obj) _MSGPACK_IS_(obj, STR) |
| #define | MSGPACK_IS_BIN (obj) _MSGPACK_IS_(obj, BIN) |
| #define | MSGPACK_IS_DICT (obj) _MSGPACK_IS_(obj, DICT) |
| #define | MSGPACK_IS_ARRAY (obj) _MSGPACK_IS_(obj, ARRAY) |
| #define | MSGPACK_NIL 0xC0 |
| #define | MSGPACK_FALSE 0xC2 |
| #define | MSGPACK_TRUE 0xC3 |
| #define | MSGPACK_INIT_WITH_BUFFER (name, _buf, _len) |
| #define | MSGPACK_INIT_CONTEXT_WITH_BUFFER (context, _buf, _len) |
| #define | MSGPACK_INIT_WITH_WRITER (name, _writer, _user) |
| #define | MSGPACK_SET_WRITER (context, _writer, _user) |
| #define | MSGPACK_BUFFER_USED (ctx) (uint16_t)((ctx)->buffer.ptr - (ctx)->buffer.buffer) |
| #define | MSGPACK_BUFFER_REMAINING (ctx) (uint16_t)((ctx)->buffer.end - (ctx)->buffer.ptr) |
| #define | MSGPACK_DICT_GET_OBJECT (dict, key) gos_msgpack_get_dict_object ((const gos_msgpack_object_dict_t *)dict, key, MSGPACK_TYPE_ANY ) |
| #define | MSGPACK_ARRAY_GET_OBJECT (array, index) gos_msgpack_get_array_object (( gos_msgpack_object_array_t *)array, index, MSGPACK_TYPE_ANY ) |
| #define | MSGPACK_FOREACH (dict_or_array, callback, arg) gos_msgpack_foreach ((const gos_msgpack_object_t *)dict_or_array, callback, arg, 0) |
| #define | MSGPACK_FOREACH_RECURSIVE (dict_or_array, callback, arg) gos_msgpack_foreach ((const gos_msgpack_object_t *)dict_or_array, callback, arg, UINT32_MAX) |
| #define | MSGPACK_FREE_OBJECTS (obj) gos_msgpack_free_objects (obj) |
Detailed Description
MessagePack macros.
Macro Definition Documentation
◆ MSGPACK_ARRAY
| #define MSGPACK_ARRAY | ( |
obj,
|
|
index
|
|||
| ) | gos_msgpack_get_array_object (( gos_msgpack_object_array_t *)obj, index, MSGPACK_TYPE_ANY ) |
Get MessagePack object at specific index of array
◆ MSGPACK_ARRAY_ARRAY
| #define MSGPACK_ARRAY_ARRAY | ( |
obj,
|
|
index
|
|||
| ) | ( gos_msgpack_object_array_t *) MSGPACK_ARRAY_TYPE (obj, index, ARRAY) |
Get MessagePack array at index with a ARRAY type, return NULL if the entry is found but the wrong type
◆ MSGPACK_ARRAY_BIN
| #define MSGPACK_ARRAY_BIN | ( |
obj,
|
|
index
|
|||
| ) | ( gos_msgpack_object_bin_t *) MSGPACK_ARRAY_TYPE (obj, index, BIN) |
Get MessagePack array at index with a BIN type, return NULL if the entry is found but the wrong type
◆ MSGPACK_ARRAY_DICT
| #define MSGPACK_ARRAY_DICT | ( |
obj,
|
|
index
|
|||
| ) | ( gos_msgpack_object_dict_t *) MSGPACK_ARRAY_TYPE (obj, index, DICT) |
Get MessagePack array at index with a DICT type, return NULL if the entry is found but the wrong type
◆ MSGPACK_ARRAY_GET_OBJECT
| #define MSGPACK_ARRAY_GET_OBJECT | ( |
array,
|
|
index
|
|||
| ) | gos_msgpack_get_array_object (( gos_msgpack_object_array_t *)array, index, MSGPACK_TYPE_ANY ) |
Return the object a the corresponding index in an array
- See also
- gos_msgpack_get_array_object() for more info
- Examples:
- utility/msgpack/read_write_buffer.c , and utility/msgpack/read_write_stream.c .
◆ MSGPACK_ARRAY_INT
| #define MSGPACK_ARRAY_INT | ( |
obj,
|
|
index
|
|||
| ) | MSGPACK_ARRAY_TYPE (obj, index, INT) |
Get MessagePack array at index with a signed integer (unsigned and bool included) type, return NULL if the entry is found but the wrong type
◆ MSGPACK_ARRAY_LENGTH
| #define MSGPACK_ARRAY_LENGTH | ( |
obj
|
) | ((( gos_msgpack_object_array_t *)obj)->count) |
Return the number of entries in an array
- Examples:
- network/http_server_stream/main.c .
◆ MSGPACK_ARRAY_STR
| #define MSGPACK_ARRAY_STR | ( |
obj,
|
|
index
|
|||
| ) | ( gos_msgpack_object_str_t *) MSGPACK_ARRAY_TYPE (obj, index, STR) |
Get MessagePack array at index with a STR type, return NULL if the entry is found but the wrong type
- Examples:
- network/http_server_stream/main.c .
◆ MSGPACK_ARRAY_TYPE
| #define MSGPACK_ARRAY_TYPE | ( |
obj,
|
|
index,
|
|||
type
|
|||
| ) | gos_msgpack_get_array_object (( gos_msgpack_object_array_t *)obj, index, MSGPACK_TYPE_ ## type) |
Get MessagePack array at index with a specific type, return NULL if the entry is found but the wrong type
◆ MSGPACK_ARRAY_UINT
| #define MSGPACK_ARRAY_UINT | ( |
obj,
|
|
index
|
|||
| ) | MSGPACK_ARRAY_TYPE (obj, index, UINT) |
Get MessagePack array at index with a unsigned integer (signed and bool included) type, return NULL if the entry is found but the wrong type
◆ MSGPACK_BIN
| #define MSGPACK_BIN | ( |
obj,
|
|
mem,
|
|||
max_length
|
|||
| ) | memcpy(mem, MSGPACK_BIN_VALUE (obj), MIN (max_length, MSGPACK_BIN_LENGTH (obj))) |
Copy BIN obj contents to buffer
- Examples:
- demo/secure_element/commands.c .
◆ MSGPACK_BIN_CMP
| #define MSGPACK_BIN_CMP | ( |
obj,
|
|
mem
|
|||
| ) | memcmp( MSGPACK_BIN_VALUE (obj), mem, MSGPACK_BIN_LENGTH (obj)) |
Compare binary MessagePack object to another binary value
◆ MSGPACK_BIN_LENGTH
| #define MSGPACK_BIN_LENGTH | ( |
obj
|
) | ((const gos_msgpack_object_bin_t *)(obj))->length |
Get binary MessagePack object's length
◆ MSGPACK_BIN_VALUE
| #define MSGPACK_BIN_VALUE | ( |
obj
|
) | ((const gos_msgpack_object_bin_t *)(obj))->data |
Get binary MessagePack object's value
◆ MSGPACK_BOOL
| #define MSGPACK_BOOL | ( |
obj
|
) | _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object8_t , boolean) |
Get MessagePack object as boolean
- Examples:
- utility/msgpack/read_write_buffer.c , and utility/msgpack/read_write_stream.c .
◆ MSGPACK_BUFFER_REMAINING
| #define MSGPACK_BUFFER_REMAINING | ( |
ctx
|
) | (uint16_t)((ctx)->buffer.end - (ctx)->buffer.ptr) |
Return the number of data buffer bytes unused (i.e. available) by a gos_msgpack_context_t
- Parameters
-
ctxgos_msgpack_context_t initialized with a data buffer
◆ MSGPACK_BUFFER_USED
| #define MSGPACK_BUFFER_USED | ( |
ctx
|
) | (uint16_t)((ctx)->buffer.ptr - (ctx)->buffer.buffer) |
Return the number of data buffer bytes currently used by a gos_msgpack_context_t
- Parameters
-
ctxgos_msgpack_context_t initialized with a data buffer
◆ MSGPACK_DICT
| #define MSGPACK_DICT | ( |
obj,
|
|
key
|
|||
| ) | gos_msgpack_get_dict_object (( gos_msgpack_object_dict_t *)obj, key, MSGPACK_TYPE_ANY ) |
Get MessagePack object with specific key in dictionary (aka map)
- Examples:
- demo/3d_demo/main.c , and demo/accelerometer_stream/main.c .
◆ MSGPACK_DICT_ARRAY
| #define MSGPACK_DICT_ARRAY | ( |
obj,
|
|
key
|
|||
| ) | ( gos_msgpack_object_array_t *) MSGPACK_DICT_TYPE (obj, key, ARRAY) |
Get MessagePack dictionary entry with a ARRAY type, return NULL if the entry is found but the wrong type
◆ MSGPACK_DICT_BIN
| #define MSGPACK_DICT_BIN | ( |
obj,
|
|
key
|
|||
| ) | ( gos_msgpack_object_bin_t *) MSGPACK_DICT_TYPE (obj, key, BIN) |
Get MessagePack dictionary entry with a BIN type, return NULL if the entry is found but the wrong type
- Examples:
- demo/secure_element/commands.c .
◆ MSGPACK_DICT_DICT
| #define MSGPACK_DICT_DICT | ( |
obj,
|
|
key
|
|||
| ) | ( gos_msgpack_object_dict_t *) MSGPACK_DICT_TYPE (obj, key, DICT) |
Get MessagePack dictionary entry with a DICT type, return NULL if the entry is found but the wrong type
- Examples:
- hurricane/security_camera/camera.c , and hurricane/security_camera/main.c .
◆ MSGPACK_DICT_GET_OBJECT
| #define MSGPACK_DICT_GET_OBJECT | ( |
dict,
|
|
key
|
|||
| ) | gos_msgpack_get_dict_object ((const gos_msgpack_object_dict_t *)dict, key, MSGPACK_TYPE_ANY ) |
Return an object for the corresponding key in a dictionary
- See also
- gos_msgpack_get_dict_object for more info
- Examples:
- utility/msgpack/read_write_buffer.c , and utility/msgpack/read_write_stream.c .
◆ MSGPACK_DICT_INT
| #define MSGPACK_DICT_INT | ( |
obj,
|
|
key
|
|||
| ) | MSGPACK_DICT_TYPE (obj, key, INT_OR_UINT) |
Get MessagePack dictionary entry with an signed integer (unsigned and bool included) type. Use MSGPACK_DICT_TYPE(obj, key, INT) if you specifically need a signed integer. return NULL if the entry is found but the wrong type
- Examples:
- hurricane/arducam/camera.c , and hurricane/security_camera/camera.c .
◆ MSGPACK_DICT_STR
| #define MSGPACK_DICT_STR | ( |
obj,
|
|
key
|
|||
| ) | ( gos_msgpack_object_str_t *) MSGPACK_DICT_TYPE (obj, key, STR) |
Get MessagePack dictionary entry with a STR type, return NULL if the entry is found but the wrong type
◆ MSGPACK_DICT_TYPE
| #define MSGPACK_DICT_TYPE | ( |
obj,
|
|
key,
|
|||
type
|
|||
| ) | gos_msgpack_get_dict_object (( gos_msgpack_object_dict_t *)obj, key, MSGPACK_TYPE_ ## type) |
Get MessagePack dictionary entry with a specific type, return NULL if the entry is found but the wrong type
◆ MSGPACK_DICT_UINT
| #define MSGPACK_DICT_UINT | ( |
obj,
|
|
key
|
|||
| ) | MSGPACK_DICT_TYPE (obj, key, INT_OR_UINT) |
Get MessagePack dictionary entry with a unsigned integer (signed and bool included) type, Use MSGPACK_DICT_TYPE(obj, key, UINT) if you specifically need an unsigned integer. return NULL if the entry is found but the wrong type
◆ MSGPACK_DOUBLE
| #define MSGPACK_DOUBLE | ( |
obj
|
) | _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object64_t , dbl) |
Get MessagePack object as double
◆ MSGPACK_FALSE
| #define MSGPACK_FALSE 0xC2 |
Raw value of a MessagePack FALSE boolean typed object
◆ MSGPACK_FLOAT
| #define MSGPACK_FLOAT | ( |
obj
|
) | _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object32_t , flt) |
Get MessagePack object as float
◆ MSGPACK_FOREACH
| #define MSGPACK_FOREACH | ( |
dict_or_array,
|
|
callback,
|
|||
arg
|
|||
| ) | gos_msgpack_foreach ((const gos_msgpack_object_t *)dict_or_array, callback, arg, 0) |
Non-recursively iterate the key/value pairs of a dictionary or entries in array
- See also
- gos_msgpack_foreach() for more info
◆ MSGPACK_FOREACH_RECURSIVE
| #define MSGPACK_FOREACH_RECURSIVE | ( |
dict_or_array,
|
|
callback,
|
|||
arg
|
|||
| ) | gos_msgpack_foreach ((const gos_msgpack_object_t *)dict_or_array, callback, arg, UINT32_MAX) |
Recursively iterate the key/value pairs of a dictionary or entries in array
- See also
- gos_msgpack_foreach() for more info
- Examples:
- cloud/dps_demo/main.c , and dms/messages/main.c .
◆ MSGPACK_FREE_OBJECTS
| #define MSGPACK_FREE_OBJECTS | ( |
obj
|
) | gos_msgpack_free_objects (obj) |
De-allocate all objects assoicated with supplied object
- See also
- gos_msgpack_free_objects() for more info
- Examples:
- utility/msgpack/read_write_buffer.c , and utility/msgpack/read_write_stream.c .
◆ MSGPACK_INIT_CONTEXT_WITH_BUFFER
| #define MSGPACK_INIT_CONTEXT_WITH_BUFFER | ( |
context,
|
|
_buf,
|
|||
_len
|
|||
| ) |
Declare and initialize a gos_msgpack_context_t with the supplied buffer
- Parameters
-
contextPointer to gos_msgpack_context_t being initialized _bufData buffer to initialize context with _lenLength of supplied data buffer
◆ MSGPACK_INIT_WITH_BUFFER
| #define MSGPACK_INIT_WITH_BUFFER | ( |
name,
|
|
_buf,
|
|||
_len
|
|||
| ) |
Declare and initialize a gos_msgpack_context_t with the supplied buffer
- Parameters
-
nameThe variable name of gos_msgpack_context_t being declared _bufData buffer to initialize context with _lenLength of supplied data buffer
◆ MSGPACK_INIT_WITH_WRITER
| #define MSGPACK_INIT_WITH_WRITER | ( |
name,
|
|
_writer,
|
|||
_user
|
|||
| ) |
Declare and initialize a gos_msgpack_context_t with the supplied gos_msgpack_writer_t
- Parameters
-
nameThe variable name of gos_msgpack_context_t being declared _writerMessagePack data writer, see gos_msgpack_writer_t _userOptional user argument given to the data writer
- Examples:
- system/core_dump/main.c , and utility/msgpack/read_write_stream.c .
◆ MSGPACK_INT
| #define MSGPACK_INT | ( |
obj
|
) | gos_msgpack_get_int (obj) |
Get MessagePack object as a signed 32bit value
- See also
- gos_gos_msgpack_get_int() for more info
- Examples:
- hurricane/arducam/camera.c , and hurricane/security_camera/camera.c .
◆ MSGPACK_INT16
| #define MSGPACK_INT16 | ( |
obj
|
) | _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object16_t , s) |
Get MessagePack object as signed 16bit
- See also
- MSGPACK_INT() to automatically determine the integer bit size
◆ MSGPACK_INT32
| #define MSGPACK_INT32 | ( |
obj
|
) | _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object32_t , s) |
Get MessagePack object as signed 32bit
- See also
- MSGPACK_INT() to automatically determine the integer bit size
◆ MSGPACK_INT64
| #define MSGPACK_INT64 | ( |
obj
|
) | _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object64_t , s) |
Get MessagePack object as signed 64bit
- See also
- MSGPACK_LONG() to automatically determine the integer bit size
◆ MSGPACK_INT8
| #define MSGPACK_INT8 | ( |
obj
|
) | _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object8_t , s) |
Get MessagePack object as signed 8bit
- See also
- MSGPACK_INT() to automatically determine the integer bit size
◆ MSGPACK_IS_ARRAY
| #define MSGPACK_IS_ARRAY | ( |
obj
|
) | _MSGPACK_IS_(obj, ARRAY) |
Return true if MessagePack object is an array
- Examples:
- utility/msgpack/read_write_buffer.c , and utility/msgpack/read_write_stream.c .
◆ MSGPACK_IS_BIN
| #define MSGPACK_IS_BIN | ( |
obj
|
) | _MSGPACK_IS_(obj, BIN) |
Return true if MessagePack object is a binary string
- Examples:
- utility/msgpack/read_write_buffer.c , and utility/msgpack/read_write_stream.c .
◆ MSGPACK_IS_BOOL
| #define MSGPACK_IS_BOOL | ( |
obj
|
) | _MSGPACK_IS_(obj, BOOL) |
Return true if MessagePack object is a boolean
- Examples:
- utility/msgpack/read_write_buffer.c , and utility/msgpack/read_write_stream.c .
◆ MSGPACK_IS_DICT
| #define MSGPACK_IS_DICT | ( |
obj
|
) | _MSGPACK_IS_(obj, DICT) |
Return true if MessagePack object is a dictionary (aka map)
- Examples:
- utility/msgpack/read_write_buffer.c , and utility/msgpack/read_write_stream.c .
◆ MSGPACK_IS_DOUBLE
| #define MSGPACK_IS_DOUBLE | ( |
obj
|
) | _MSGPACK_IS_(obj, DOUBLE) |
Return true if MessagePack object is a double
◆ MSGPACK_IS_FLOAT
| #define MSGPACK_IS_FLOAT | ( |
obj
|
) | _MSGPACK_IS_(obj, FLOAT) |
Return true if MessagePack object is a float
◆ MSGPACK_IS_INT
| #define MSGPACK_IS_INT | ( |
obj
|
) | gos_msgpack_object_is_type (( gos_msgpack_object_t *)obj, MSGPACK_TYPE_INT ) |
Return true if MessagePack object is an signed integer
◆ MSGPACK_IS_INT16
| #define MSGPACK_IS_INT16 | ( |
obj
|
) | _MSGPACK_IS_(obj, INT16) |
Return true if MessagePack object is a signed 16bit integer
◆ MSGPACK_IS_INT32
| #define MSGPACK_IS_INT32 | ( |
obj
|
) | _MSGPACK_IS_(obj, INT32) |
Return true if MessagePack object is a signed 32bit integer
◆ MSGPACK_IS_INT64
| #define MSGPACK_IS_INT64 | ( |
obj
|
) | _MSGPACK_IS_(obj, INT64) |
Return true if MessagePack object is a signed 64bit integer
◆ MSGPACK_IS_INT8
| #define MSGPACK_IS_INT8 | ( |
obj
|
) | _MSGPACK_IS_(obj, INT8) |
Return true if MessagePack object is a signed 8bit integer
◆ MSGPACK_IS_NIL
| #define MSGPACK_IS_NIL | ( |
obj
|
) | _MSGPACK_IS_(obj, NIL) |
Return true if MessagePack object is a NIL (i.e. NULL value)
◆ MSGPACK_IS_STR
| #define MSGPACK_IS_STR | ( |
obj
|
) | _MSGPACK_IS_(obj, STR) |
Return true if MessagePack object is a string
- Examples:
- utility/msgpack/read_write_buffer.c , and utility/msgpack/read_write_stream.c .
◆ MSGPACK_IS_UINT
| #define MSGPACK_IS_UINT | ( |
obj
|
) | gos_msgpack_object_is_type (( gos_msgpack_object_t *)obj, MSGPACK_TYPE_UINT ) |
Return true if MessagePack object is an unsigned integer
◆ MSGPACK_IS_UINT16
| #define MSGPACK_IS_UINT16 | ( |
obj
|
) | _MSGPACK_IS_(obj, UINT16) |
Return true if MessagePack object is an unsigned 16bit integer
◆ MSGPACK_IS_UINT32
| #define MSGPACK_IS_UINT32 | ( |
obj
|
) | _MSGPACK_IS_(obj, UINT32) |
Return true if MessagePack object is an unsigned 32bit integer
◆ MSGPACK_IS_UINT64
| #define MSGPACK_IS_UINT64 | ( |
obj
|
) | _MSGPACK_IS_(obj, UINT64) |
Return true if MessagePack object is an unsigned 64bit integer
◆ MSGPACK_IS_UINT8
| #define MSGPACK_IS_UINT8 | ( |
obj
|
) | _MSGPACK_IS_(obj, UINT8) |
Return true if MessagePack object is an unsigned 8bit integer
◆ MSGPACK_LONG
| #define MSGPACK_LONG | ( |
obj,
|
|
buffer
|
|||
| ) | gos_msgpack_get_long (obj, buffer) |
Get MessagePack object as a signed 64bit value
- See also
- gos_gos_msgpack_get_int() for more info
◆ MSGPACK_NIL
| #define MSGPACK_NIL 0xC0 |
Raw value of a MessagePack NIL typed object
◆ MSGPACK_SET_WRITER
| #define MSGPACK_SET_WRITER | ( |
context,
|
|
_writer,
|
|||
_user
|
|||
| ) |
Configure the given gos_msgpack_context_t with a gos_msgpack_writer_t
- Parameters
-
contextPointer to previously declared/allocated gos_msgpack_context_t _writerMessagePack data writer, see gos_msgpack_writer_t _userOptional user argument given to the data writer
◆ MSGPACK_STR
| #define MSGPACK_STR | ( |
obj,
|
|
buffer,
|
|||
max_length
|
|||
| ) | gos_msgpack_get_str (( gos_msgpack_object_t *)obj, buffer, max_length) |
Copy STR obj contents to buffer with null-terminator
- See also
- gos_msgpack_get_str() for more info
◆ MSGPACK_STR_CMP
| #define MSGPACK_STR_CMP | ( |
obj,
|
|
str
|
|||
| ) | gos_msgpack_str_cmp (( gos_msgpack_object_t *)obj, str) |
Compare string MessagePack object to another string
◆ MSGPACK_STR_LENGTH
| #define MSGPACK_STR_LENGTH | ( |
obj
|
) | ((const gos_msgpack_object_str_t *)(obj))->length |
Get MessagePack object string length
◆ MSGPACK_STR_VALUE
| #define MSGPACK_STR_VALUE | ( |
obj
|
) | ((const gos_msgpack_object_str_t *)(obj))->data |
Get string MessagePack object's string value
- Note
- The string value is NOT null-terminated
- See also
- MSGPACK_STR()
◆ MSGPACK_TO_STR
| #define MSGPACK_TO_STR | ( |
obj,
|
|
buffer,
|
|||
max_length
|
|||
| ) | gos_msgpack_to_str (( gos_msgpack_object_t *)obj, buffer, max_length) |
Convert an object to a string and add to buffer
- Note
- The buffer must be at least 32 bytes
- Examples:
- cloud/dps_demo/main.c , dms/messages/main.c , and hurricane/security_camera/main.c .
◆ MSGPACK_TRUE
| #define MSGPACK_TRUE 0xC3 |
Raw value of a MessagePack TRUE boolean typed object
◆ MSGPACK_UINT
| #define MSGPACK_UINT | ( |
obj
|
) | gos_msgpack_get_uint (obj) |
Get MessagePack object as an unsigned 32bit value
- See also
- gos_gos_msgpack_get_int() for more info
◆ MSGPACK_UINT16
| #define MSGPACK_UINT16 | ( |
obj
|
) | _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object16_t , u) |
Get MessagePack object as unsigned 16bit
- See also
- MSGPACK_UINT() to automatically determine the integer bit size
◆ MSGPACK_UINT32
| #define MSGPACK_UINT32 | ( |
obj
|
) | _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object32_t , u) |
Get MessagePack object as unsigned 32bit
- See also
- MSGPACK_UINT() to automatically determine the integer bit size
◆ MSGPACK_UINT64
| #define MSGPACK_UINT64 | ( |
obj
|
) | _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object64_t , u) |
Get MessagePack object as unsigned 64bit
- See also
- MSGPACK_ULONG() to automatically determine the integer bit size
◆ MSGPACK_UINT8
| #define MSGPACK_UINT8 | ( |
obj
|
) | _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object8_t , u) |
Get MessagePack object as unsigned 8bit
- See also
- MSGPACK_UINT() to automatically determine the integer bit size
◆ MSGPACK_ULONG
| #define MSGPACK_ULONG | ( |
obj,
|
|
buffer
|
|||
| ) | gos_msgpack_get_ulong (obj, buffer) |
Get MessagePack object as an unsigned 64bit value
- See also
- gos_gos_msgpack_get_int() for more info
- Examples:
- utility/msgpack/read_write_buffer.c , and utility/msgpack/read_write_stream.c .