Status Codes

Description

Status codes.

Functions

int32_t sl_status_get_string_n (sl_status_t status, char *buffer, uint32_t buffer_length)
sl_status_get_string_n()
void sl_status_print (sl_status_t status)
sl_status_print()

Macros

#define SL_STATUS_SPACE_MASK ((sl_status_t)0xFF00)
#define SL_STATUS_GENERIC_SPACE ((sl_status_t)0x0000)
#define SL_STATUS_PLATFORM_1_SPACE ((sl_status_t)0x0100)
#define SL_STATUS_PLATFORM_2_SPACE ((sl_status_t)0x0200)
#define SL_STATUS_HARDWARE_SPACE ((sl_status_t)0x0300)
#define SL_STATUS_BLUETOOTH_SPACE ((sl_status_t)0x0400)
#define SL_STATUS_BLUETOOTH_MESH_SPACE ((sl_status_t)0x0500)
#define SL_STATUS_CAN_CANOPEN_SPACE ((sl_status_t)0x0600)
#define SL_STATUS_CONNECT_SPACE ((sl_status_t)0x0700)
#define SL_STATUS_NET_SUITE_SPACE ((sl_status_t)0x0800)
#define SL_STATUS_THREAD_SPACE ((sl_status_t)0x0900)
#define SL_STATUS_USB_SPACE ((sl_status_t)0x0A00)
#define SL_STATUS_WIFI_SPACE ((sl_status_t)0x0B00)
#define SL_STATUS_ZIGBEE_SPACE ((sl_status_t)0x0C00)
#define SL_STATUS_Z_WAVE_SPACE ((sl_status_t)0x0D00)
#define SL_STATUS_GECKO_OS_1_SPACE ((sl_status_t)0x0E00)
#define SL_STATUS_GECKO_OS_2_SPACE ((sl_status_t)0x0F00)
#define SL_STATUS_BLUETOOTH_CTRL_SPACE ((sl_status_t)0x1000)
#define SL_STATUS_BLUETOOTH_ATT_SPACE ((sl_status_t)0x1100)
#define SL_STATUS_BLUETOOTH_SMP_SPACE ((sl_status_t)0x1200)
#define SL_STATUS_BLUETOOTH_MESH_FOUNDATION_SPACE ((sl_status_t)0x1300)
#define SL_STATUS_WISUN_SPACE ((sl_status_t)0x1400)
#define SL_STATUS_OK ((sl_status_t)0x0000)
No error.
#define SL_STATUS_FAIL ((sl_status_t)0x0001)
Generic error.
#define SL_STATUS_INVALID_STATE ((sl_status_t)0x0002)
Generic invalid state error.
#define SL_STATUS_NOT_READY ((sl_status_t)0x0003)
Module is not ready for requested operation.
#define SL_STATUS_BUSY ((sl_status_t)0x0004)
Module is busy and cannot carry out requested operation.
#define SL_STATUS_IN_PROGRESS ((sl_status_t)0x0005)
Operation is in progress and not yet complete (pass or fail).
#define SL_STATUS_ABORT ((sl_status_t)0x0006)
Operation aborted.
#define SL_STATUS_TIMEOUT ((sl_status_t)0x0007)
Operation timed out.
#define SL_STATUS_PERMISSION ((sl_status_t)0x0008)
Operation not allowed per permissions.
#define SL_STATUS_WOULD_BLOCK ((sl_status_t)0x0009)
Non-blocking operation would block.
#define SL_STATUS_IDLE ((sl_status_t)0x000A)
Operation/module is Idle, cannot carry requested operation.
#define SL_STATUS_IS_WAITING ((sl_status_t)0x000B)
Operation cannot be done while construct is waiting.
#define SL_STATUS_NONE_WAITING ((sl_status_t)0x000C)
No task/construct waiting/pending for that action/event.
#define SL_STATUS_SUSPENDED ((sl_status_t)0x000D)
Operation cannot be done while construct is suspended.
#define SL_STATUS_NOT_AVAILABLE ((sl_status_t)0x000E)
Feature not available due to software configuration.
#define SL_STATUS_NOT_SUPPORTED ((sl_status_t)0x000F)
Feature not supported.
#define SL_STATUS_INITIALIZATION ((sl_status_t)0x0010)
Initialization failed.
#define SL_STATUS_NOT_INITIALIZED ((sl_status_t)0x0011)
Module has not been initialized.
#define SL_STATUS_ALREADY_INITIALIZED ((sl_status_t)0x0012)
Module has already been initialized.
#define SL_STATUS_DELETED ((sl_status_t)0x0013)
Object/construct has been deleted.
#define SL_STATUS_ISR ((sl_status_t)0x0014)
Illegal call from ISR.
#define SL_STATUS_NETWORK_UP ((sl_status_t)0x0015)
Illegal call because network is up.
#define SL_STATUS_NETWORK_DOWN ((sl_status_t)0x0016)
Illegal call because network is down.
#define SL_STATUS_NOT_JOINED ((sl_status_t)0x0017)
Failure due to not being joined in a network.
#define SL_STATUS_NO_BEACONS ((sl_status_t)0x0018)
Invalid operation as there are no beacons.
#define SL_STATUS_ALLOCATION_FAILED ((sl_status_t)0x0019)
Generic allocation error.
#define SL_STATUS_NO_MORE_RESOURCE ((sl_status_t)0x001A)
No more resource available to perform the operation.
#define SL_STATUS_EMPTY ((sl_status_t)0x001B)
Item/list/queue is empty.
#define SL_STATUS_FULL ((sl_status_t)0x001C)
Item/list/queue is full.
#define SL_STATUS_WOULD_OVERFLOW ((sl_status_t)0x001D)
Item would overflow.
#define SL_STATUS_HAS_OVERFLOWED ((sl_status_t)0x001E)
Item/list/queue has been overflowed.
#define SL_STATUS_OWNERSHIP ((sl_status_t)0x001F)
Generic ownership error.
#define SL_STATUS_IS_OWNER ((sl_status_t)0x0020)
Already/still owning resource.
#define SL_STATUS_INVALID_PARAMETER ((sl_status_t)0x0021)
Generic invalid argument or consequence of invalid argument.
#define SL_STATUS_NULL_POINTER ((sl_status_t)0x0022)
Invalid null pointer received as argument.
#define SL_STATUS_INVALID_CONFIGURATION ((sl_status_t)0x0023)
Invalid configuration provided.
#define SL_STATUS_INVALID_MODE ((sl_status_t)0x0024)
Invalid mode.
#define SL_STATUS_INVALID_HANDLE ((sl_status_t)0x0025)
Invalid handle.
#define SL_STATUS_INVALID_TYPE ((sl_status_t)0x0026)
Invalid type for operation.
#define SL_STATUS_INVALID_INDEX ((sl_status_t)0x0027)
Invalid index.
#define SL_STATUS_INVALID_RANGE ((sl_status_t)0x0028)
Invalid range.
#define SL_STATUS_INVALID_KEY ((sl_status_t)0x0029)
Invalid key.
#define SL_STATUS_INVALID_CREDENTIALS ((sl_status_t)0x002A)
Invalid credentials.
#define SL_STATUS_INVALID_COUNT ((sl_status_t)0x002B)
Invalid count.
#define SL_STATUS_INVALID_SIGNATURE ((sl_status_t)0x002C)
Invalid signature / verification failed.
#define SL_STATUS_NOT_FOUND ((sl_status_t)0x002D)
Item could not be found.
#define SL_STATUS_ALREADY_EXISTS ((sl_status_t)0x002E)
Item already exists.
#define SL_STATUS_IO ((sl_status_t)0x002F)
Generic I/O failure.
#define SL_STATUS_IO_TIMEOUT ((sl_status_t)0x0030)
I/O failure due to timeout.
#define SL_STATUS_TRANSMIT ((sl_status_t)0x0031)
Generic transmission error.
#define SL_STATUS_TRANSMIT_UNDERFLOW ((sl_status_t)0x0032)
Transmit underflowed.
#define SL_STATUS_TRANSMIT_INCOMPLETE ((sl_status_t)0x0033)
Transmit is incomplete.
#define SL_STATUS_TRANSMIT_BUSY ((sl_status_t)0x0034)
Transmit is busy.
#define SL_STATUS_RECEIVE ((sl_status_t)0x0035)
Generic reception error.
#define SL_STATUS_OBJECT_READ ((sl_status_t)0x0036)
Failed to read on/via given object.
#define SL_STATUS_OBJECT_WRITE ((sl_status_t)0x0037)
Failed to write on/via given object.
#define SL_STATUS_MESSAGE_TOO_LONG ((sl_status_t)0x0038)
Message is too long.
#define SL_STATUS_EEPROM_MFG_VERSION_MISMATCH ((sl_status_t)0x0039)
#define SL_STATUS_EEPROM_STACK_VERSION_MISMATCH ((sl_status_t)0x003A)
#define SL_STATUS_FLASH_WRITE_INHIBITED ((sl_status_t)0x003B)
Flash write is inhibited.
#define SL_STATUS_FLASH_VERIFY_FAILED ((sl_status_t)0x003C)
Flash verification failed.
#define SL_STATUS_FLASH_PROGRAM_FAILED ((sl_status_t)0x003D)
Flash programming failed.
#define SL_STATUS_FLASH_ERASE_FAILED ((sl_status_t)0x003E)
Flash erase failed.
#define SL_STATUS_MAC_NO_DATA ((sl_status_t)0x003F)
#define SL_STATUS_MAC_NO_ACK_RECEIVED ((sl_status_t)0x0040)
#define SL_STATUS_MAC_INDIRECT_TIMEOUT ((sl_status_t)0x0041)
#define SL_STATUS_MAC_UNKNOWN_HEADER_TYPE ((sl_status_t)0x0042)
#define SL_STATUS_MAC_ACK_HEADER_TYPE ((sl_status_t)0x0043)
#define SL_STATUS_MAC_COMMAND_TRANSMIT_FAILURE ((sl_status_t)0x0044)
#define SL_STATUS_CLI_STORAGE_NVM_OPEN_ERROR ((sl_status_t)0x0045)
Error in open NVM.
#define SL_STATUS_SECURITY_IMAGE_CHECKSUM_ERROR ((sl_status_t)0x0046)
Image checksum is not valid.
#define SL_STATUS_SECURITY_DECRYPT_ERROR ((sl_status_t)0x0047)
Decryption failed.
#define SL_STATUS_COMMAND_IS_INVALID ((sl_status_t)0x0048)
Command was not recognized.
#define SL_STATUS_COMMAND_TOO_LONG ((sl_status_t)0x0049)
Command or parameter maximum length exceeded.
#define SL_STATUS_COMMAND_INCOMPLETE ((sl_status_t)0x004A)
Data received does not form a complete command.
#define SL_STATUS_BUS_ERROR ((sl_status_t)0x004B)
Bus error, e.g. invalid DMA address.
#define SL_STATUS_CCA_FAILURE ((sl_status_t)0x004C)
#define SL_STATUS_MAC_SCANNING ((sl_status_t)0x004D)
#define SL_STATUS_MAC_INCORRECT_SCAN_TYPE ((sl_status_t)0x004E)
#define SL_STATUS_INVALID_CHANNEL_MASK ((sl_status_t)0x004F)
#define SL_STATUS_BAD_SCAN_DURATION ((sl_status_t)0x0050)
#define SL_STATUS_BT_OUT_OF_BONDS ((sl_status_t)0x0402)
Bonding procedure can't be started because device has no space left for bond.
#define SL_STATUS_BT_UNSPECIFIED ((sl_status_t)0x0403)
Unspecified error.
#define SL_STATUS_BT_HARDWARE ((sl_status_t)0x0404)
Hardware failure.
#define SL_STATUS_BT_NO_BONDING ((sl_status_t)0x0406)
The bonding does not exist.
#define SL_STATUS_BT_CRYPTO ((sl_status_t)0x0407)
Error using crypto functions.
#define SL_STATUS_BT_DATA_CORRUPTED ((sl_status_t)0x0408)
Data was corrupted.
#define SL_STATUS_BT_INVALID_SYNC_HANDLE ((sl_status_t)0x040A)
Invalid periodic advertising sync handle.
#define SL_STATUS_BT_INVALID_MODULE_ACTION ((sl_status_t)0x040B)
Bluetooth cannot be used on this hardware.
#define SL_STATUS_BT_RADIO ((sl_status_t)0x040C)
Error received from radio.
#define SL_STATUS_BT_L2CAP_REMOTE_DISCONNECTED ((sl_status_t)0x040D)
Returned when remote disconnects the connection-oriented channel by sending disconnection request.
#define SL_STATUS_BT_L2CAP_LOCAL_DISCONNECTED ((sl_status_t)0x040E)
Returned when local host disconnect the connection-oriented channel by sending disconnection request.
#define SL_STATUS_BT_L2CAP_CID_NOT_EXIST ((sl_status_t)0x040F)
Returned when local host did not find a connection-oriented channel with given destination CID.
#define SL_STATUS_BT_L2CAP_LE_DISCONNECTED ((sl_status_t)0x0410)
Returned when connection-oriented channel disconnected due to LE connection is dropped.
#define SL_STATUS_BT_L2CAP_FLOW_CONTROL_VIOLATED ((sl_status_t)0x0412)
Returned when connection-oriented channel disconnected due to remote end send data even without credit.
#define SL_STATUS_BT_L2CAP_FLOW_CONTROL_CREDIT_OVERFLOWED ((sl_status_t)0x0413)
Returned when connection-oriented channel disconnected due to remote end send flow control credits exceed 65535.
#define SL_STATUS_BT_L2CAP_NO_FLOW_CONTROL_CREDIT ((sl_status_t)0x0414)
Returned when connection-oriented channel has run out of flow control credit and local application still trying to send data.
#define SL_STATUS_BT_L2CAP_CONNECTION_REQUEST_TIMEOUT ((sl_status_t)0x0415)
Returned when connection-oriented channel has not received connection response message within maximum timeout.
#define SL_STATUS_BT_L2CAP_INVALID_CID ((sl_status_t)0x0416)
Returned when local host received a connection-oriented channel connection response with an invalid destination CID.
#define SL_STATUS_BT_L2CAP_WRONG_STATE ((sl_status_t)0x0417)
Returned when local host application tries to send a command which is not suitable for L2CAP channel's current state.
#define SL_STATUS_BT_PS_STORE_FULL ((sl_status_t)0x041B)
Flash reserved for PS store is full.
#define SL_STATUS_BT_PS_KEY_NOT_FOUND ((sl_status_t)0x041C)
PS key not found.
#define SL_STATUS_BT_APPLICATION_MISMATCHED_OR_INSUFFICIENT_SECURITY ((sl_status_t)0x041D)
Mismatched or insufficient security level.
#define SL_STATUS_BT_APPLICATION_ENCRYPTION_DECRYPTION_ERROR ((sl_status_t)0x041E)
Encrypion/decryption operation failed.
#define SL_STATUS_BT_CTRL_UNKNOWN_CONNECTION_IDENTIFIER ((sl_status_t)0x1002)
Connection does not exist, or connection open request was cancelled.
#define SL_STATUS_BT_CTRL_AUTHENTICATION_FAILURE ((sl_status_t)0x1005)
Pairing or authentication failed due to incorrect results in the pairing or authentication procedure. This could be due to an incorrect PIN or Link Key.
#define SL_STATUS_BT_CTRL_PIN_OR_KEY_MISSING ((sl_status_t)0x1006)
Pairing failed because of missing PIN, or authentication failed because of missing Key.
#define SL_STATUS_BT_CTRL_MEMORY_CAPACITY_EXCEEDED ((sl_status_t)0x1007)
Controller is out of memory.
#define SL_STATUS_BT_CTRL_CONNECTION_TIMEOUT ((sl_status_t)0x1008)
Link supervision timeout has expired.
#define SL_STATUS_BT_CTRL_CONNECTION_LIMIT_EXCEEDED ((sl_status_t)0x1009)
Controller is at limit of connections it can support.
#define SL_STATUS_BT_CTRL_SYNCHRONOUS_CONNECTIONTION_LIMIT_EXCEEDED ((sl_status_t)0x100A)
The Synchronous Connection Limit to a Device Exceeded error code indicates that the Controller has reached the limit to the number of synchronous connections that can be achieved to a device.
#define SL_STATUS_BT_CTRL_ACL_CONNECTION_ALREADY_EXISTS ((sl_status_t)0x100B)
The ACL Connection Already Exists error code indicates that an attempt to create a new ACL Connection to a device when there is already a connection to this device.
#define SL_STATUS_BT_CTRL_COMMAND_DISALLOWED ((sl_status_t)0x100C)
Command requested cannot be executed because the Controller is in a state where it cannot process this command at this time.
#define SL_STATUS_BT_CTRL_CONNECTION_REJECTED_DUE_TO_LIMITED_RESOURCES ((sl_status_t)0x100D)
The Connection Rejected Due To Limited Resources error code indicates that an incoming connection was rejected due to limited resources.
#define SL_STATUS_BT_CTRL_CONNECTION_REJECTED_DUE_TO_SECURITY_REASONS ((sl_status_t)0x100E)
The Connection Rejected Due To Security Reasons error code indicates that a connection was rejected due to security requirements not being fulfilled, like authentication or pairing.
#define SL_STATUS_BT_CTRL_CONNECTION_REJECTED_DUE_TO_UNACCEPTABLE_BD_ADDR ((sl_status_t)0x100F)
The Connection was rejected because this device does not accept the BD_ADDR. This may be because the device will only accept connections from specific BD_ADDRs.
#define SL_STATUS_BT_CTRL_CONNECTION_ACCEPT_TIMEOUT_EXCEEDED ((sl_status_t)0x1010)
The Connection Accept Timeout has been exceeded for this connection attempt.
#define SL_STATUS_BT_CTRL_UNSUPPORTED_FEATURE_OR_PARAMETER_VALUE ((sl_status_t)0x1011)
A feature or parameter value in the HCI command is not supported.
#define SL_STATUS_BT_CTRL_INVALID_COMMAND_PARAMETERS ((sl_status_t)0x1012)
Command contained invalid parameters.
#define SL_STATUS_BT_CTRL_REMOTE_USER_TERMINATED ((sl_status_t)0x1013)
User on the remote device terminated the connection.
#define SL_STATUS_BT_CTRL_REMOTE_DEVICE_TERMINATED_CONNECTION_DUE_TO_LOW_RESOURCES ((sl_status_t)0x1014)
The remote device terminated the connection because of low resources.
#define SL_STATUS_BT_CTRL_REMOTE_POWERING_OFF ((sl_status_t)0x1015)
Remote Device Terminated Connection due to Power Off.
#define SL_STATUS_BT_CTRL_CONNECTION_TERMINATED_BY_LOCAL_HOST ((sl_status_t)0x1016)
Local device terminated the connection.
#define SL_STATUS_BT_CTRL_REPEATED_ATTEMPTS ((sl_status_t)0x1017)
The Controller is disallowing an authentication or pairing procedure because too little time has elapsed since the last authentication or pairing attempt failed.
#define SL_STATUS_BT_CTRL_PAIRING_NOT_ALLOWED ((sl_status_t)0x1018)
The device does not allow pairing. This can be for example, when a device only allows pairing during a certain time window after some user input allows pairing.
#define SL_STATUS_BT_CTRL_UNSUPPORTED_REMOTE_FEATURE ((sl_status_t)0x101A)
The remote device does not support the feature associated with the issued command.
#define SL_STATUS_BT_CTRL_UNSPECIFIED_ERROR ((sl_status_t)0x101F)
No other error code specified is appropriate to use.
#define SL_STATUS_BT_CTRL_LL_RESPONSE_TIMEOUT ((sl_status_t)0x1022)
Connection terminated due to link-layer procedure timeout.
#define SL_STATUS_BT_CTRL_LL_PROCEDURE_COLLISION ((sl_status_t)0x1023)
LL procedure has collided with the same transaction or procedure that is already in progress.
#define SL_STATUS_BT_CTRL_ENCRYPTION_MODE_NOT_ACCEPTABLE ((sl_status_t)0x1025)
The requested encryption mode is not acceptable at this time.
#define SL_STATUS_BT_CTRL_LINK_KEY_CANNOT_BE_CHANGED ((sl_status_t)0x1026)
Link key cannot be changed because a fixed unit key is being used.
#define SL_STATUS_BT_CTRL_INSTANT_PASSED ((sl_status_t)0x1028)
LMP PDU or LL PDU that includes an instant cannot be performed because the instant when this would have occurred has passed.
#define SL_STATUS_BT_CTRL_PAIRING_WITH_UNIT_KEY_NOT_SUPPORTED ((sl_status_t)0x1029)
It was not possible to pair as a unit key was requested and it is not supported.
#define SL_STATUS_BT_CTRL_DIFFERENT_TRANSACTION_COLLISION ((sl_status_t)0x102A)
LMP transaction was started that collides with an ongoing transaction.
#define SL_STATUS_BT_CTRL_CHANNEL_ASSESSMENT_NOT_SUPPORTED ((sl_status_t)0x102E)
The Controller cannot perform channel assessment because it is not supported.
#define SL_STATUS_BT_CTRL_INSUFFICIENT_SECURITY ((sl_status_t)0x102F)
The HCI command or LMP PDU sent is only possible on an encrypted link.
#define SL_STATUS_BT_CTRL_PARAMETER_OUT_OF_MANDATORY_RANGE ((sl_status_t)0x1030)
A parameter value requested is outside the mandatory range of parameters for the given HCI command or LMP PDU.
#define SL_STATUS_BT_CTRL_SIMPLE_PAIRING_NOT_SUPPORTED_BY_HOST ((sl_status_t)0x1037)
The IO capabilities request or response was rejected because the sending Host does not support Secure Simple Pairing even though the receiving Link Manager does.
#define SL_STATUS_BT_CTRL_HOST_BUSY_PAIRING ((sl_status_t)0x1038)
The Host is busy with another pairing operation and unable to support the requested pairing. The receiving device should retry pairing again later.
#define SL_STATUS_BT_CTRL_CONNECTION_REJECTED_DUE_TO_NO_SUITABLE_CHANNEL_FOUND ((sl_status_t)0x1039)
The Controller could not calculate an appropriate value for the Channel selection operation.
#define SL_STATUS_BT_CTRL_CONTROLLER_BUSY ((sl_status_t)0x103A)
Operation was rejected because the controller is busy and unable to process the request.
#define SL_STATUS_BT_CTRL_UNACCEPTABLE_CONNECTION_INTERVAL ((sl_status_t)0x103B)
Remote device terminated the connection because of an unacceptable connection interval.
#define SL_STATUS_BT_CTRL_ADVERTISING_TIMEOUT ((sl_status_t)0x103C)
Ddvertising for a fixed duration completed or, for directed advertising, that advertising completed without a connection being created.
#define SL_STATUS_BT_CTRL_CONNECTION_TERMINATED_DUE_TO_MIC_FAILURE ((sl_status_t)0x103D)
Connection was terminated because the Message Integrity Check (MIC) failed on a received packet.
#define SL_STATUS_BT_CTRL_CONNECTION_FAILED_TO_BE_ESTABLISHED ((sl_status_t)0x103E)
LL initiated a connection but the connection has failed to be established. Controller did not receive any packets from remote end.
#define SL_STATUS_BT_CTRL_MAC_CONNECTION_FAILED ((sl_status_t)0x103F)
The MAC of the 802.11 AMP was requested to connect to a peer, but the connection failed.
#define SL_STATUS_BT_CTRL_COARSE_CLOCK_ADJUSTMENT_REJECTED_BUT_WILL_TRY_TO_ADJUST_USING_CLOCK_DRAGGING ((sl_status_t)0x1040)
The master, at this time, is unable to make a coarse adjustment to the piconet clock, using the supplied parameters. Instead the master will attempt to move the clock using clock dragging.
#define SL_STATUS_BT_CTRL_UNKNOWN_ADVERTISING_IDENTIFIER ((sl_status_t)0x1042)
A command was sent from the Host that should identify an Advertising or Sync handle, but the Advertising or Sync handle does not exist.
#define SL_STATUS_BT_CTRL_LIMIT_REACHED ((sl_status_t)0x1043)
Number of operations requested has been reached and has indicated the completion of the activity (e.g., advertising or scanning).
#define SL_STATUS_BT_CTRL_OPERATION_CANCELLED_BY_HOST ((sl_status_t)0x1044)
A request to the Controller issued by the Host and still pending was successfully canceled.
#define SL_STATUS_BT_CTRL_PACKET_TOO_LONG ((sl_status_t)0x1045)
An attempt was made to send or receive a packet that exceeds the maximum allowed packet l.
#define SL_STATUS_BT_ATT_INVALID_HANDLE ((sl_status_t)0x1101)
The attribute handle given was not valid on this server.
#define SL_STATUS_BT_ATT_READ_NOT_PERMITTED ((sl_status_t)0x1102)
The attribute cannot be read.
#define SL_STATUS_BT_ATT_WRITE_NOT_PERMITTED ((sl_status_t)0x1103)
The attribute cannot be written.
#define SL_STATUS_BT_ATT_INVALID_PDU ((sl_status_t)0x1104)
The attribute PDU was invalid.
#define SL_STATUS_BT_ATT_INSUFFICIENT_AUTHENTICATION ((sl_status_t)0x1105)
The attribute requires authentication before it can be read or written.
#define SL_STATUS_BT_ATT_REQUEST_NOT_SUPPORTED ((sl_status_t)0x1106)
Attribute Server does not support the request received from the client.
#define SL_STATUS_BT_ATT_INVALID_OFFSET ((sl_status_t)0x1107)
Offset specified was past the end of the attribute.
#define SL_STATUS_BT_ATT_INSUFFICIENT_AUTHORIZATION ((sl_status_t)0x1108)
The attribute requires authorization before it can be read or written.
#define SL_STATUS_BT_ATT_PREPARE_QUEUE_FULL ((sl_status_t)0x1109)
Too many prepare writes have been queueud.
#define SL_STATUS_BT_ATT_ATT_NOT_FOUND ((sl_status_t)0x110A)
No attribute found within the given attribute handle range.
#define SL_STATUS_BT_ATT_ATT_NOT_LONG ((sl_status_t)0x110B)
The attribute cannot be read or written using the Read Blob Request.
#define SL_STATUS_BT_ATT_INSUFFICIENT_ENC_KEY_SIZE ((sl_status_t)0x110C)
The Encryption Key Size used for encrypting this link is insufficient.
#define SL_STATUS_BT_ATT_INVALID_ATT_LENGTH ((sl_status_t)0x110D)
The attribute value length is invalid for the operation.
#define SL_STATUS_BT_ATT_UNLIKELY_ERROR ((sl_status_t)0x110E)
The attribute request that was requested has encountered an error that was unlikely, and therefore could not be completed as requested.
#define SL_STATUS_BT_ATT_INSUFFICIENT_ENCRYPTION ((sl_status_t)0x110F)
The attribute requires encryption before it can be read or written.
#define SL_STATUS_BT_ATT_UNSUPPORTED_GROUP_TYPE ((sl_status_t)0x1110)
The attribute type is not a supported grouping attribute as defined by a higher layer specification.
#define SL_STATUS_BT_ATT_INSUFFICIENT_RESOURCES ((sl_status_t)0x1111)
Insufficient Resources to complete the request.
#define SL_STATUS_BT_ATT_OUT_OF_SYNC ((sl_status_t)0x1112)
The server requests the client to rediscover the database.
#define SL_STATUS_BT_ATT_VALUE_NOT_ALLOWED ((sl_status_t)0x1113)
The attribute parameter value was not allowed.
#define SL_STATUS_BT_ATT_APPLICATION ((sl_status_t)0x1180)
When this is returned in a BGAPI response, the application tried to read or write the value of a user attribute from the GATT databa.
#define SL_STATUS_BT_ATT_WRITE_REQUEST_REJECTED ((sl_status_t)0x11FC)
The requested write operation cannot be fulfilled for reasons other than permissions.
#define SL_STATUS_BT_ATT_CLIENT_CHARACTERISTIC_CONFIGURATION_DESCRIPTOR_IMPROPERLY_CONFIGURED ((sl_status_t)0x11FD)
The Client Characteristic Configuration descriptor is not configured according to the requirements of the profile or service.
#define SL_STATUS_BT_ATT_PROCEDURE_ALREADY_IN_PROGRESS ((sl_status_t)0x11FE)
The profile or service request cannot be serviced because an operation that has been previously triggered is still in progress.
#define SL_STATUS_BT_ATT_OUT_OF_RANGE ((sl_status_t)0x11FF)
The attribute value is out of range as defined by a profile or service specification.
#define SL_STATUS_BT_SMP_PASSKEY_ENTRY_FAILED ((sl_status_t)0x1201)
The user input of passkey failed, for example, the user cancelled the operation.
#define SL_STATUS_BT_SMP_OOB_NOT_AVAILABLE ((sl_status_t)0x1202)
Out of Band data is not available for authentication.
#define SL_STATUS_BT_SMP_AUTHENTICATION_REQUIREMENTS ((sl_status_t)0x1203)
The pairing procedure cannot be performed as authentication requirements cannot be met due to IO capabilities of one or both devices.
#define SL_STATUS_BT_SMP_CONFIRM_VALUE_FAILED ((sl_status_t)0x1204)
The confirm value does not match the calculated compare value.
#define SL_STATUS_BT_SMP_PAIRING_NOT_SUPPORTED ((sl_status_t)0x1205)
Pairing is not supported by the device.
#define SL_STATUS_BT_SMP_ENCRYPTION_KEY_SIZE ((sl_status_t)0x1206)
The resultant encryption key size is insufficient for the security requirements of this device.
#define SL_STATUS_BT_SMP_COMMAND_NOT_SUPPORTED ((sl_status_t)0x1207)
The SMP command received is not supported on this device.
#define SL_STATUS_BT_SMP_UNSPECIFIED_REASON ((sl_status_t)0x1208)
Pairing failed due to an unspecified reason.
#define SL_STATUS_BT_SMP_REPEATED_ATTEMPTS ((sl_status_t)0x1209)
Pairing or authentication procedure is disallowed because too little time has elapsed since last pairing request or security request.
#define SL_STATUS_BT_SMP_INVALID_PARAMETERS ((sl_status_t)0x120A)
The Invalid Parameters error code indicates: the command length is invalid or a parameter is outside of the specified range.
#define SL_STATUS_BT_SMP_DHKEY_CHECK_FAILED ((sl_status_t)0x120B)
Indicates to the remote device that the DHKey Check value received doesn't match the one calculated by the local device.
#define SL_STATUS_BT_SMP_NUMERIC_COMPARISON_FAILED ((sl_status_t)0x120C)
Indicates that the confirm values in the numeric comparison protocol do not match.
#define SL_STATUS_BT_SMP_BREDR_PAIRING_IN_PROGRESS ((sl_status_t)0x120D)
Indicates that the pairing over the LE transport failed due to a Pairing Request sent over the BR/EDR transport in process.
#define SL_STATUS_BT_SMP_CROSS_TRANSPORT_KEY_DERIVATION_GENERATION_NOT_ALLOWED ((sl_status_t)0x120E)
Indicates that the BR/EDR Link Key generated on the BR/EDR transport cannot be used to derive and distribute keys for the LE transport.
#define SL_STATUS_BT_MESH_ALREADY_EXISTS ((sl_status_t)0x0501)
Returned when trying to add a key or some other unique resource with an ID which already exists.
#define SL_STATUS_BT_MESH_DOES_NOT_EXIST ((sl_status_t)0x0502)
Returned when trying to manipulate a key or some other resource with an ID which does not exist.
#define SL_STATUS_BT_MESH_LIMIT_REACHED ((sl_status_t)0x0503)
Returned when an operation cannot be executed because a pre-configured limit for keys, key bindings, elements, models, virtual addresses, provisioned devices, or provisioning sessions is reached.
#define SL_STATUS_BT_MESH_INVALID_ADDRESS ((sl_status_t)0x0504)
Returned when trying to use a reserved address or add a "pre-provisioned" device using an address already used by some other device.
#define SL_STATUS_BT_MESH_MALFORMED_DATA ((sl_status_t)0x0505)
In a BGAPI response, the user supplied malformed data; in a BGAPI event, the remote end responded with malformed or unrecognized data.
#define SL_STATUS_BT_MESH_ALREADY_INITIALIZED ((sl_status_t)0x0506)
An attempt was made to initialize a subsystem that was already initialized.
#define SL_STATUS_BT_MESH_NOT_INITIALIZED ((sl_status_t)0x0507)
An attempt was made to use a subsystem that wasn't initialized yet. Call the subsystem's init function first.
#define SL_STATUS_BT_MESH_NO_FRIEND_OFFER ((sl_status_t)0x0508)
Returned when trying to establish a friendship as a Low Power Node, but no acceptable friend offer message was received.
#define SL_STATUS_BT_MESH_PROV_LINK_CLOSED ((sl_status_t)0x0509)
Provisioning link was unexpectedly closed before provisioning was complete.
#define SL_STATUS_BT_MESH_PROV_INVALID_PDU ((sl_status_t)0x050A)
An unrecognized provisioning PDU was received.
#define SL_STATUS_BT_MESH_PROV_INVALID_PDU_FORMAT ((sl_status_t)0x050B)
A provisioning PDU with wrong length or containing field values that are out of bounds was received.
#define SL_STATUS_BT_MESH_PROV_UNEXPECTED_PDU ((sl_status_t)0x050C)
An unexpected (out of sequence) provisioning PDU was received.
#define SL_STATUS_BT_MESH_PROV_CONFIRMATION_FAILED ((sl_status_t)0x050D)
The computed confirmation value did not match the expected value.
#define SL_STATUS_BT_MESH_PROV_OUT_OF_RESOURCES ((sl_status_t)0x050E)
Provisioning could not be continued due to insufficient resources.
#define SL_STATUS_BT_MESH_PROV_DECRYPTION_FAILED ((sl_status_t)0x050F)
The provisioning data block could not be decrypted.
#define SL_STATUS_BT_MESH_PROV_UNEXPECTED_ERROR ((sl_status_t)0x0510)
An unexpected error happened during provisioning.
#define SL_STATUS_BT_MESH_PROV_CANNOT_ASSIGN_ADDR ((sl_status_t)0x0511)
Device could not assign unicast addresses to all of its elements.
#define SL_STATUS_BT_MESH_ADDRESS_TEMPORARILY_UNAVAILABLE ((sl_status_t)0x0512)
Returned when trying to reuse an address of a previously deleted device before an IV Index Update has been executed.
#define SL_STATUS_BT_MESH_ADDRESS_ALREADY_USED ((sl_status_t)0x0513)
Returned when trying to assign an address that is used by one of the devices in the Device Database, or by the Provisioner itself.
#define SL_STATUS_BT_MESH_PUBLISH_NOT_CONFIGURED ((sl_status_t)0x0514)
Application key or publish address are not set.
#define SL_STATUS_BT_MESH_APP_KEY_NOT_BOUND ((sl_status_t)0x0515)
Application key is not bound to a model.
#define SL_STATUS_BT_MESH_FOUNDATION_INVALID_ADDRESS ((sl_status_t)0x1301)
Returned when address in request was not valid.
#define SL_STATUS_BT_MESH_FOUNDATION_INVALID_MODEL ((sl_status_t)0x1302)
Returned when model identified is not found for a given element.
#define SL_STATUS_BT_MESH_FOUNDATION_INVALID_APP_KEY ((sl_status_t)0x1303)
Returned when the key identified by AppKeyIndex is not stored in the node.
#define SL_STATUS_BT_MESH_FOUNDATION_INVALID_NET_KEY ((sl_status_t)0x1304)
Returned when the key identified by NetKeyIndex is not stored in the node.
#define SL_STATUS_BT_MESH_FOUNDATION_INSUFFICIENT_RESOURCES ((sl_status_t)0x1305)
Returned when The node cannot serve the request due to insufficient resources.
#define SL_STATUS_BT_MESH_FOUNDATION_KEY_INDEX_EXISTS ((sl_status_t)0x1306)
Returned when the key identified is already stored in the node and the new NetKey value is different.
#define SL_STATUS_BT_MESH_FOUNDATION_INVALID_PUBLISH_PARAMS ((sl_status_t)0x1307)
Returned when the model does not support the publish mechanism.
#define SL_STATUS_BT_MESH_FOUNDATION_NOT_SUBSCRIBE_MODEL ((sl_status_t)0x1308)
Returned when the model does not support the subscribe mechanism.
#define SL_STATUS_BT_MESH_FOUNDATION_STORAGE_FAILURE ((sl_status_t)0x1309)
Returned when storing of the requested parameters failed.
#define SL_STATUS_BT_MESH_FOUNDATION_NOT_SUPPORTED ((sl_status_t)0x130A)
Returned when requested setting is not supported.
#define SL_STATUS_BT_MESH_FOUNDATION_CANNOT_UPDATE ((sl_status_t)0x130B)
Returned when the requested update operation cannot be performed due to general constraints.
#define SL_STATUS_BT_MESH_FOUNDATION_CANNOT_REMOVE ((sl_status_t)0x130C)
Returned when the requested delete operation cannot be performed due to general constraints.
#define SL_STATUS_BT_MESH_FOUNDATION_CANNOT_BIND ((sl_status_t)0x130D)
Returned when the requested bind operation cannot be performed due to general constraints.
#define SL_STATUS_BT_MESH_FOUNDATION_TEMPORARILY_UNABLE ((sl_status_t)0x130E)
Returned when The node cannot start advertising with Node Identity or Proxy since the maximum number of parallel advertising is reached.
#define SL_STATUS_BT_MESH_FOUNDATION_CANNOT_SET ((sl_status_t)0x130F)
Returned when the requested state cannot be set.
#define SL_STATUS_BT_MESH_FOUNDATION_UNSPECIFIED ((sl_status_t)0x1310)
Returned when an unspecified error took place.
#define SL_STATUS_BT_MESH_FOUNDATION_INVALID_BINDING ((sl_status_t)0x1311)
Returned when the NetKeyIndex and AppKeyIndex combination is not valid for a Config AppKey Update.
#define SL_STATUS_WIFI_INVALID_KEY ((sl_status_t)0x0B01)
Invalid firmware keyset.
#define SL_STATUS_WIFI_FIRMWARE_DOWNLOAD_TIMEOUT ((sl_status_t)0x0B02)
The firmware download took too long.
#define SL_STATUS_WIFI_UNSUPPORTED_MESSAGE_ID ((sl_status_t)0x0B03)
Unknown request ID or wrong interface ID used.
#define SL_STATUS_WIFI_WARNING ((sl_status_t)0x0B04)
The request is successful but some parameters have been ignored.
#define SL_STATUS_WIFI_NO_PACKET_TO_RECEIVE ((sl_status_t)0x0B05)
No Packets waiting to be received.
#define SL_STATUS_WIFI_SLEEP_GRANTED ((sl_status_t)0x0B08)
The sleep mode is granted.
#define SL_STATUS_WIFI_SLEEP_NOT_GRANTED ((sl_status_t)0x0B09)
The WFx does not go back to sleep.
#define SL_STATUS_WIFI_SECURE_LINK_MAC_KEY_ERROR ((sl_status_t)0x0B10)
The SecureLink MAC key was not found.
#define SL_STATUS_WIFI_SECURE_LINK_MAC_KEY_ALREADY_BURNED ((sl_status_t)0x0B11)
The SecureLink MAC key is already installed in OTP.
#define SL_STATUS_WIFI_SECURE_LINK_RAM_MODE_NOT_ALLOWED ((sl_status_t)0x0B12)
The SecureLink MAC key cannot be installed in RAM.
#define SL_STATUS_WIFI_SECURE_LINK_FAILED_UNKNOWN_MODE ((sl_status_t)0x0B13)
The SecureLink MAC key installation failed.
#define SL_STATUS_WIFI_SECURE_LINK_EXCHANGE_FAILED ((sl_status_t)0x0B14)
SecureLink key (re)negotiation failed.
#define SL_STATUS_WIFI_WRONG_STATE ((sl_status_t)0x0B18)
The device is in an inappropriate state to perform the request.
#define SL_STATUS_WIFI_CHANNEL_NOT_ALLOWED ((sl_status_t)0x0B19)
The request failed due to regulatory limitations.
#define SL_STATUS_WIFI_NO_MATCHING_AP ((sl_status_t)0x0B1A)
The connection request failed because no suitable AP was found.
#define SL_STATUS_WIFI_CONNECTION_ABORTED ((sl_status_t)0x0B1B)
The connection request was aborted by host.
#define SL_STATUS_WIFI_CONNECTION_TIMEOUT ((sl_status_t)0x0B1C)
The connection request failed because of a timeout.
#define SL_STATUS_WIFI_CONNECTION_REJECTED_BY_AP ((sl_status_t)0x0B1D)
The connection request failed because the AP rejected the device.
#define SL_STATUS_WIFI_CONNECTION_AUTH_FAILURE ((sl_status_t)0x0B1E)
The connection request failed because the WPA handshake did not complete successfully.
#define SL_STATUS_WIFI_RETRY_EXCEEDED ((sl_status_t)0x0B1F)
The request failed because the retry limit was exceeded.
#define SL_STATUS_WIFI_TX_LIFETIME_EXCEEDED ((sl_status_t)0x0B20)
The request failed because the MSDU life time was exceeded.

Typedefs

typedef uint32_t sl_status_t

Function Documentation

◆ sl_status_get_string_n()

int32_t sl_status_get_string_n ( sl_status_t status,
char * buffer,
uint32_t buffer_length
)

sl_status_get_string_n()

Get a copy of the status string associated to the status code passed, up to 'buffer_length' length, if the string associated to the status code is enabled. If not, the error code number, in hex, prefixed by "SL_STATUS_" will be copied in the buffer instead. For example, the buffer would either contain "SL_STATUS_FAIL" if that status string is enabled, or "SL_STATUS_0x0001" if the string is disabled, as SL_STATUS_FAIL's value is 0x0001.

Parameters
status The status code from which to obtain the status string.
buffer Pointer to a buffer in which the status string will be copied. A terminating null-character will be appended after the copied status string.
buffer_length Maximum number of characters that can be written in the buffer, including the terminating null-character. If the status string would be longer than the available length, it will be truncated and a null-terminating character will be the last character contained in the buffer.
Returns
The number of characters that would have been written if the buffer_length had been sufficiently large, not counting the terminating null character. If the status code is invalid, 0 or a negative number is returned. Notice that only when this returned value is strictly positive and less than buffer_length, the status string has been completely written in the buffer.

◆ sl_status_print()

void sl_status_print ( sl_status_t status )

sl_status_print()

Print, through printf, the string associated to the passed status code. If the string associated to the status code is enabled, the status string will be printed, for example "SL_STATUS_OK". If the string associated to the status code is disabled, the status number, in hex, prefixed by "SL_STATUS_" will be printed instead, for example "SL_STATUS_0x0000", as SL_STATUS_OK's value is 0x0000.

Parameters
status The status code of which to print the status string.

Macro Definition Documentation

◆ SL_STATUS_OK

#define SL_STATUS_OK   ((sl_status_t)0x0000)

No error.

◆ SL_STATUS_FAIL

#define SL_STATUS_FAIL   ((sl_status_t)0x0001)

Generic error.

◆ SL_STATUS_INVALID_STATE

#define SL_STATUS_INVALID_STATE   ((sl_status_t)0x0002)

Generic invalid state error.

◆ SL_STATUS_NOT_READY

#define SL_STATUS_NOT_READY   ((sl_status_t)0x0003)

Module is not ready for requested operation.

◆ SL_STATUS_BUSY

#define SL_STATUS_BUSY   ((sl_status_t)0x0004)

Module is busy and cannot carry out requested operation.

◆ SL_STATUS_IN_PROGRESS

#define SL_STATUS_IN_PROGRESS   ((sl_status_t)0x0005)

Operation is in progress and not yet complete (pass or fail).

◆ SL_STATUS_ABORT

#define SL_STATUS_ABORT   ((sl_status_t)0x0006)

Operation aborted.

◆ SL_STATUS_TIMEOUT

#define SL_STATUS_TIMEOUT   ((sl_status_t)0x0007)

Operation timed out.

◆ SL_STATUS_PERMISSION

#define SL_STATUS_PERMISSION   ((sl_status_t)0x0008)

Operation not allowed per permissions.

◆ SL_STATUS_WOULD_BLOCK

#define SL_STATUS_WOULD_BLOCK   ((sl_status_t)0x0009)

Non-blocking operation would block.

◆ SL_STATUS_IDLE

#define SL_STATUS_IDLE   ((sl_status_t)0x000A)

Operation/module is Idle, cannot carry requested operation.

◆ SL_STATUS_IS_WAITING

#define SL_STATUS_IS_WAITING   ((sl_status_t)0x000B)

Operation cannot be done while construct is waiting.

◆ SL_STATUS_NONE_WAITING

#define SL_STATUS_NONE_WAITING   ((sl_status_t)0x000C)

No task/construct waiting/pending for that action/event.

◆ SL_STATUS_SUSPENDED

#define SL_STATUS_SUSPENDED   ((sl_status_t)0x000D)

Operation cannot be done while construct is suspended.

◆ SL_STATUS_NOT_AVAILABLE

#define SL_STATUS_NOT_AVAILABLE   ((sl_status_t)0x000E)

Feature not available due to software configuration.

◆ SL_STATUS_NOT_SUPPORTED

#define SL_STATUS_NOT_SUPPORTED   ((sl_status_t)0x000F)

Feature not supported.

◆ SL_STATUS_INITIALIZATION

#define SL_STATUS_INITIALIZATION   ((sl_status_t)0x0010)

Initialization failed.

◆ SL_STATUS_NOT_INITIALIZED

#define SL_STATUS_NOT_INITIALIZED   ((sl_status_t)0x0011)

Module has not been initialized.

◆ SL_STATUS_ALREADY_INITIALIZED

#define SL_STATUS_ALREADY_INITIALIZED   ((sl_status_t)0x0012)

Module has already been initialized.

◆ SL_STATUS_DELETED

#define SL_STATUS_DELETED   ((sl_status_t)0x0013)

Object/construct has been deleted.

◆ SL_STATUS_ISR

#define SL_STATUS_ISR   ((sl_status_t)0x0014)

Illegal call from ISR.

◆ SL_STATUS_NETWORK_UP

#define SL_STATUS_NETWORK_UP   ((sl_status_t)0x0015)

Illegal call because network is up.

◆ SL_STATUS_NETWORK_DOWN

#define SL_STATUS_NETWORK_DOWN   ((sl_status_t)0x0016)

Illegal call because network is down.

◆ SL_STATUS_NOT_JOINED

#define SL_STATUS_NOT_JOINED   ((sl_status_t)0x0017)

Failure due to not being joined in a network.

◆ SL_STATUS_NO_BEACONS

#define SL_STATUS_NO_BEACONS   ((sl_status_t)0x0018)

Invalid operation as there are no beacons.

◆ SL_STATUS_ALLOCATION_FAILED

#define SL_STATUS_ALLOCATION_FAILED   ((sl_status_t)0x0019)

Generic allocation error.

◆ SL_STATUS_NO_MORE_RESOURCE

#define SL_STATUS_NO_MORE_RESOURCE   ((sl_status_t)0x001A)

No more resource available to perform the operation.

◆ SL_STATUS_EMPTY

#define SL_STATUS_EMPTY   ((sl_status_t)0x001B)

Item/list/queue is empty.

◆ SL_STATUS_FULL

#define SL_STATUS_FULL   ((sl_status_t)0x001C)

Item/list/queue is full.

◆ SL_STATUS_WOULD_OVERFLOW

#define SL_STATUS_WOULD_OVERFLOW   ((sl_status_t)0x001D)

Item would overflow.

◆ SL_STATUS_HAS_OVERFLOWED

#define SL_STATUS_HAS_OVERFLOWED   ((sl_status_t)0x001E)

Item/list/queue has been overflowed.

◆ SL_STATUS_OWNERSHIP

#define SL_STATUS_OWNERSHIP   ((sl_status_t)0x001F)

Generic ownership error.

◆ SL_STATUS_IS_OWNER

#define SL_STATUS_IS_OWNER   ((sl_status_t)0x0020)

Already/still owning resource.

◆ SL_STATUS_INVALID_PARAMETER

#define SL_STATUS_INVALID_PARAMETER   ((sl_status_t)0x0021)

Generic invalid argument or consequence of invalid argument.

◆ SL_STATUS_NULL_POINTER

#define SL_STATUS_NULL_POINTER   ((sl_status_t)0x0022)

Invalid null pointer received as argument.

◆ SL_STATUS_INVALID_CONFIGURATION

#define SL_STATUS_INVALID_CONFIGURATION   ((sl_status_t)0x0023)

Invalid configuration provided.

◆ SL_STATUS_INVALID_MODE

#define SL_STATUS_INVALID_MODE   ((sl_status_t)0x0024)

Invalid mode.

◆ SL_STATUS_INVALID_HANDLE

#define SL_STATUS_INVALID_HANDLE   ((sl_status_t)0x0025)

Invalid handle.

◆ SL_STATUS_INVALID_TYPE

#define SL_STATUS_INVALID_TYPE   ((sl_status_t)0x0026)

Invalid type for operation.

◆ SL_STATUS_INVALID_INDEX

#define SL_STATUS_INVALID_INDEX   ((sl_status_t)0x0027)

Invalid index.

◆ SL_STATUS_INVALID_RANGE

#define SL_STATUS_INVALID_RANGE   ((sl_status_t)0x0028)

Invalid range.

◆ SL_STATUS_INVALID_KEY

#define SL_STATUS_INVALID_KEY   ((sl_status_t)0x0029)

Invalid key.

◆ SL_STATUS_INVALID_CREDENTIALS

#define SL_STATUS_INVALID_CREDENTIALS   ((sl_status_t)0x002A)

Invalid credentials.

◆ SL_STATUS_INVALID_COUNT

#define SL_STATUS_INVALID_COUNT   ((sl_status_t)0x002B)

Invalid count.

◆ SL_STATUS_INVALID_SIGNATURE

#define SL_STATUS_INVALID_SIGNATURE   ((sl_status_t)0x002C)

Invalid signature / verification failed.

◆ SL_STATUS_NOT_FOUND

#define SL_STATUS_NOT_FOUND   ((sl_status_t)0x002D)

Item could not be found.

◆ SL_STATUS_ALREADY_EXISTS

#define SL_STATUS_ALREADY_EXISTS   ((sl_status_t)0x002E)

Item already exists.

◆ SL_STATUS_IO

#define SL_STATUS_IO   ((sl_status_t)0x002F)

Generic I/O failure.

◆ SL_STATUS_IO_TIMEOUT

#define SL_STATUS_IO_TIMEOUT   ((sl_status_t)0x0030)

I/O failure due to timeout.

◆ SL_STATUS_TRANSMIT

#define SL_STATUS_TRANSMIT   ((sl_status_t)0x0031)

Generic transmission error.

◆ SL_STATUS_TRANSMIT_UNDERFLOW

#define SL_STATUS_TRANSMIT_UNDERFLOW   ((sl_status_t)0x0032)

Transmit underflowed.

◆ SL_STATUS_TRANSMIT_INCOMPLETE

#define SL_STATUS_TRANSMIT_INCOMPLETE   ((sl_status_t)0x0033)

Transmit is incomplete.

◆ SL_STATUS_TRANSMIT_BUSY

#define SL_STATUS_TRANSMIT_BUSY   ((sl_status_t)0x0034)

Transmit is busy.

◆ SL_STATUS_RECEIVE

#define SL_STATUS_RECEIVE   ((sl_status_t)0x0035)

Generic reception error.

◆ SL_STATUS_OBJECT_READ

#define SL_STATUS_OBJECT_READ   ((sl_status_t)0x0036)

Failed to read on/via given object.

◆ SL_STATUS_OBJECT_WRITE

#define SL_STATUS_OBJECT_WRITE   ((sl_status_t)0x0037)

Failed to write on/via given object.

◆ SL_STATUS_MESSAGE_TOO_LONG

#define SL_STATUS_MESSAGE_TOO_LONG   ((sl_status_t)0x0038)

Message is too long.

◆ SL_STATUS_FLASH_WRITE_INHIBITED

#define SL_STATUS_FLASH_WRITE_INHIBITED   ((sl_status_t)0x003B)

Flash write is inhibited.

◆ SL_STATUS_FLASH_VERIFY_FAILED

#define SL_STATUS_FLASH_VERIFY_FAILED   ((sl_status_t)0x003C)

Flash verification failed.

◆ SL_STATUS_FLASH_PROGRAM_FAILED

#define SL_STATUS_FLASH_PROGRAM_FAILED   ((sl_status_t)0x003D)

Flash programming failed.

◆ SL_STATUS_FLASH_ERASE_FAILED

#define SL_STATUS_FLASH_ERASE_FAILED   ((sl_status_t)0x003E)

Flash erase failed.

◆ SL_STATUS_CLI_STORAGE_NVM_OPEN_ERROR

#define SL_STATUS_CLI_STORAGE_NVM_OPEN_ERROR   ((sl_status_t)0x0045)

Error in open NVM.

◆ SL_STATUS_SECURITY_IMAGE_CHECKSUM_ERROR

#define SL_STATUS_SECURITY_IMAGE_CHECKSUM_ERROR   ((sl_status_t)0x0046)

Image checksum is not valid.

◆ SL_STATUS_SECURITY_DECRYPT_ERROR

#define SL_STATUS_SECURITY_DECRYPT_ERROR   ((sl_status_t)0x0047)

Decryption failed.

◆ SL_STATUS_COMMAND_IS_INVALID

#define SL_STATUS_COMMAND_IS_INVALID   ((sl_status_t)0x0048)

Command was not recognized.

◆ SL_STATUS_COMMAND_TOO_LONG

#define SL_STATUS_COMMAND_TOO_LONG   ((sl_status_t)0x0049)

Command or parameter maximum length exceeded.

◆ SL_STATUS_COMMAND_INCOMPLETE

#define SL_STATUS_COMMAND_INCOMPLETE   ((sl_status_t)0x004A)

Data received does not form a complete command.

◆ SL_STATUS_BUS_ERROR

#define SL_STATUS_BUS_ERROR   ((sl_status_t)0x004B)

Bus error, e.g. invalid DMA address.

◆ SL_STATUS_BT_OUT_OF_BONDS

#define SL_STATUS_BT_OUT_OF_BONDS   ((sl_status_t)0x0402)

Bonding procedure can't be started because device has no space left for bond.

◆ SL_STATUS_BT_UNSPECIFIED

#define SL_STATUS_BT_UNSPECIFIED   ((sl_status_t)0x0403)

Unspecified error.

◆ SL_STATUS_BT_HARDWARE

#define SL_STATUS_BT_HARDWARE   ((sl_status_t)0x0404)

Hardware failure.

◆ SL_STATUS_BT_NO_BONDING

#define SL_STATUS_BT_NO_BONDING   ((sl_status_t)0x0406)

The bonding does not exist.

◆ SL_STATUS_BT_CRYPTO

#define SL_STATUS_BT_CRYPTO   ((sl_status_t)0x0407)

Error using crypto functions.

◆ SL_STATUS_BT_DATA_CORRUPTED

#define SL_STATUS_BT_DATA_CORRUPTED   ((sl_status_t)0x0408)

Data was corrupted.

◆ SL_STATUS_BT_INVALID_SYNC_HANDLE

#define SL_STATUS_BT_INVALID_SYNC_HANDLE   ((sl_status_t)0x040A)

Invalid periodic advertising sync handle.

◆ SL_STATUS_BT_INVALID_MODULE_ACTION

#define SL_STATUS_BT_INVALID_MODULE_ACTION   ((sl_status_t)0x040B)

Bluetooth cannot be used on this hardware.

◆ SL_STATUS_BT_RADIO

#define SL_STATUS_BT_RADIO   ((sl_status_t)0x040C)

Error received from radio.

◆ SL_STATUS_BT_L2CAP_REMOTE_DISCONNECTED

#define SL_STATUS_BT_L2CAP_REMOTE_DISCONNECTED   ((sl_status_t)0x040D)

Returned when remote disconnects the connection-oriented channel by sending disconnection request.

◆ SL_STATUS_BT_L2CAP_LOCAL_DISCONNECTED

#define SL_STATUS_BT_L2CAP_LOCAL_DISCONNECTED   ((sl_status_t)0x040E)

Returned when local host disconnect the connection-oriented channel by sending disconnection request.

◆ SL_STATUS_BT_L2CAP_CID_NOT_EXIST

#define SL_STATUS_BT_L2CAP_CID_NOT_EXIST   ((sl_status_t)0x040F)

Returned when local host did not find a connection-oriented channel with given destination CID.

◆ SL_STATUS_BT_L2CAP_LE_DISCONNECTED

#define SL_STATUS_BT_L2CAP_LE_DISCONNECTED   ((sl_status_t)0x0410)

Returned when connection-oriented channel disconnected due to LE connection is dropped.

◆ SL_STATUS_BT_L2CAP_FLOW_CONTROL_VIOLATED

#define SL_STATUS_BT_L2CAP_FLOW_CONTROL_VIOLATED   ((sl_status_t)0x0412)

Returned when connection-oriented channel disconnected due to remote end send data even without credit.

◆ SL_STATUS_BT_L2CAP_FLOW_CONTROL_CREDIT_OVERFLOWED

#define SL_STATUS_BT_L2CAP_FLOW_CONTROL_CREDIT_OVERFLOWED   ((sl_status_t)0x0413)

Returned when connection-oriented channel disconnected due to remote end send flow control credits exceed 65535.

◆ SL_STATUS_BT_L2CAP_NO_FLOW_CONTROL_CREDIT

#define SL_STATUS_BT_L2CAP_NO_FLOW_CONTROL_CREDIT   ((sl_status_t)0x0414)

Returned when connection-oriented channel has run out of flow control credit and local application still trying to send data.

◆ SL_STATUS_BT_L2CAP_CONNECTION_REQUEST_TIMEOUT

#define SL_STATUS_BT_L2CAP_CONNECTION_REQUEST_TIMEOUT   ((sl_status_t)0x0415)

Returned when connection-oriented channel has not received connection response message within maximum timeout.

◆ SL_STATUS_BT_L2CAP_INVALID_CID

#define SL_STATUS_BT_L2CAP_INVALID_CID   ((sl_status_t)0x0416)

Returned when local host received a connection-oriented channel connection response with an invalid destination CID.

◆ SL_STATUS_BT_L2CAP_WRONG_STATE

#define SL_STATUS_BT_L2CAP_WRONG_STATE   ((sl_status_t)0x0417)

Returned when local host application tries to send a command which is not suitable for L2CAP channel's current state.

◆ SL_STATUS_BT_PS_STORE_FULL

#define SL_STATUS_BT_PS_STORE_FULL   ((sl_status_t)0x041B)

Flash reserved for PS store is full.

◆ SL_STATUS_BT_PS_KEY_NOT_FOUND

#define SL_STATUS_BT_PS_KEY_NOT_FOUND   ((sl_status_t)0x041C)

PS key not found.

◆ SL_STATUS_BT_APPLICATION_MISMATCHED_OR_INSUFFICIENT_SECURITY

#define SL_STATUS_BT_APPLICATION_MISMATCHED_OR_INSUFFICIENT_SECURITY   ((sl_status_t)0x041D)

Mismatched or insufficient security level.

◆ SL_STATUS_BT_APPLICATION_ENCRYPTION_DECRYPTION_ERROR

#define SL_STATUS_BT_APPLICATION_ENCRYPTION_DECRYPTION_ERROR   ((sl_status_t)0x041E)

Encrypion/decryption operation failed.

◆ SL_STATUS_BT_CTRL_UNKNOWN_CONNECTION_IDENTIFIER

#define SL_STATUS_BT_CTRL_UNKNOWN_CONNECTION_IDENTIFIER   ((sl_status_t)0x1002)

Connection does not exist, or connection open request was cancelled.

◆ SL_STATUS_BT_CTRL_AUTHENTICATION_FAILURE

#define SL_STATUS_BT_CTRL_AUTHENTICATION_FAILURE   ((sl_status_t)0x1005)

Pairing or authentication failed due to incorrect results in the pairing or authentication procedure. This could be due to an incorrect PIN or Link Key.

◆ SL_STATUS_BT_CTRL_PIN_OR_KEY_MISSING

#define SL_STATUS_BT_CTRL_PIN_OR_KEY_MISSING   ((sl_status_t)0x1006)

Pairing failed because of missing PIN, or authentication failed because of missing Key.

◆ SL_STATUS_BT_CTRL_MEMORY_CAPACITY_EXCEEDED

#define SL_STATUS_BT_CTRL_MEMORY_CAPACITY_EXCEEDED   ((sl_status_t)0x1007)

Controller is out of memory.

◆ SL_STATUS_BT_CTRL_CONNECTION_TIMEOUT

#define SL_STATUS_BT_CTRL_CONNECTION_TIMEOUT   ((sl_status_t)0x1008)

Link supervision timeout has expired.

◆ SL_STATUS_BT_CTRL_CONNECTION_LIMIT_EXCEEDED

#define SL_STATUS_BT_CTRL_CONNECTION_LIMIT_EXCEEDED   ((sl_status_t)0x1009)

Controller is at limit of connections it can support.

◆ SL_STATUS_BT_CTRL_SYNCHRONOUS_CONNECTIONTION_LIMIT_EXCEEDED

#define SL_STATUS_BT_CTRL_SYNCHRONOUS_CONNECTIONTION_LIMIT_EXCEEDED   ((sl_status_t)0x100A)

The Synchronous Connection Limit to a Device Exceeded error code indicates that the Controller has reached the limit to the number of synchronous connections that can be achieved to a device.

◆ SL_STATUS_BT_CTRL_ACL_CONNECTION_ALREADY_EXISTS

#define SL_STATUS_BT_CTRL_ACL_CONNECTION_ALREADY_EXISTS   ((sl_status_t)0x100B)

The ACL Connection Already Exists error code indicates that an attempt to create a new ACL Connection to a device when there is already a connection to this device.

◆ SL_STATUS_BT_CTRL_COMMAND_DISALLOWED

#define SL_STATUS_BT_CTRL_COMMAND_DISALLOWED   ((sl_status_t)0x100C)

Command requested cannot be executed because the Controller is in a state where it cannot process this command at this time.

◆ SL_STATUS_BT_CTRL_CONNECTION_REJECTED_DUE_TO_LIMITED_RESOURCES

#define SL_STATUS_BT_CTRL_CONNECTION_REJECTED_DUE_TO_LIMITED_RESOURCES   ((sl_status_t)0x100D)

The Connection Rejected Due To Limited Resources error code indicates that an incoming connection was rejected due to limited resources.

◆ SL_STATUS_BT_CTRL_CONNECTION_REJECTED_DUE_TO_SECURITY_REASONS

#define SL_STATUS_BT_CTRL_CONNECTION_REJECTED_DUE_TO_SECURITY_REASONS   ((sl_status_t)0x100E)

The Connection Rejected Due To Security Reasons error code indicates that a connection was rejected due to security requirements not being fulfilled, like authentication or pairing.

◆ SL_STATUS_BT_CTRL_CONNECTION_REJECTED_DUE_TO_UNACCEPTABLE_BD_ADDR

#define SL_STATUS_BT_CTRL_CONNECTION_REJECTED_DUE_TO_UNACCEPTABLE_BD_ADDR   ((sl_status_t)0x100F)

The Connection was rejected because this device does not accept the BD_ADDR. This may be because the device will only accept connections from specific BD_ADDRs.

◆ SL_STATUS_BT_CTRL_CONNECTION_ACCEPT_TIMEOUT_EXCEEDED

#define SL_STATUS_BT_CTRL_CONNECTION_ACCEPT_TIMEOUT_EXCEEDED   ((sl_status_t)0x1010)

The Connection Accept Timeout has been exceeded for this connection attempt.

◆ SL_STATUS_BT_CTRL_UNSUPPORTED_FEATURE_OR_PARAMETER_VALUE

#define SL_STATUS_BT_CTRL_UNSUPPORTED_FEATURE_OR_PARAMETER_VALUE   ((sl_status_t)0x1011)

A feature or parameter value in the HCI command is not supported.

◆ SL_STATUS_BT_CTRL_INVALID_COMMAND_PARAMETERS

#define SL_STATUS_BT_CTRL_INVALID_COMMAND_PARAMETERS   ((sl_status_t)0x1012)

Command contained invalid parameters.

◆ SL_STATUS_BT_CTRL_REMOTE_USER_TERMINATED

#define SL_STATUS_BT_CTRL_REMOTE_USER_TERMINATED   ((sl_status_t)0x1013)

User on the remote device terminated the connection.

◆ SL_STATUS_BT_CTRL_REMOTE_DEVICE_TERMINATED_CONNECTION_DUE_TO_LOW_RESOURCES

#define SL_STATUS_BT_CTRL_REMOTE_DEVICE_TERMINATED_CONNECTION_DUE_TO_LOW_RESOURCES   ((sl_status_t)0x1014)

The remote device terminated the connection because of low resources.

◆ SL_STATUS_BT_CTRL_REMOTE_POWERING_OFF

#define SL_STATUS_BT_CTRL_REMOTE_POWERING_OFF   ((sl_status_t)0x1015)

Remote Device Terminated Connection due to Power Off.

◆ SL_STATUS_BT_CTRL_CONNECTION_TERMINATED_BY_LOCAL_HOST

#define SL_STATUS_BT_CTRL_CONNECTION_TERMINATED_BY_LOCAL_HOST   ((sl_status_t)0x1016)

Local device terminated the connection.

◆ SL_STATUS_BT_CTRL_REPEATED_ATTEMPTS

#define SL_STATUS_BT_CTRL_REPEATED_ATTEMPTS   ((sl_status_t)0x1017)

The Controller is disallowing an authentication or pairing procedure because too little time has elapsed since the last authentication or pairing attempt failed.

◆ SL_STATUS_BT_CTRL_PAIRING_NOT_ALLOWED

#define SL_STATUS_BT_CTRL_PAIRING_NOT_ALLOWED   ((sl_status_t)0x1018)

The device does not allow pairing. This can be for example, when a device only allows pairing during a certain time window after some user input allows pairing.

◆ SL_STATUS_BT_CTRL_UNSUPPORTED_REMOTE_FEATURE

#define SL_STATUS_BT_CTRL_UNSUPPORTED_REMOTE_FEATURE   ((sl_status_t)0x101A)

The remote device does not support the feature associated with the issued command.

◆ SL_STATUS_BT_CTRL_UNSPECIFIED_ERROR

#define SL_STATUS_BT_CTRL_UNSPECIFIED_ERROR   ((sl_status_t)0x101F)

No other error code specified is appropriate to use.

◆ SL_STATUS_BT_CTRL_LL_RESPONSE_TIMEOUT

#define SL_STATUS_BT_CTRL_LL_RESPONSE_TIMEOUT   ((sl_status_t)0x1022)

Connection terminated due to link-layer procedure timeout.

◆ SL_STATUS_BT_CTRL_LL_PROCEDURE_COLLISION

#define SL_STATUS_BT_CTRL_LL_PROCEDURE_COLLISION   ((sl_status_t)0x1023)

LL procedure has collided with the same transaction or procedure that is already in progress.

◆ SL_STATUS_BT_CTRL_ENCRYPTION_MODE_NOT_ACCEPTABLE

#define SL_STATUS_BT_CTRL_ENCRYPTION_MODE_NOT_ACCEPTABLE   ((sl_status_t)0x1025)

The requested encryption mode is not acceptable at this time.

◆ SL_STATUS_BT_CTRL_LINK_KEY_CANNOT_BE_CHANGED

#define SL_STATUS_BT_CTRL_LINK_KEY_CANNOT_BE_CHANGED   ((sl_status_t)0x1026)

Link key cannot be changed because a fixed unit key is being used.

◆ SL_STATUS_BT_CTRL_INSTANT_PASSED

#define SL_STATUS_BT_CTRL_INSTANT_PASSED   ((sl_status_t)0x1028)

LMP PDU or LL PDU that includes an instant cannot be performed because the instant when this would have occurred has passed.

◆ SL_STATUS_BT_CTRL_PAIRING_WITH_UNIT_KEY_NOT_SUPPORTED

#define SL_STATUS_BT_CTRL_PAIRING_WITH_UNIT_KEY_NOT_SUPPORTED   ((sl_status_t)0x1029)

It was not possible to pair as a unit key was requested and it is not supported.

◆ SL_STATUS_BT_CTRL_DIFFERENT_TRANSACTION_COLLISION

#define SL_STATUS_BT_CTRL_DIFFERENT_TRANSACTION_COLLISION   ((sl_status_t)0x102A)

LMP transaction was started that collides with an ongoing transaction.

◆ SL_STATUS_BT_CTRL_CHANNEL_ASSESSMENT_NOT_SUPPORTED

#define SL_STATUS_BT_CTRL_CHANNEL_ASSESSMENT_NOT_SUPPORTED   ((sl_status_t)0x102E)

The Controller cannot perform channel assessment because it is not supported.

◆ SL_STATUS_BT_CTRL_INSUFFICIENT_SECURITY

#define SL_STATUS_BT_CTRL_INSUFFICIENT_SECURITY   ((sl_status_t)0x102F)

The HCI command or LMP PDU sent is only possible on an encrypted link.

◆ SL_STATUS_BT_CTRL_PARAMETER_OUT_OF_MANDATORY_RANGE

#define SL_STATUS_BT_CTRL_PARAMETER_OUT_OF_MANDATORY_RANGE   ((sl_status_t)0x1030)

A parameter value requested is outside the mandatory range of parameters for the given HCI command or LMP PDU.

◆ SL_STATUS_BT_CTRL_SIMPLE_PAIRING_NOT_SUPPORTED_BY_HOST

#define SL_STATUS_BT_CTRL_SIMPLE_PAIRING_NOT_SUPPORTED_BY_HOST   ((sl_status_t)0x1037)

The IO capabilities request or response was rejected because the sending Host does not support Secure Simple Pairing even though the receiving Link Manager does.

◆ SL_STATUS_BT_CTRL_HOST_BUSY_PAIRING

#define SL_STATUS_BT_CTRL_HOST_BUSY_PAIRING   ((sl_status_t)0x1038)

The Host is busy with another pairing operation and unable to support the requested pairing. The receiving device should retry pairing again later.

◆ SL_STATUS_BT_CTRL_CONNECTION_REJECTED_DUE_TO_NO_SUITABLE_CHANNEL_FOUND

#define SL_STATUS_BT_CTRL_CONNECTION_REJECTED_DUE_TO_NO_SUITABLE_CHANNEL_FOUND   ((sl_status_t)0x1039)

The Controller could not calculate an appropriate value for the Channel selection operation.

◆ SL_STATUS_BT_CTRL_CONTROLLER_BUSY

#define SL_STATUS_BT_CTRL_CONTROLLER_BUSY   ((sl_status_t)0x103A)

Operation was rejected because the controller is busy and unable to process the request.

◆ SL_STATUS_BT_CTRL_UNACCEPTABLE_CONNECTION_INTERVAL

#define SL_STATUS_BT_CTRL_UNACCEPTABLE_CONNECTION_INTERVAL   ((sl_status_t)0x103B)

Remote device terminated the connection because of an unacceptable connection interval.

◆ SL_STATUS_BT_CTRL_ADVERTISING_TIMEOUT

#define SL_STATUS_BT_CTRL_ADVERTISING_TIMEOUT   ((sl_status_t)0x103C)

Ddvertising for a fixed duration completed or, for directed advertising, that advertising completed without a connection being created.

◆ SL_STATUS_BT_CTRL_CONNECTION_TERMINATED_DUE_TO_MIC_FAILURE

#define SL_STATUS_BT_CTRL_CONNECTION_TERMINATED_DUE_TO_MIC_FAILURE   ((sl_status_t)0x103D)

Connection was terminated because the Message Integrity Check (MIC) failed on a received packet.

◆ SL_STATUS_BT_CTRL_CONNECTION_FAILED_TO_BE_ESTABLISHED

#define SL_STATUS_BT_CTRL_CONNECTION_FAILED_TO_BE_ESTABLISHED   ((sl_status_t)0x103E)

LL initiated a connection but the connection has failed to be established. Controller did not receive any packets from remote end.

◆ SL_STATUS_BT_CTRL_MAC_CONNECTION_FAILED

#define SL_STATUS_BT_CTRL_MAC_CONNECTION_FAILED   ((sl_status_t)0x103F)

The MAC of the 802.11 AMP was requested to connect to a peer, but the connection failed.

◆ SL_STATUS_BT_CTRL_COARSE_CLOCK_ADJUSTMENT_REJECTED_BUT_WILL_TRY_TO_ADJUST_USING_CLOCK_DRAGGING

#define SL_STATUS_BT_CTRL_COARSE_CLOCK_ADJUSTMENT_REJECTED_BUT_WILL_TRY_TO_ADJUST_USING_CLOCK_DRAGGING   ((sl_status_t)0x1040)

The master, at this time, is unable to make a coarse adjustment to the piconet clock, using the supplied parameters. Instead the master will attempt to move the clock using clock dragging.

◆ SL_STATUS_BT_CTRL_UNKNOWN_ADVERTISING_IDENTIFIER

#define SL_STATUS_BT_CTRL_UNKNOWN_ADVERTISING_IDENTIFIER   ((sl_status_t)0x1042)

A command was sent from the Host that should identify an Advertising or Sync handle, but the Advertising or Sync handle does not exist.

◆ SL_STATUS_BT_CTRL_LIMIT_REACHED

#define SL_STATUS_BT_CTRL_LIMIT_REACHED   ((sl_status_t)0x1043)

Number of operations requested has been reached and has indicated the completion of the activity (e.g., advertising or scanning).

◆ SL_STATUS_BT_CTRL_OPERATION_CANCELLED_BY_HOST

#define SL_STATUS_BT_CTRL_OPERATION_CANCELLED_BY_HOST   ((sl_status_t)0x1044)

A request to the Controller issued by the Host and still pending was successfully canceled.

◆ SL_STATUS_BT_CTRL_PACKET_TOO_LONG

#define SL_STATUS_BT_CTRL_PACKET_TOO_LONG   ((sl_status_t)0x1045)

An attempt was made to send or receive a packet that exceeds the maximum allowed packet l.

◆ SL_STATUS_BT_ATT_INVALID_HANDLE

#define SL_STATUS_BT_ATT_INVALID_HANDLE   ((sl_status_t)0x1101)

The attribute handle given was not valid on this server.

◆ SL_STATUS_BT_ATT_READ_NOT_PERMITTED

#define SL_STATUS_BT_ATT_READ_NOT_PERMITTED   ((sl_status_t)0x1102)

The attribute cannot be read.

◆ SL_STATUS_BT_ATT_WRITE_NOT_PERMITTED

#define SL_STATUS_BT_ATT_WRITE_NOT_PERMITTED   ((sl_status_t)0x1103)

The attribute cannot be written.

◆ SL_STATUS_BT_ATT_INVALID_PDU

#define SL_STATUS_BT_ATT_INVALID_PDU   ((sl_status_t)0x1104)

The attribute PDU was invalid.

◆ SL_STATUS_BT_ATT_INSUFFICIENT_AUTHENTICATION

#define SL_STATUS_BT_ATT_INSUFFICIENT_AUTHENTICATION   ((sl_status_t)0x1105)

The attribute requires authentication before it can be read or written.

◆ SL_STATUS_BT_ATT_REQUEST_NOT_SUPPORTED

#define SL_STATUS_BT_ATT_REQUEST_NOT_SUPPORTED   ((sl_status_t)0x1106)

Attribute Server does not support the request received from the client.

◆ SL_STATUS_BT_ATT_INVALID_OFFSET

#define SL_STATUS_BT_ATT_INVALID_OFFSET   ((sl_status_t)0x1107)

Offset specified was past the end of the attribute.

◆ SL_STATUS_BT_ATT_INSUFFICIENT_AUTHORIZATION

#define SL_STATUS_BT_ATT_INSUFFICIENT_AUTHORIZATION   ((sl_status_t)0x1108)

The attribute requires authorization before it can be read or written.

◆ SL_STATUS_BT_ATT_PREPARE_QUEUE_FULL

#define SL_STATUS_BT_ATT_PREPARE_QUEUE_FULL   ((sl_status_t)0x1109)

Too many prepare writes have been queueud.

◆ SL_STATUS_BT_ATT_ATT_NOT_FOUND

#define SL_STATUS_BT_ATT_ATT_NOT_FOUND   ((sl_status_t)0x110A)

No attribute found within the given attribute handle range.

◆ SL_STATUS_BT_ATT_ATT_NOT_LONG

#define SL_STATUS_BT_ATT_ATT_NOT_LONG   ((sl_status_t)0x110B)

The attribute cannot be read or written using the Read Blob Request.

◆ SL_STATUS_BT_ATT_INSUFFICIENT_ENC_KEY_SIZE

#define SL_STATUS_BT_ATT_INSUFFICIENT_ENC_KEY_SIZE   ((sl_status_t)0x110C)

The Encryption Key Size used for encrypting this link is insufficient.

◆ SL_STATUS_BT_ATT_INVALID_ATT_LENGTH

#define SL_STATUS_BT_ATT_INVALID_ATT_LENGTH   ((sl_status_t)0x110D)

The attribute value length is invalid for the operation.

◆ SL_STATUS_BT_ATT_UNLIKELY_ERROR

#define SL_STATUS_BT_ATT_UNLIKELY_ERROR   ((sl_status_t)0x110E)

The attribute request that was requested has encountered an error that was unlikely, and therefore could not be completed as requested.

◆ SL_STATUS_BT_ATT_INSUFFICIENT_ENCRYPTION

#define SL_STATUS_BT_ATT_INSUFFICIENT_ENCRYPTION   ((sl_status_t)0x110F)

The attribute requires encryption before it can be read or written.

◆ SL_STATUS_BT_ATT_UNSUPPORTED_GROUP_TYPE

#define SL_STATUS_BT_ATT_UNSUPPORTED_GROUP_TYPE   ((sl_status_t)0x1110)

The attribute type is not a supported grouping attribute as defined by a higher layer specification.

◆ SL_STATUS_BT_ATT_INSUFFICIENT_RESOURCES

#define SL_STATUS_BT_ATT_INSUFFICIENT_RESOURCES   ((sl_status_t)0x1111)

Insufficient Resources to complete the request.

◆ SL_STATUS_BT_ATT_OUT_OF_SYNC

#define SL_STATUS_BT_ATT_OUT_OF_SYNC   ((sl_status_t)0x1112)

The server requests the client to rediscover the database.

◆ SL_STATUS_BT_ATT_VALUE_NOT_ALLOWED

#define SL_STATUS_BT_ATT_VALUE_NOT_ALLOWED   ((sl_status_t)0x1113)

The attribute parameter value was not allowed.

◆ SL_STATUS_BT_ATT_APPLICATION

#define SL_STATUS_BT_ATT_APPLICATION   ((sl_status_t)0x1180)

When this is returned in a BGAPI response, the application tried to read or write the value of a user attribute from the GATT databa.

◆ SL_STATUS_BT_ATT_WRITE_REQUEST_REJECTED

#define SL_STATUS_BT_ATT_WRITE_REQUEST_REJECTED   ((sl_status_t)0x11FC)

The requested write operation cannot be fulfilled for reasons other than permissions.

◆ SL_STATUS_BT_ATT_CLIENT_CHARACTERISTIC_CONFIGURATION_DESCRIPTOR_IMPROPERLY_CONFIGURED

#define SL_STATUS_BT_ATT_CLIENT_CHARACTERISTIC_CONFIGURATION_DESCRIPTOR_IMPROPERLY_CONFIGURED   ((sl_status_t)0x11FD)

The Client Characteristic Configuration descriptor is not configured according to the requirements of the profile or service.

◆ SL_STATUS_BT_ATT_PROCEDURE_ALREADY_IN_PROGRESS

#define SL_STATUS_BT_ATT_PROCEDURE_ALREADY_IN_PROGRESS   ((sl_status_t)0x11FE)

The profile or service request cannot be serviced because an operation that has been previously triggered is still in progress.

◆ SL_STATUS_BT_ATT_OUT_OF_RANGE

#define SL_STATUS_BT_ATT_OUT_OF_RANGE   ((sl_status_t)0x11FF)

The attribute value is out of range as defined by a profile or service specification.

◆ SL_STATUS_BT_SMP_PASSKEY_ENTRY_FAILED

#define SL_STATUS_BT_SMP_PASSKEY_ENTRY_FAILED   ((sl_status_t)0x1201)

The user input of passkey failed, for example, the user cancelled the operation.

◆ SL_STATUS_BT_SMP_OOB_NOT_AVAILABLE

#define SL_STATUS_BT_SMP_OOB_NOT_AVAILABLE   ((sl_status_t)0x1202)

Out of Band data is not available for authentication.

◆ SL_STATUS_BT_SMP_AUTHENTICATION_REQUIREMENTS

#define SL_STATUS_BT_SMP_AUTHENTICATION_REQUIREMENTS   ((sl_status_t)0x1203)

The pairing procedure cannot be performed as authentication requirements cannot be met due to IO capabilities of one or both devices.

◆ SL_STATUS_BT_SMP_CONFIRM_VALUE_FAILED

#define SL_STATUS_BT_SMP_CONFIRM_VALUE_FAILED   ((sl_status_t)0x1204)

The confirm value does not match the calculated compare value.

◆ SL_STATUS_BT_SMP_PAIRING_NOT_SUPPORTED

#define SL_STATUS_BT_SMP_PAIRING_NOT_SUPPORTED   ((sl_status_t)0x1205)

Pairing is not supported by the device.

◆ SL_STATUS_BT_SMP_ENCRYPTION_KEY_SIZE

#define SL_STATUS_BT_SMP_ENCRYPTION_KEY_SIZE   ((sl_status_t)0x1206)

The resultant encryption key size is insufficient for the security requirements of this device.

◆ SL_STATUS_BT_SMP_COMMAND_NOT_SUPPORTED

#define SL_STATUS_BT_SMP_COMMAND_NOT_SUPPORTED   ((sl_status_t)0x1207)

The SMP command received is not supported on this device.

◆ SL_STATUS_BT_SMP_UNSPECIFIED_REASON

#define SL_STATUS_BT_SMP_UNSPECIFIED_REASON   ((sl_status_t)0x1208)

Pairing failed due to an unspecified reason.

◆ SL_STATUS_BT_SMP_REPEATED_ATTEMPTS

#define SL_STATUS_BT_SMP_REPEATED_ATTEMPTS   ((sl_status_t)0x1209)

Pairing or authentication procedure is disallowed because too little time has elapsed since last pairing request or security request.

◆ SL_STATUS_BT_SMP_INVALID_PARAMETERS

#define SL_STATUS_BT_SMP_INVALID_PARAMETERS   ((sl_status_t)0x120A)

The Invalid Parameters error code indicates: the command length is invalid or a parameter is outside of the specified range.

◆ SL_STATUS_BT_SMP_DHKEY_CHECK_FAILED

#define SL_STATUS_BT_SMP_DHKEY_CHECK_FAILED   ((sl_status_t)0x120B)

Indicates to the remote device that the DHKey Check value received doesn't match the one calculated by the local device.

◆ SL_STATUS_BT_SMP_NUMERIC_COMPARISON_FAILED

#define SL_STATUS_BT_SMP_NUMERIC_COMPARISON_FAILED   ((sl_status_t)0x120C)

Indicates that the confirm values in the numeric comparison protocol do not match.

◆ SL_STATUS_BT_SMP_BREDR_PAIRING_IN_PROGRESS

#define SL_STATUS_BT_SMP_BREDR_PAIRING_IN_PROGRESS   ((sl_status_t)0x120D)

Indicates that the pairing over the LE transport failed due to a Pairing Request sent over the BR/EDR transport in process.

◆ SL_STATUS_BT_SMP_CROSS_TRANSPORT_KEY_DERIVATION_GENERATION_NOT_ALLOWED

#define SL_STATUS_BT_SMP_CROSS_TRANSPORT_KEY_DERIVATION_GENERATION_NOT_ALLOWED   ((sl_status_t)0x120E)

Indicates that the BR/EDR Link Key generated on the BR/EDR transport cannot be used to derive and distribute keys for the LE transport.

◆ SL_STATUS_BT_MESH_ALREADY_EXISTS

#define SL_STATUS_BT_MESH_ALREADY_EXISTS   ((sl_status_t)0x0501)

Returned when trying to add a key or some other unique resource with an ID which already exists.

◆ SL_STATUS_BT_MESH_DOES_NOT_EXIST

#define SL_STATUS_BT_MESH_DOES_NOT_EXIST   ((sl_status_t)0x0502)

Returned when trying to manipulate a key or some other resource with an ID which does not exist.

◆ SL_STATUS_BT_MESH_LIMIT_REACHED

#define SL_STATUS_BT_MESH_LIMIT_REACHED   ((sl_status_t)0x0503)

Returned when an operation cannot be executed because a pre-configured limit for keys, key bindings, elements, models, virtual addresses, provisioned devices, or provisioning sessions is reached.

◆ SL_STATUS_BT_MESH_INVALID_ADDRESS

#define SL_STATUS_BT_MESH_INVALID_ADDRESS   ((sl_status_t)0x0504)

Returned when trying to use a reserved address or add a "pre-provisioned" device using an address already used by some other device.

◆ SL_STATUS_BT_MESH_MALFORMED_DATA

#define SL_STATUS_BT_MESH_MALFORMED_DATA   ((sl_status_t)0x0505)

In a BGAPI response, the user supplied malformed data; in a BGAPI event, the remote end responded with malformed or unrecognized data.

◆ SL_STATUS_BT_MESH_ALREADY_INITIALIZED

#define SL_STATUS_BT_MESH_ALREADY_INITIALIZED   ((sl_status_t)0x0506)

An attempt was made to initialize a subsystem that was already initialized.

◆ SL_STATUS_BT_MESH_NOT_INITIALIZED

#define SL_STATUS_BT_MESH_NOT_INITIALIZED   ((sl_status_t)0x0507)

An attempt was made to use a subsystem that wasn't initialized yet. Call the subsystem's init function first.

◆ SL_STATUS_BT_MESH_NO_FRIEND_OFFER

#define SL_STATUS_BT_MESH_NO_FRIEND_OFFER   ((sl_status_t)0x0508)

Returned when trying to establish a friendship as a Low Power Node, but no acceptable friend offer message was received.

◆ SL_STATUS_BT_MESH_PROV_LINK_CLOSED

#define SL_STATUS_BT_MESH_PROV_LINK_CLOSED   ((sl_status_t)0x0509)

Provisioning link was unexpectedly closed before provisioning was complete.

◆ SL_STATUS_BT_MESH_PROV_INVALID_PDU

#define SL_STATUS_BT_MESH_PROV_INVALID_PDU   ((sl_status_t)0x050A)

An unrecognized provisioning PDU was received.

◆ SL_STATUS_BT_MESH_PROV_INVALID_PDU_FORMAT

#define SL_STATUS_BT_MESH_PROV_INVALID_PDU_FORMAT   ((sl_status_t)0x050B)

A provisioning PDU with wrong length or containing field values that are out of bounds was received.

◆ SL_STATUS_BT_MESH_PROV_UNEXPECTED_PDU

#define SL_STATUS_BT_MESH_PROV_UNEXPECTED_PDU   ((sl_status_t)0x050C)

An unexpected (out of sequence) provisioning PDU was received.

◆ SL_STATUS_BT_MESH_PROV_CONFIRMATION_FAILED

#define SL_STATUS_BT_MESH_PROV_CONFIRMATION_FAILED   ((sl_status_t)0x050D)

The computed confirmation value did not match the expected value.

◆ SL_STATUS_BT_MESH_PROV_OUT_OF_RESOURCES

#define SL_STATUS_BT_MESH_PROV_OUT_OF_RESOURCES   ((sl_status_t)0x050E)

Provisioning could not be continued due to insufficient resources.

◆ SL_STATUS_BT_MESH_PROV_DECRYPTION_FAILED

#define SL_STATUS_BT_MESH_PROV_DECRYPTION_FAILED   ((sl_status_t)0x050F)

The provisioning data block could not be decrypted.

◆ SL_STATUS_BT_MESH_PROV_UNEXPECTED_ERROR

#define SL_STATUS_BT_MESH_PROV_UNEXPECTED_ERROR   ((sl_status_t)0x0510)

An unexpected error happened during provisioning.

◆ SL_STATUS_BT_MESH_PROV_CANNOT_ASSIGN_ADDR

#define SL_STATUS_BT_MESH_PROV_CANNOT_ASSIGN_ADDR   ((sl_status_t)0x0511)

Device could not assign unicast addresses to all of its elements.

◆ SL_STATUS_BT_MESH_ADDRESS_TEMPORARILY_UNAVAILABLE

#define SL_STATUS_BT_MESH_ADDRESS_TEMPORARILY_UNAVAILABLE   ((sl_status_t)0x0512)

Returned when trying to reuse an address of a previously deleted device before an IV Index Update has been executed.

◆ SL_STATUS_BT_MESH_ADDRESS_ALREADY_USED

#define SL_STATUS_BT_MESH_ADDRESS_ALREADY_USED   ((sl_status_t)0x0513)

Returned when trying to assign an address that is used by one of the devices in the Device Database, or by the Provisioner itself.

◆ SL_STATUS_BT_MESH_PUBLISH_NOT_CONFIGURED

#define SL_STATUS_BT_MESH_PUBLISH_NOT_CONFIGURED   ((sl_status_t)0x0514)

Application key or publish address are not set.

◆ SL_STATUS_BT_MESH_APP_KEY_NOT_BOUND

#define SL_STATUS_BT_MESH_APP_KEY_NOT_BOUND   ((sl_status_t)0x0515)

Application key is not bound to a model.

◆ SL_STATUS_BT_MESH_FOUNDATION_INVALID_ADDRESS

#define SL_STATUS_BT_MESH_FOUNDATION_INVALID_ADDRESS   ((sl_status_t)0x1301)

Returned when address in request was not valid.

◆ SL_STATUS_BT_MESH_FOUNDATION_INVALID_MODEL

#define SL_STATUS_BT_MESH_FOUNDATION_INVALID_MODEL   ((sl_status_t)0x1302)

Returned when model identified is not found for a given element.

◆ SL_STATUS_BT_MESH_FOUNDATION_INVALID_APP_KEY

#define SL_STATUS_BT_MESH_FOUNDATION_INVALID_APP_KEY   ((sl_status_t)0x1303)

Returned when the key identified by AppKeyIndex is not stored in the node.

◆ SL_STATUS_BT_MESH_FOUNDATION_INVALID_NET_KEY

#define SL_STATUS_BT_MESH_FOUNDATION_INVALID_NET_KEY   ((sl_status_t)0x1304)

Returned when the key identified by NetKeyIndex is not stored in the node.

◆ SL_STATUS_BT_MESH_FOUNDATION_INSUFFICIENT_RESOURCES

#define SL_STATUS_BT_MESH_FOUNDATION_INSUFFICIENT_RESOURCES   ((sl_status_t)0x1305)

Returned when The node cannot serve the request due to insufficient resources.

◆ SL_STATUS_BT_MESH_FOUNDATION_KEY_INDEX_EXISTS

#define SL_STATUS_BT_MESH_FOUNDATION_KEY_INDEX_EXISTS   ((sl_status_t)0x1306)

Returned when the key identified is already stored in the node and the new NetKey value is different.

◆ SL_STATUS_BT_MESH_FOUNDATION_INVALID_PUBLISH_PARAMS

#define SL_STATUS_BT_MESH_FOUNDATION_INVALID_PUBLISH_PARAMS   ((sl_status_t)0x1307)

Returned when the model does not support the publish mechanism.

◆ SL_STATUS_BT_MESH_FOUNDATION_NOT_SUBSCRIBE_MODEL

#define SL_STATUS_BT_MESH_FOUNDATION_NOT_SUBSCRIBE_MODEL   ((sl_status_t)0x1308)

Returned when the model does not support the subscribe mechanism.

◆ SL_STATUS_BT_MESH_FOUNDATION_STORAGE_FAILURE

#define SL_STATUS_BT_MESH_FOUNDATION_STORAGE_FAILURE   ((sl_status_t)0x1309)

Returned when storing of the requested parameters failed.

◆ SL_STATUS_BT_MESH_FOUNDATION_NOT_SUPPORTED

#define SL_STATUS_BT_MESH_FOUNDATION_NOT_SUPPORTED   ((sl_status_t)0x130A)

Returned when requested setting is not supported.

◆ SL_STATUS_BT_MESH_FOUNDATION_CANNOT_UPDATE

#define SL_STATUS_BT_MESH_FOUNDATION_CANNOT_UPDATE   ((sl_status_t)0x130B)

Returned when the requested update operation cannot be performed due to general constraints.

◆ SL_STATUS_BT_MESH_FOUNDATION_CANNOT_REMOVE

#define SL_STATUS_BT_MESH_FOUNDATION_CANNOT_REMOVE   ((sl_status_t)0x130C)

Returned when the requested delete operation cannot be performed due to general constraints.

◆ SL_STATUS_BT_MESH_FOUNDATION_CANNOT_BIND

#define SL_STATUS_BT_MESH_FOUNDATION_CANNOT_BIND   ((sl_status_t)0x130D)

Returned when the requested bind operation cannot be performed due to general constraints.

◆ SL_STATUS_BT_MESH_FOUNDATION_TEMPORARILY_UNABLE

#define SL_STATUS_BT_MESH_FOUNDATION_TEMPORARILY_UNABLE   ((sl_status_t)0x130E)

Returned when The node cannot start advertising with Node Identity or Proxy since the maximum number of parallel advertising is reached.

◆ SL_STATUS_BT_MESH_FOUNDATION_CANNOT_SET

#define SL_STATUS_BT_MESH_FOUNDATION_CANNOT_SET   ((sl_status_t)0x130F)

Returned when the requested state cannot be set.

◆ SL_STATUS_BT_MESH_FOUNDATION_UNSPECIFIED

#define SL_STATUS_BT_MESH_FOUNDATION_UNSPECIFIED   ((sl_status_t)0x1310)

Returned when an unspecified error took place.

◆ SL_STATUS_BT_MESH_FOUNDATION_INVALID_BINDING

#define SL_STATUS_BT_MESH_FOUNDATION_INVALID_BINDING   ((sl_status_t)0x1311)

Returned when the NetKeyIndex and AppKeyIndex combination is not valid for a Config AppKey Update.

◆ SL_STATUS_WIFI_INVALID_KEY

#define SL_STATUS_WIFI_INVALID_KEY   ((sl_status_t)0x0B01)

Invalid firmware keyset.

◆ SL_STATUS_WIFI_FIRMWARE_DOWNLOAD_TIMEOUT

#define SL_STATUS_WIFI_FIRMWARE_DOWNLOAD_TIMEOUT   ((sl_status_t)0x0B02)

The firmware download took too long.

◆ SL_STATUS_WIFI_UNSUPPORTED_MESSAGE_ID

#define SL_STATUS_WIFI_UNSUPPORTED_MESSAGE_ID   ((sl_status_t)0x0B03)

Unknown request ID or wrong interface ID used.

◆ SL_STATUS_WIFI_WARNING

#define SL_STATUS_WIFI_WARNING   ((sl_status_t)0x0B04)

The request is successful but some parameters have been ignored.

◆ SL_STATUS_WIFI_NO_PACKET_TO_RECEIVE

#define SL_STATUS_WIFI_NO_PACKET_TO_RECEIVE   ((sl_status_t)0x0B05)

No Packets waiting to be received.

◆ SL_STATUS_WIFI_SLEEP_GRANTED

#define SL_STATUS_WIFI_SLEEP_GRANTED   ((sl_status_t)0x0B08)

The sleep mode is granted.

◆ SL_STATUS_WIFI_SLEEP_NOT_GRANTED

#define SL_STATUS_WIFI_SLEEP_NOT_GRANTED   ((sl_status_t)0x0B09)

The WFx does not go back to sleep.

◆ SL_STATUS_WIFI_SECURE_LINK_MAC_KEY_ERROR

#define SL_STATUS_WIFI_SECURE_LINK_MAC_KEY_ERROR   ((sl_status_t)0x0B10)

The SecureLink MAC key was not found.

◆ SL_STATUS_WIFI_SECURE_LINK_MAC_KEY_ALREADY_BURNED

#define SL_STATUS_WIFI_SECURE_LINK_MAC_KEY_ALREADY_BURNED   ((sl_status_t)0x0B11)

The SecureLink MAC key is already installed in OTP.

◆ SL_STATUS_WIFI_SECURE_LINK_RAM_MODE_NOT_ALLOWED

#define SL_STATUS_WIFI_SECURE_LINK_RAM_MODE_NOT_ALLOWED   ((sl_status_t)0x0B12)

The SecureLink MAC key cannot be installed in RAM.

◆ SL_STATUS_WIFI_SECURE_LINK_FAILED_UNKNOWN_MODE

#define SL_STATUS_WIFI_SECURE_LINK_FAILED_UNKNOWN_MODE   ((sl_status_t)0x0B13)

The SecureLink MAC key installation failed.

◆ SL_STATUS_WIFI_SECURE_LINK_EXCHANGE_FAILED

#define SL_STATUS_WIFI_SECURE_LINK_EXCHANGE_FAILED   ((sl_status_t)0x0B14)

SecureLink key (re)negotiation failed.

◆ SL_STATUS_WIFI_WRONG_STATE

#define SL_STATUS_WIFI_WRONG_STATE   ((sl_status_t)0x0B18)

The device is in an inappropriate state to perform the request.

◆ SL_STATUS_WIFI_CHANNEL_NOT_ALLOWED

#define SL_STATUS_WIFI_CHANNEL_NOT_ALLOWED   ((sl_status_t)0x0B19)

The request failed due to regulatory limitations.

◆ SL_STATUS_WIFI_NO_MATCHING_AP

#define SL_STATUS_WIFI_NO_MATCHING_AP   ((sl_status_t)0x0B1A)

The connection request failed because no suitable AP was found.

◆ SL_STATUS_WIFI_CONNECTION_ABORTED

#define SL_STATUS_WIFI_CONNECTION_ABORTED   ((sl_status_t)0x0B1B)

The connection request was aborted by host.

◆ SL_STATUS_WIFI_CONNECTION_TIMEOUT

#define SL_STATUS_WIFI_CONNECTION_TIMEOUT   ((sl_status_t)0x0B1C)

The connection request failed because of a timeout.

◆ SL_STATUS_WIFI_CONNECTION_REJECTED_BY_AP

#define SL_STATUS_WIFI_CONNECTION_REJECTED_BY_AP   ((sl_status_t)0x0B1D)

The connection request failed because the AP rejected the device.

◆ SL_STATUS_WIFI_CONNECTION_AUTH_FAILURE

#define SL_STATUS_WIFI_CONNECTION_AUTH_FAILURE   ((sl_status_t)0x0B1E)

The connection request failed because the WPA handshake did not complete successfully.

◆ SL_STATUS_WIFI_RETRY_EXCEEDED

#define SL_STATUS_WIFI_RETRY_EXCEEDED   ((sl_status_t)0x0B1F)

The request failed because the retry limit was exceeded.

◆ SL_STATUS_WIFI_TX_LIFETIME_EXCEEDED

#define SL_STATUS_WIFI_TX_LIFETIME_EXCEEDED   ((sl_status_t)0x0B20)

The request failed because the MSDU life time was exceeded.