Description

Digital Signature Algorithms (ECDSA, EdDSA).

API for using digital signatures with the SE.

Functions

sl_status_t sl_se_ecc_sign ( sl_se_command_context_t *cmd_ctx, const sl_se_key_descriptor_t *key, sl_se_hash_type_t hash_alg, bool hashed_message, const unsigned char *message, size_t message_len, unsigned char *signature, size_t signature_len)
This function computes Elliptic-Curve Cryptography (ECC) digital signatures of a message.
sl_status_t sl_se_ecc_verify ( sl_se_command_context_t *cmd_ctx, const sl_se_key_descriptor_t *key, sl_se_hash_type_t hash_alg, bool hashed_message, const unsigned char *message, size_t message_len, const unsigned char *signature, size_t signature_len)
This function verifies Elliptic-Curve Cryptography (ECC) digital signatures of a message.

Function Documentation

◆ sl_se_ecc_sign()

sl_status_t sl_se_ecc_sign ( sl_se_command_context_t * cmd_ctx,
const sl_se_key_descriptor_t * key,
sl_se_hash_type_t hash_alg,
bool hashed_message,
const unsigned char * message,
size_t message_len,
unsigned char * signature,
size_t signature_len
)

This function computes Elliptic-Curve Cryptography (ECC) digital signatures of a message.

Note
Edwards-curve Digital Signature Algorithm (EdDSA) generates a message digest using the input message for computing signatures. The input parameters hash_alg and hashed_message do not apply for EdDSA.

P-521 Elliptic Curve for Elliptic Curve Digital Signature Algorithm (ECDSA) expects a 544 bits (68 bytes) buffer for storing private keys, and a 1088 bits (136 bytes) buffer for storing public keys and signatures. The first 23 bits of d, Qx, Qy, R and S are padding bits to comply word-aligned addressing.

Parameters
[in] cmd_ctx Pointer to an SE command context object.
[in] key Pointer to sl_se_key_descriptor_t structure.
[in] hash_alg Which hashing algorithm to use. Ignored for EdDSA keys, since EdDSA always uses SHA-512 for Ed25519 and SHA-3 for Ed448.
[in] hashed_message The input message is a message digest. Ignored for EdDSA keys, and treated as false.
[in] message The message to be used to compute the signature.
[in] message_len The length of message.
[out] signature The computed signature.
[in] signature_len The length of the computed signature.
Returns
SL_STATUS_OK when the command was executed successfully, otherwise an appropiate error code (sl_status.h).

◆ sl_se_ecc_verify()

sl_status_t sl_se_ecc_verify ( sl_se_command_context_t * cmd_ctx,
const sl_se_key_descriptor_t * key,
sl_se_hash_type_t hash_alg,
bool hashed_message,
const unsigned char * message,
size_t message_len,
const unsigned char * signature,
size_t signature_len
)

This function verifies Elliptic-Curve Cryptography (ECC) digital signatures of a message.

Note
The input parameters hash_alg and hashed_message do not apply for Edwards-curve Digital Signature Algorithm (EdDSA).

P-521 Elliptic Curve for Elliptic Curve Digital Signature Algorithm (ECDSA) expects a 544 bits (68 bytes) buffer for storing private keys, and a 1088 bits (136 bytes) buffer for storing public keys and signatures. The first 23 bits of d, Qx, Qy, R and S are padding bits to comply word-aligned addressing.

Parameters
[in] cmd_ctx Pointer to an SE command context object.
[in] key Pointer to sl_se_key_descriptor_t structure.
[in] hash_alg Which hashing algorithm to use. Ignored for EdDSA keys, since EdDSA always uses SHA-512 for Ed25519 and SHA-3 for Ed448.
[in] hashed_message The input message is a message digest. Ignored for EdDSA keys, and treated as false.
[in] message The message to be used to compute signatures.
[in] message_len The length of message.
[in] signature The signature to be verified.
[in] signature_len The length of signature.
Returns
SL_STATUS_OK if the signature is successfully verified, otherwise an appropiate error code (sl_status.h).