Description

TEMPDRV error codes.

Macros

#define ECODE_EMDRV_TEMPDRV_OK ( ECODE_OK )
Success return value.
#define ECODE_EMDRV_TEMPDRV_NO_INIT ( ECODE_EMDRV_TEMPDRV_BASE | 0x00000001)
Function requires prior initialization.
#define ECODE_EMDRV_TEMPDRV_PARAM_ERROR ( ECODE_EMDRV_TEMPDRV_BASE | 0x00000002)
Illegal input parameter.
#define ECODE_EMDRV_TEMPDRV_BAD_LIMIT ( ECODE_EMDRV_TEMPDRV_BASE | 0x00000003)
Temperature mismatch with limit.
#define ECODE_EMDRV_TEMPDRV_NO_CALLBACK ( ECODE_EMDRV_TEMPDRV_BASE | 0x00000004)
Can't find callback.
#define ECODE_EMDRV_TEMPDRV_NO_SPACE ( ECODE_EMDRV_TEMPDRV_BASE | 0x00000005)
No more space to register.
#define ECODE_EMDRV_TEMPDRV_TEMP_UNDER ( ECODE_EMDRV_TEMPDRV_BASE | 0x00000006)
Requested temperature below measurable range.
#define ECODE_EMDRV_TEMPDRV_TEMP_OVER ( ECODE_EMDRV_TEMPDRV_BASE | 0x00000007)
Requested temperature above measurable range.
#define ECODE_EMDRV_TEMPDRV_DUP_TEMP ( ECODE_EMDRV_TEMPDRV_BASE | 0x00000008)
Requested temperature is a duplicate.

Macro Definition Documentation

◆ ECODE_EMDRV_TEMPDRV_OK

#define ECODE_EMDRV_TEMPDRV_OK   ( ECODE_OK )

Success return value.

◆ ECODE_EMDRV_TEMPDRV_NO_INIT

#define ECODE_EMDRV_TEMPDRV_NO_INIT   ( ECODE_EMDRV_TEMPDRV_BASE | 0x00000001)

Function requires prior initialization.

◆ ECODE_EMDRV_TEMPDRV_PARAM_ERROR

#define ECODE_EMDRV_TEMPDRV_PARAM_ERROR   ( ECODE_EMDRV_TEMPDRV_BASE | 0x00000002)

Illegal input parameter.

◆ ECODE_EMDRV_TEMPDRV_BAD_LIMIT

#define ECODE_EMDRV_TEMPDRV_BAD_LIMIT   ( ECODE_EMDRV_TEMPDRV_BASE | 0x00000003)

Temperature mismatch with limit.

◆ ECODE_EMDRV_TEMPDRV_NO_CALLBACK

#define ECODE_EMDRV_TEMPDRV_NO_CALLBACK   ( ECODE_EMDRV_TEMPDRV_BASE | 0x00000004)

Can't find callback.

◆ ECODE_EMDRV_TEMPDRV_NO_SPACE

#define ECODE_EMDRV_TEMPDRV_NO_SPACE   ( ECODE_EMDRV_TEMPDRV_BASE | 0x00000005)

No more space to register.

◆ ECODE_EMDRV_TEMPDRV_TEMP_UNDER

#define ECODE_EMDRV_TEMPDRV_TEMP_UNDER   ( ECODE_EMDRV_TEMPDRV_BASE | 0x00000006)

Requested temperature below measurable range.

◆ ECODE_EMDRV_TEMPDRV_TEMP_OVER

#define ECODE_EMDRV_TEMPDRV_TEMP_OVER   ( ECODE_EMDRV_TEMPDRV_BASE | 0x00000007)

Requested temperature above measurable range.

◆ ECODE_EMDRV_TEMPDRV_DUP_TEMP

#define ECODE_EMDRV_TEMPDRV_DUP_TEMP   ( ECODE_EMDRV_TEMPDRV_BASE | 0x00000008)

Requested temperature is a duplicate.