System Initialization and Action Processing

Description

System Initialization and Action Processing.

System Init

System Init provides a function for initializing the system and the products:

This function calls a set of functions that are automatically generated and located in autogen/sl_event_handler.c . Handlers can be registered for the following events using the Event Handler API provided by the Event Handler component:

  • platform_init -> sl_platform_init()
  • driver_init -> sl_driver_init()
  • service_init -> sl_service_init()
  • stack_init -> sl_stack_init()
  • internal_app_init -> sl_internal_app_init()

These events are fired in the order listed above when sl_system_init() is called.

System Kernel

System Kernel component provides a function for starting the kernel:

This function calls a functions that is automatically generated and located in $autogen/sl_event_handler.c . Handlers can be registered for the following events using the Event Handler API provided by the Event Handler component:

  • kernel_start -> sl_kernel_start()

The event is fired when sl_system_kernel_start() is called.

System Process Action

System Process Action component provides a function for running the products from a super loop:

This function calls a set of functions that are automatically generated and located in $autogen/sl_event_handler.c . Handlers can be registered for the following events using the Event Handler API provided by the Event Handler component:

  • platform_process_action -> sl_platform_process_action()
  • service_process_action -> sl_service_process_action()
  • stack_process_action -> sl_stack_process_action()
  • internal_app_process_action -> sl_internal_process_action()

These events are fired in the order listed above when sl_system_process_action() is called.

Usage example:

#if defined(SL_COMPONENT_CATALOG_PRESENT)
#include "sl_component_catalog.h"
#endif
#include "sl_system_init.h"
#include "sl_power_manager.h"
#include "app.h"
#if defined(SL_CATALOG_KERNEL_PRESENT)
#include "sl_system_kernel.h"
#else
#include "sl_system_process_action.h"
#endif
int main( void )
{
// Initialize Silicon Labs device, system, service(s) and protocol stack(s).
// Note that if the kernel is present, processing task(s) will be created by
// this call.
// Initialize the application.
app_init();
#if defined(SL_CATALOG_KERNEL_PRESENT)
// Start the kernel. Task(s) created in app_init() will start running.
#else
do {
// Do not remove this call: Silicon Labs components process action routine
// must be called from the super loop.
// Application process.
app_process_action();
// Let the CPU go to sleep if the system allow it.
} while (1);
#endif // SL_CATALOG_KERNEL_PRESENT
}

Functions

void sl_system_process_action (void)
System processing action.
void sl_system_kernel_start (void)
Start the kernel.
void sl_system_init (void)
Initialize Silicon Labs products.

Function Documentation

◆ sl_system_process_action()

void sl_system_process_action ( void )

System processing action.

◆ sl_system_kernel_start()

void sl_system_kernel_start ( void )

Start the kernel.

◆ sl_system_init()

void sl_system_init ( void )

Initialize Silicon Labs products.