USB_EndpointDescriptor_TypeDef Struct Reference

USB Endpoint Descriptor.

#include <em_usb.h>

Data Fields

uint8_t bLength
Size of this descriptor in bytes

uint8_t bDescriptorType
Constant ENDPOINT Descriptor Type

uint8_t bEndpointAddress
The address of the endpoint

uint8_t bmAttributes
This field describes the endpoint attributes

uint16_t wMaxPacketSize
Maximum packet size for the endpoint

uint8_t bInterval
Interval for polling EP for data transfers

USB Endpoint Descriptor.

Field Documentation

bLength

uint8_t USB_EndpointDescriptor_TypeDef::bLength

Size of this descriptor in bytes

bDescriptorType

uint8_t USB_EndpointDescriptor_TypeDef::bDescriptorType

Constant ENDPOINT Descriptor Type

bEndpointAddress

uint8_t USB_EndpointDescriptor_TypeDef::bEndpointAddress

The address of the endpoint

bmAttributes

uint8_t USB_EndpointDescriptor_TypeDef::bmAttributes

This field describes the endpoint attributes

wMaxPacketSize

uint16_t USB_EndpointDescriptor_TypeDef::wMaxPacketSize

Maximum packet size for the endpoint

bInterval

uint8_t USB_EndpointDescriptor_TypeDef::bInterval

Interval for polling EP for data transfers