Description

Macros

#define ECODE_EMDRV_DMADRV_OK ( ECODE_OK )
A successful return value.
#define ECODE_EMDRV_DMADRV_PARAM_ERROR ( ECODE_EMDRV_DMADRV_BASE | 0x00000001)
An illegal input parameter.
#define ECODE_EMDRV_DMADRV_NOT_INITIALIZED ( ECODE_EMDRV_DMADRV_BASE | 0x00000002)
DMA is not initialized.
#define ECODE_EMDRV_DMADRV_ALREADY_INITIALIZED ( ECODE_EMDRV_DMADRV_BASE | 0x00000003)
DMA has already been initialized.
#define ECODE_EMDRV_DMADRV_CHANNELS_EXHAUSTED ( ECODE_EMDRV_DMADRV_BASE | 0x00000004)
No DMA channels available.
#define ECODE_EMDRV_DMADRV_IN_USE ( ECODE_EMDRV_DMADRV_BASE | 0x00000005)
DMA is in use.
#define ECODE_EMDRV_DMADRV_ALREADY_FREED ( ECODE_EMDRV_DMADRV_BASE | 0x00000006)
A DMA channel was free.
#define ECODE_EMDRV_DMADRV_CH_NOT_ALLOCATED ( ECODE_EMDRV_DMADRV_BASE | 0x00000007)
A channel is not reserved.

Macro Definition Documentation

◆ ECODE_EMDRV_DMADRV_OK

#define ECODE_EMDRV_DMADRV_OK   ( ECODE_OK )

A successful return value.

◆ ECODE_EMDRV_DMADRV_PARAM_ERROR

#define ECODE_EMDRV_DMADRV_PARAM_ERROR   ( ECODE_EMDRV_DMADRV_BASE | 0x00000001)

An illegal input parameter.

◆ ECODE_EMDRV_DMADRV_NOT_INITIALIZED

#define ECODE_EMDRV_DMADRV_NOT_INITIALIZED   ( ECODE_EMDRV_DMADRV_BASE | 0x00000002)

DMA is not initialized.

◆ ECODE_EMDRV_DMADRV_ALREADY_INITIALIZED

#define ECODE_EMDRV_DMADRV_ALREADY_INITIALIZED   ( ECODE_EMDRV_DMADRV_BASE | 0x00000003)

DMA has already been initialized.

◆ ECODE_EMDRV_DMADRV_CHANNELS_EXHAUSTED

#define ECODE_EMDRV_DMADRV_CHANNELS_EXHAUSTED   ( ECODE_EMDRV_DMADRV_BASE | 0x00000004)

No DMA channels available.

◆ ECODE_EMDRV_DMADRV_IN_USE

#define ECODE_EMDRV_DMADRV_IN_USE   ( ECODE_EMDRV_DMADRV_BASE | 0x00000005)

DMA is in use.

◆ ECODE_EMDRV_DMADRV_ALREADY_FREED

#define ECODE_EMDRV_DMADRV_ALREADY_FREED   ( ECODE_EMDRV_DMADRV_BASE | 0x00000006)

A DMA channel was free.

◆ ECODE_EMDRV_DMADRV_CH_NOT_ALLOCATED

#define ECODE_EMDRV_DMADRV_CH_NOT_ALLOCATED   ( ECODE_EMDRV_DMADRV_BASE | 0x00000007)

A channel is not reserved.