Description

Macros

#define ECODE_EMDRV_SPIDRV_OK ( ECODE_OK )
A successful return value.
#define ECODE_EMDRV_SPIDRV_ILLEGAL_HANDLE ( ECODE_EMDRV_SPIDRV_BASE | 0x00000001)
An illegal SPI handle.
#define ECODE_EMDRV_SPIDRV_PARAM_ERROR ( ECODE_EMDRV_SPIDRV_BASE | 0x00000002)
An illegal input parameter.
#define ECODE_EMDRV_SPIDRV_BUSY ( ECODE_EMDRV_SPIDRV_BASE | 0x00000003)
The SPI port is busy.
#define ECODE_EMDRV_SPIDRV_TIMER_ALLOC_ERROR ( ECODE_EMDRV_SPIDRV_BASE | 0x00000004)
Unable to allocate timeout timer.
#define ECODE_EMDRV_SPIDRV_TIMEOUT ( ECODE_EMDRV_SPIDRV_BASE | 0x00000005)
An SPI transfer timeout.
#define ECODE_EMDRV_SPIDRV_IDLE ( ECODE_EMDRV_SPIDRV_BASE | 0x00000006)
No SPI transfer in progress.
#define ECODE_EMDRV_SPIDRV_ABORTED ( ECODE_EMDRV_SPIDRV_BASE | 0x00000007)
An SPI transfer has been aborted.
#define ECODE_EMDRV_SPIDRV_MODE_ERROR ( ECODE_EMDRV_SPIDRV_BASE | 0x00000008)
SPI master used slave API or vica versa.
#define ECODE_EMDRV_SPIDRV_DMA_ALLOC_ERROR ( ECODE_EMDRV_SPIDRV_BASE | 0x00000009)
Unable to allocate DMA channels.

Macro Definition Documentation

◆ ECODE_EMDRV_SPIDRV_OK

#define ECODE_EMDRV_SPIDRV_OK   ( ECODE_OK )

A successful return value.

◆ ECODE_EMDRV_SPIDRV_ILLEGAL_HANDLE

#define ECODE_EMDRV_SPIDRV_ILLEGAL_HANDLE   ( ECODE_EMDRV_SPIDRV_BASE | 0x00000001)

An illegal SPI handle.

◆ ECODE_EMDRV_SPIDRV_PARAM_ERROR

#define ECODE_EMDRV_SPIDRV_PARAM_ERROR   ( ECODE_EMDRV_SPIDRV_BASE | 0x00000002)

An illegal input parameter.

◆ ECODE_EMDRV_SPIDRV_BUSY

#define ECODE_EMDRV_SPIDRV_BUSY   ( ECODE_EMDRV_SPIDRV_BASE | 0x00000003)

The SPI port is busy.

◆ ECODE_EMDRV_SPIDRV_TIMER_ALLOC_ERROR

#define ECODE_EMDRV_SPIDRV_TIMER_ALLOC_ERROR   ( ECODE_EMDRV_SPIDRV_BASE | 0x00000004)

Unable to allocate timeout timer.

◆ ECODE_EMDRV_SPIDRV_TIMEOUT

#define ECODE_EMDRV_SPIDRV_TIMEOUT   ( ECODE_EMDRV_SPIDRV_BASE | 0x00000005)

An SPI transfer timeout.

◆ ECODE_EMDRV_SPIDRV_IDLE

#define ECODE_EMDRV_SPIDRV_IDLE   ( ECODE_EMDRV_SPIDRV_BASE | 0x00000006)

No SPI transfer in progress.

◆ ECODE_EMDRV_SPIDRV_ABORTED

#define ECODE_EMDRV_SPIDRV_ABORTED   ( ECODE_EMDRV_SPIDRV_BASE | 0x00000007)

An SPI transfer has been aborted.

◆ ECODE_EMDRV_SPIDRV_MODE_ERROR

#define ECODE_EMDRV_SPIDRV_MODE_ERROR   ( ECODE_EMDRV_SPIDRV_BASE | 0x00000008)

SPI master used slave API or vica versa.

◆ ECODE_EMDRV_SPIDRV_DMA_ALLOC_ERROR

#define ECODE_EMDRV_SPIDRV_DMA_ALLOC_ERROR   ( ECODE_EMDRV_SPIDRV_BASE | 0x00000009)

Unable to allocate DMA channels.