|
|
|
void
|
emberZclResetAttributes
(
EmberZclEndpointId_t
endpointId)
|
|
|
|
EmberZclStatus_t
|
emberZclReadAttribute
(
EmberZclEndpointId_t
endpointId, const
EmberZclClusterSpec_t
*clusterSpec,
EmberZclAttributeId_t
attributeId, void *buffer, size_t bufferLength)
|
|
|
|
EmberZclStatus_t
|
emberZclWriteAttribute
(
EmberZclEndpointId_t
endpointId, const
EmberZclClusterSpec_t
*clusterSpec,
EmberZclAttributeId_t
attributeId, const void *buffer, size_t bufferLength)
|
|
|
|
EmberZclStatus_t
|
emberZclExternalAttributeChanged
(
EmberZclEndpointId_t
endpointId, const
EmberZclClusterSpec_t
*clusterSpec,
EmberZclAttributeId_t
attributeId, const void *buffer, size_t bufferLength)
|
|
|
|
EmberStatus
|
emberZclSendAttributeRead
(const
EmberZclDestination_t
*destination, const
EmberZclClusterSpec_t
*clusterSpec, const
EmberZclAttributeId_t
*attributeIds, size_t attributeIdsCount, const
EmberZclReadAttributeResponseHandler
handler
)
|
|
|
|
EmberStatus
|
emberZclSendAttributeWrite
(const
EmberZclDestination_t
*destination, const
EmberZclClusterSpec_t
*clusterSpec, const
EmberZclAttributeWriteData_t
*attributeWriteData, size_t attributeWriteDataCount, const
EmberZclWriteAttributeResponseHandler
handler
)
|
See
zcl-core-types.h
for source code.
See
zcl-core.h
for source code.
|
#define EMBER_ZCL_ATTRIBUTE_CLUSTER_REVISION 0xFFFD
|
An attribute identifier for the Cluster revision.
A distinguished value that represents a null (invalid) attribute identifier.
|
#define EMBER_ZCL_ATTRIBUTE_REPORTING_STATUS 0xFFFE
|
An attribute identifier for a Reporting status.
A distinguished value that represents a null (invalid) cluster revision.
|
#define EMBER_ZCL_CLUSTER_REVISION_PRE_ZCL6 0
|
A cluster revision for Pre-ZCL 6 specification.
|
#define EMBER_ZCL_CLUSTER_REVISION_ZCL6 1
|
A cluster revision for ZCL 6 specification.
A handler fired when reading attributes.
-
Parameters
-
status
|
A message status
|
context
|
A context of a read attribute
|
buffer
|
A content of a read attribute
|
bufferLength
|
Content length
|
-
Note
-
context->status
shows whether attribute was read successfully or if an error occured. If successful, a buffer contains an attribute value. If unsuccessful, the buffer is irrelevant.
-
See also
-
emberZclSendAttributeRead()
A handler fired when writing attributes.
-
Parameters
-
status
|
A message status
|
context
|
A context of a written attribute
|
-
Note
-
context->status
shows whether attribute was written successfully or if an error occured.
-
See also
-
emberZclSendAttributeWrite()
This function notifies the core code that an externally stored attribute has changed.
-
Parameters
-
endpointId
|
An endpoint identifier of the attribute
|
clusterSpec
|
A cluster specification of the attribute
|
attributeId
|
An attribute identifier that is changed
|
buffer
|
A buffer to write the attribute from
|
bufferLength
|
Length of the write buffer
|
-
Returns
-
-
Note
-
emberZclPostAttributeChangeCallback
is triggered for a successful call to this function.
This function reads the value of an attibute.
-
Parameters
-
endpointId
|
An endpoint identifier of the attribute
|
clusterSpec
|
A cluster specification of the attribute
|
attributeId
|
An attribute identifier to read
|
buffer
|
A buffer to read the attribute into
|
bufferLength
|
Length of the read buffer
|
-
Returns
-
-
Note
-
emberZclReadExternalAttributeCallback
is triggered if attribute is externally stored. If so, the result of that call is returned.
This function resets all local attributes on given endpoint.
-
Parameters
-
endpointId
|
An endpoint identifier
|
-
Note
-
emberZclPostAttributeChangeCallback
is triggered after each attribute is changed.
This function sends an attribute read command to a specified destination.
-
Parameters
-
destination
|
A location to read the attribute from
|
clusterSpec
|
A cluster specification of the attribute
|
attributeIds
|
An array of attribute IDs to read
|
attributeIdsCount
|
A total count of
EmberZclAttributeId_t
elements in a passed array
|
handler
|
callback that is triggered for a response
|
-
Returns
-
-
See also
-
EmberZclReadAttributeResponseHandler()
This function sends an attribute write command to a specified destination.
-
Parameters
-
destination
|
A location to write the attribute to
|
clusterSpec
|
A cluster specification of the attribute
|
attributeWriteData
|
An array containing write data for attributes
|
attributeWriteDataCount
|
A total count of
EmberZclAttributeWriteData_t
elements in a passed array
|
handler
|
A callback that is triggered for a response
|
-
Returns
-
-
See also
-
EmberZclWriteAttributeResponseHandler()
This function writes the value of an attibute.
-
Parameters
-
endpointId
|
An endpoint identifier of the attribute
|
clusterSpec
|
A cluster specification of the attribute
|
attributeId
|
An attribute identifier to write
|
buffer
|
A buffer to write the attribute from
|
bufferLength
|
Length of the write buffer
|
-
Returns
-
-
Note
-
emberZclWriteExternalAttributeCallback
is triggered if the attribute is externally stored. If so, the result of that call is returned.
-
emberZclPostAttributeChangeCallback
is triggered after the attribute is successfully changed.