See
zcl-core-types.h
for source code.
|
#define EMBER_ZCL_LONG_STRING_LENGTH_INVALID 0xFFFF
|
Invalid long string length.
|
#define EMBER_ZCL_LONG_STRING_LENGTH_MAX 0xFFFE
|
Maximum long string length.
|
#define EMBER_ZCL_LONG_STRING_OVERHEAD 2
|
|
#define EMBER_ZCL_STRING_LENGTH_INVALID 0xFF
|
|
#define EMBER_ZCL_STRING_LENGTH_MAX 0xFE
|
|
#define EMBER_ZCL_STRING_OVERHEAD 1
|
|
#define EMBER_ZCL_URI_MAX_LENGTH 120
|
The longest ZCL/IP URI is: coaps://nih:sha-256;<uid>:PPPPP/zcl/g/GGGG/RMMMM_CCCC/a/AAAA where <uid> is a 256-bit UID represented as 64 hexadecimal characters, PPPPP is a 16-bit UDP port in decimal, GGGG is the 16-bit group ID in hexadecimal, R is c or s for client or server, MMMM is the 16-bit manufacturer code in hexadecimal, CCCC is the 16-bit cluster ID in hexadecimal, and AAAA is the 16-bit attribute ID in hexadecimal. An extra byte is reserved for a null terminator.
|
#define EMBER_ZCL_URI_PATH_CLUSTER_ID_MAX_LENGTH 11
|
The longest cluster ID in a ZCL/IP URI path is manufacturer-specific: RMMMM_CCCC where R is c or s for client or server, MMMM is the 16-bit manufacturer code, and CCCC is the 16-bit cluster ID. An extra byte is reserved for a null terminator.
|
#define EMBER_ZCL_URI_PATH_MANUFACTURER_CODE_CLUSTER_ID_SEPARATOR '_'
|
Manufacturer codes, if present, are separated from the cluster ID by an underscore.
|
#define EMBER_ZCL_URI_PATH_MAX_LENGTH 29
|
The longest ZCL/IP URI path is a manufacturer-specific attribute request sent to a group: zcl/g/GGGG/RMMMM_CCCC/a/AAAA where GGGG is the 16-bit group ID, R is c or s for client or server, MMMM is the 16-bit manufacturer code, CCCC is the 16-bit cluster ID, and AAAA is the 16-bit attribute ID. An extra byte is reserved for a null terminator.
|
uint16_t emberZclLongStringLength
|
(
|
const uint8_t *
|
buffer
|
)
|
|
This function returns the length of the octet or character data in a given long string.
-
Parameters
-
-
Returns
-
length of string
|
uint16_t emberZclLongStringSize
|
(
|
const uint8_t *
|
buffer
|
)
|
|
This function returns the size of a given long string including overhead and data.
-
Parameters
-
-
Returns
-
size of string
|
uint8_t emberZclStringLength
|
(
|
const uint8_t *
|
buffer
|
)
|
|
This function returns the length of the octet or character data in a given string.
-
Parameters
-
-
Returns
-
length of string
|
uint8_t emberZclStringSize
|
(
|
const uint8_t *
|
buffer
|
)
|
|
This function returns the size of a given string including overhead and data.
-
Parameters
-
-
Returns
-
size of string