Structure to hold information about an 802.15.4 beacon for use on the application.
#include <
network-management.h
>
|
bool EmberMacBeaconData::allowingJoin
|
|
uint8_t EmberMacBeaconData::channel
|
|
uint8_t EmberMacBeaconData::extendedPanId[8]
|
|
uint8_t EmberMacBeaconData::longId[8]
|
|
uint8_t EmberMacBeaconData::lqi
|
|
uint8_t EmberMacBeaconData::networkId[16]
|
|
uint16_t EmberMacBeaconData::panId
|
|
uint8_t EmberMacBeaconData::protocolId
|
|
int8_t EmberMacBeaconData::rssi
|
|
uint16_t EmberMacBeaconData::shortId
|
|
uint8_t EmberMacBeaconData::steeringData[16]
|
|
uint8_t EmberMacBeaconData::steeringDataLength
|
|
uint8_t EmberMacBeaconData::version
|
The documentation for this struct was generated from the following file: