Sample API functions for playing tunes on a piezo buzzer.
Functions |
|
| void | halPlayTune_P (uint8_t PGM *tune, bool bkg) |
|
Plays a tune on the piezo buzzer.
|
|
| void | halStackIndicatePresence (void) |
|
Causes something to happen on a node (such as playing a tune on the buzzer) that can be used to indicate where it physically is.
|
|
Note Definitions |
|
|
Flats are used instead of sharps because # is a special character. |
|
| #define | NOTE_C3 119 |
|
A note which can be used in tune structure definitions.
|
|
| #define | NOTE_Db3 112 |
|
A note which can be used in tune structure definitions.
|
|
| #define | NOTE_D3 106 |
|
A note which can be used in tune structure definitions.
|
|
| #define | NOTE_Eb3 100 |
|
A note which can be used in tune structure definitions.
|
|
| #define | NOTE_E3 94 |
|
A note which can be used in tune structure definitions.
|
|
| #define | NOTE_F3 89 |
|
A note which can be used in tune structure definitions.
|
|
| #define | NOTE_Gb3 84 |
|
A note which can be used in tune structure definitions.
|
|
| #define | NOTE_G3 79 |
|
A note which can be used in tune structure definitions.
|
|
| #define | NOTE_Ab3 74 |
|
A note which can be used in tune structure definitions.
|
|
| #define | NOTE_A3 70 |
|
A note which can be used in tune structure definitions.
|
|
| #define | NOTE_Bb3 66 |
|
A note which can be used in tune structure definitions.
|
|
| #define | NOTE_B3 63 |
|
A note which can be used in tune structure definitions.
|
|
| #define | NOTE_C4 59 |
|
A note which can be used in tune structure definitions.
|
|
| #define | NOTE_Db4 55 |
|
A note which can be used in tune structure definitions.
|
|
| #define | NOTE_D4 52 |
|
A note which can be used in tune structure definitions.
|
|
| #define | NOTE_Eb4 49 |
|
A note which can be used in tune structure definitions.
|
|
| #define | NOTE_E4 46 |
|
A note which can be used in tune structure definitions.
|
|
| #define | NOTE_F4 44 |
|
A note which can be used in tune structure definitions.
|
|
| #define | NOTE_Gb4 41 |
|
A note which can be used in tune structure definitions.
|
|
| #define | NOTE_G4 39 |
|
A note which can be used in tune structure definitions.
|
|
| #define | NOTE_Ab4 37 |
|
A note which can be used in tune structure definitions.
|
|
| #define | NOTE_A4 35 |
|
A note which can be used in tune structure definitions.
|
|
| #define | NOTE_Bb4 33 |
|
A note which can be used in tune structure definitions.
|
|
| #define | NOTE_B4 31 |
|
A note which can be used in tune structure definitions.
|
|
| #define | NOTE_C5 29 |
|
A note which can be used in tune structure definitions.
|
|
| #define | NOTE_Db5 27 |
|
A note which can be used in tune structure definitions.
|
|
| #define | NOTE_D5 26 |
|
A note which can be used in tune structure definitions.
|
|
| #define | NOTE_Eb5 24 |
|
A note which can be used in tune structure definitions.
|
|
| #define | NOTE_E5 23 |
|
A note which can be used in tune structure definitions.
|
|
| #define | NOTE_F5 21 |
|
A note which can be used in tune structure definitions.
|
|
| #define | NOTE_Gb5 20 |
|
A note which can be used in tune structure definitions.
|
|
| #define | NOTE_G5 19 |
|
A note which can be used in tune structure definitions.
|
|
| #define | NOTE_Ab5 18 |
|
A note which can be used in tune structure definitions.
|
|
| #define | NOTE_A5 17 |
|
A note which can be used in tune structure definitions.
|
|
| #define | NOTE_Bb5 16 |
|
A note which can be used in tune structure definitions.
|
|
| #define | NOTE_B5 15 |
|
A note which can be used in tune structure definitions.
|
|
Detailed Description
See
buzzer.h
for source code.
Macro Definition Documentation
| #define NOTE_A3 70 |
| #define NOTE_A4 35 |
| #define NOTE_A5 17 |
| #define NOTE_Ab3 74 |
| #define NOTE_Ab4 37 |
| #define NOTE_Ab5 18 |
| #define NOTE_B3 63 |
| #define NOTE_B4 31 |
| #define NOTE_B5 15 |
| #define NOTE_Bb3 66 |
| #define NOTE_Bb4 33 |
| #define NOTE_Bb5 16 |
| #define NOTE_C3 119 |
| #define NOTE_C4 59 |
| #define NOTE_C5 29 |
| #define NOTE_D3 106 |
| #define NOTE_D4 52 |
| #define NOTE_D5 26 |
| #define NOTE_Db3 112 |
| #define NOTE_Db4 55 |
| #define NOTE_Db5 27 |
| #define NOTE_E3 94 |
| #define NOTE_E4 46 |
| #define NOTE_E5 23 |
| #define NOTE_Eb3 100 |
| #define NOTE_Eb4 49 |
| #define NOTE_Eb5 24 |
| #define NOTE_F3 89 |
| #define NOTE_F4 44 |
| #define NOTE_F5 21 |
| #define NOTE_G3 79 |
| #define NOTE_G4 39 |
| #define NOTE_G5 19 |
| #define NOTE_Gb3 84 |
| #define NOTE_Gb4 41 |
| #define NOTE_Gb5 20 |
Function Documentation
| void halPlayTune_P | ( | uint8_t PGM * |
tune,
|
| bool |
bkg
|
||
| ) |
The tune is played in the background if ::bkg is true. Otherwise, the API blocks until the playback of the tune is complete. halPlayTune_P() is not meant to be called back-to-back.
- Parameters
-
tuneA pointer to tune to play. bkgDetermines whether the tune plays in the background. If true, tune plays in background; if false, tune plays in foreground.
A tune is implemented as follows:
| void halStackIndicatePresence | ( | void |
|
) |