Identify Server Callbacks
Functions |
|
| void | emberZclIdentifyServerStartIdentifyingCallback ( EmberZclEndpointId_t endpointId, uint16_t identifyTimeS) |
|
Start Identifying.
|
|
| void | emberZclIdentifyServerStopIdentifyingCallback ( EmberZclEndpointId_t endpointId) |
|
Stop Identifying.
|
|
Detailed Description
These callbacks are contributed by the Identify Server plugin.
Function Documentation
| void emberZclIdentifyServerStartIdentifyingCallback | ( | EmberZclEndpointId_t |
endpointId,
|
| uint16_t |
identifyTimeS
|
||
| ) |
This function is called when the device should start identifying. The device should continue to identify until emberZclIdentifyServerStopIdentifyingCallback is called.
| void emberZclIdentifyServerStopIdentifyingCallback | ( | EmberZclEndpointId_t |
endpointId
|
) |
This function is called when the device should stop identifying.