EmberChildEntry Struct Reference
#include <
network-management.h
>
Data Fields |
|
| uint16_t | flags |
| uint8_t | macExtendedId [8] |
| uint32_t | timeoutSeconds |
| uint16_t | secondsSinceLastTransaction |
| int8_t | rssi |
Field Documentation
| uint16_t EmberChildEntry::flags |
| uint8_t EmberChildEntry::macExtendedId[8] |
| int8_t EmberChildEntry::rssi |
| uint16_t EmberChildEntry::secondsSinceLastTransaction |
| uint32_t EmberChildEntry::timeoutSeconds |
The documentation for this struct was generated from the following file:
-
network-management.h