Bulb PWM Driver Callbacks
Functions |
|
| uint16_t | halBulbPwmDriverFrequencyCallback (void) |
|
A callback used to configure the frequency of the PWM driver. This is called by the bulb-pwm driver upon initialization to determine the frequency at which the PWM driver should be driven. It should return either the frequency, in Hz, or USE_DEFAULT_FREQUENCY to indicate that the plugin should use the default value. The default value is 1000 Hz, but can be overridden by a macro in the board header if a user wishes.
|
|
| void | halBulbPwmDriverInitCompleteCallback (void) |
|
Function to indicate that the PWM driver has been initialized and the bulb should drive the initial LED PWM values at this time.
|
|
| void | halBulbPwmDriverBlinkOnCallback (void) |
|
This callback is generated during blinking behavior when it is time to turn the bulb on. While the plugin will determine when to blink the bulb on or off, it is up to this callback to determine how to turn the bulb on.
|
|
| void | halBulbPwmDriverBlinkOffCallback (void) |
|
This callback is generated during blinking behavior when it is time to turn the bulb off. While the plugin will determine when to blink the bulb on or off, it is up to this callback to determine how to turn the bulb off.
|
|
| void | halBulbPwmDriverBlinkStartCallback (void) |
|
This callback is generated when the application layer makes a call to initiate blinking behavior. It warns the application layer PWM code to not attempt to drive the LEDs directly and interfere with the blinking behavior.
|
|
| void | halBulbPwmDriverBlinkStopCallback (void) |
|
This callback is generated when the current blinking command finishes. The application layer PWM code must then determine what the bulb drive should be, based on the current appliation layer attributes (i.e. level, on/off, color XY, etc.)
|
|
Detailed Description
These callbacks are contributed by the Bulb PWM Driver plugin.
Function Documentation
| void halBulbPwmDriverBlinkOffCallback | ( | void |
|
) |
Should be implemented by an application layer configuration plugin.
| void halBulbPwmDriverBlinkOnCallback | ( | void |
|
) |
Should be implemented by an application layer configuration plugin.
| void halBulbPwmDriverBlinkStartCallback | ( | void |
|
) |
Should be implemented by an application layer configuration plugin.
| void halBulbPwmDriverBlinkStopCallback | ( | void |
|
) |
Should be implemented by an application layer configuration plugin.
| uint16_t halBulbPwmDriverFrequencyCallback | ( | void |
|
) |
Should be implemented by an application layer configuration plugin.
| void halBulbPwmDriverInitCompleteCallback | ( | void |
|
) |
Should be implemented by an application layer configuration plugin.