The command interpreter.
|
|
|
struct
|
EmberCommandEntry
|
|
|
Command entry for a command table.
|
|
|
|
struct
|
EmberCommandState
|
|
|
For use when declaring a separate command streams. The fields are not accessed directly by the application.
|
|
|
|
#define
|
MAX_TOKEN_COUNT
(
EMBER_MAX_COMMAND_ARGUMENTS
+ 1)
|
|
|
|
#define
|
MAX_COMMAND_TABLE_NESTING
16
|
|
|
|
#define
|
emberBinaryCommand
emberBinaryCommandEntryAction
|
|
|
|
#define
|
emberBinaryNestedCommand
emberBinaryCommandEntrySubMenu
|
|
|
|
#define
|
emberBinaryCommandEntryAction
(identifier, command, arguments, description) { { (PGM_P)identifier }, command, arguments, description }
|
|
|
|
#define
|
emberBinaryCommandEntrySubMenu
(identifier, nestedCommands, description) { { (PGM_P)identifier },
NULL
, description, nestedCommands }
|
|
|
|
#define
|
emberCommandEntryAction
(name, command, arguments, description) { { name }, command, arguments, description }
|
|
|
|
#define
|
emberCommandEntrySubMenu
(name, nestedCommands, description) { { name },
NULL
, (PGM_P)nestedCommands, description }
|
|
|
|
#define
|
emberCommandEntryTerminator
() { {
NULL
},
NULL
,
NULL
,
NULL
}
|
|
|
|
#define
|
emberCommand
emberCommandEntryAction
|
|
|
|
#define
|
emberNestedCommand
emberCommandEntrySubMenu
|
|
|
|
#define
|
emberProcessCommandInput
(port)
emberProcessCommandString
(
NULL
, port)
|
|
|
This function processes input coming in on the given serial port.
|
|
|
|
void
|
emberCommandErrorHandler
(
EmberCommandStatus
status,
EmberCommandEntry
*command)
|
|
|
|
void
|
emberPrintCommandUsage
(
EmberCommandEntry
*entry)
|
|
|
|
void
|
emberPrintCommandUsageNotes
(void)
|
|
|
|
void
|
emberPrintCommandTable
(void)
|
|
|
|
void
|
emberCommandClearBuffer
(void)
|
|
|
|
void
|
emberCommandReaderInit
(void)
|
|
|
This function initializes the command interpreter.
|
|
|
|
bool
|
emberProcessCommandString
(const uint8_t *input, uint16_t sizeOrPort)
|
|
|
This function processes the given string as a command.
|
|
|
|
void
|
emberInitializeCommandState
(
EmberCommandState
*state)
|
|
|
This function must be called to initialize a command state before passing it to
emberRunBinaryCommandInterpreter()
or
emberRunAsciiCommandInterpreter()
.
|
|
|
|
bool
|
emberRunBinaryCommandInterpreter
(
EmberCommandState
*state,
EmberCommandEntry
*commands,
EmberCommandErrorHandler
*errorHandler, const uint8_t *input, uint16_t sizeOrPort)
|
|
|
For use to process binary commands when additional different command streams are being used.
|
|
|
|
bool
|
emberRunAsciiCommandInterpreter
(
EmberCommandState
*state,
EmberCommandEntry
*commands,
EmberCommandErrorHandler
*errorHandler, const uint8_t *input, uint16_t sizeOrPort)
|
|
|
For use to process ASCII commands when additional different command streams are being used.
|
|
|
|
void
|
emberCommandReaderSetDefaultBase
(uint8_t base)
|
|
|
|
Use the following functions in your functions that process commands to retrieve arguments from the command interpreter. These functions pull out unsigned integers, signed integers, and strings, and hex strings. Index 0 is the first command argument.
|
|
uint8_t
|
emberCommandArgumentCount
(void)
|
|
|
|
uint32_t
|
emberUnsignedCommandArgument
(uint8_t argNum)
|
|
|
|
int32_t
|
emberSignedCommandArgument
(uint8_t argNum)
|
|
|
|
uint8_t *
|
emberStringCommandArgument
(int8_t argNum, uint8_t *length)
|
|
|
|
uint8_t *
|
emberLongStringCommandArgument
(int8_t argNum, uint16_t *length)
|
|
|
|
const char *
|
emberCommandName
(void)
|
|
|
|
uint8_t
|
emberGetStringArgument
(int8_t argNum, uint8_t *destination, uint8_t maxLength, bool leftPad)
|
|
|
|
bool
|
emberGetIpArgument
(uint8_t index, uint8_t *target)
|
|
|
|
bool
|
emberGetIpv6AddressArgument
(uint8_t index,
EmberIpv6Address
*dst)
|
|
|
This function parses an IPv6 address in a CLI command.
|
|
|
|
bool
|
emberGetIpv6PrefixArgument
(uint8_t index,
EmberIpv6Address
*dst, uint8_t *dstPrefixBits)
|
|
|
This function parses an IPv6 prefix in a CLI command.
|
|
|
|
void
|
emberGetExtendedPanIdArgument
(int8_t index, uint8_t *extendedPanId)
|
|
|
|
#define
|
emberGetKeyArgument
(index, keyDataPointer)
|
|
|
|
#define
|
emberGetEui64Argument
(index, eui64)
emberGetExtendedPanIdArgument
(index, (eui64)->bytes)
|
Processes commands coming from the serial port.
Interpret serial port commands. See command-interpreter2.c for source code.
See the following application usage example followed by a brief explanation.
1
// Usage: network form 22 0xAB12 -3 { 00 01 02 A3 A4 A5 A6 A7 }
4
uint8_t channel = emberUnsignedCommandArgument(0);
5
uint16_t panId = emberUnsignedCommandArgument(1);
6
int8_t power = emberSignedCommandArgument(2);
8
uint8_t *eui64 = emberStringCommandArgument(3, &length);
10
... call emberFormNetwork() etc
14
// The table of network commands.
15
EmberCommandEntry networkCommands[] = {
16
emberCommandEntryAction("form", formCommand, "uvsh", "Form a network"),
17
emberCommandEntryAction("join", joinCommand, "uvsh", "join a network"),
19
emberCommandEntryTerminator()
22
EmberCommandEntry systemCommands[] = {
23
emberCommandEntrySubMenu("network", networkCommands, "Network form/join commands"),
25
emberCommandEntryTerminator()
28
// The main command table. A SubMenu with an empty command name processes
29
// the commands in the subtable as if they were in the main table.
30
EmberCommandEntry emberCommandTable[] = {
31
emberCommandEntrySubMenu("", systemCommands, ""),
32
emberCommandEntryAction("status", statusCommand, "Prints application status),
34
emberCommandEntryTerminator()
39
emberCommandReaderInit();
42
// Process input and print prompt if it returns true.
43
if (emberProcessCommandInput(serialPort)) {
44
emberSerialPrintf(1, "%p>", PROMPT);
-
Applications specify the commands that can be interpreted by defining the emberCommandTable array of type
EmberCommandEntry
. The table includes the following information for each command:
-
The full command name.
-
Your application's function name that implements the command.
-
An
EmberCommandEntry::argumentTypes
string specifies the number and types of arguments the command accepts. See ::argumentTypes for details.
-
A description string explains the command.
-
A default error handler
emberCommandErrorHandler()
is provided to deal with incorrect command input. Applications may override it.
-
The application calls
emberCommandReaderInit()
to initalize, and
emberProcessCommandInput()
in its main loop.
-
Within the application's command functions, use emberXXXCommandArgument() functions to retrieve command arguments.
The command interpreter does extensive processing and validation of the command input before calling the function that implements the command. It checks that the number, type, syntax, and range of all arguments are correct. It performs any conversions necessary (for example, converting integers and strings input in hexadecimal notation into the corresponding bytes), so that no additional parsing is necessary within command functions. If there is an error in the command input,
emberCommandErrorHandler()
is called rather than a command function.
The command interpreter allows inexact matches of command names. The input command may be either shorter or longer than the actual command. However, if more than one inexact match is found and there is no exact match, an error of type EMBER_CMD_ERR_NO_SUCH_COMMAND will be generated. To disable this feature, define EMBER_REQUIRE_EXACT_COMMAND_NAME in the application configuration header.
|
#define EMBER_COMMAND_BUFFER_LENGTH 100
|
The maximum number of arguments a command can have. A nested command counts as an argument.
|
#define EMBER_COMMAND_INTERPRETER_HAS_DESCRIPTION_FIELD
|
Whether or not the command entry structure will include descriptions for the commands and error information. This consumes additional CONST space. By default descriptions are not included.
|
#define EMBER_COMMAND_INTERPRETER_NO_ERROR_MESSAGE
|
Whether or not error messages are included. This consumes additional CONST space. By default error messages are included.
The maximum message size for custom commands reserves three bytes for the length (1 bytes) and the custom command identifier (2 bytes).
|
#define EMBER_MAX_COMMAND_ARGUMENTS 14
|
The maximum number of arguments a command can have. A nested command counts as an argument.
|
#define emberBinaryCommandEntryAction
|
(
|
|
identifier,
|
|
|
|
|
command,
|
|
|
|
|
arguments,
|
|
|
|
|
description
|
|
|
)
|
|
{ { (PGM_P)identifier }, command, arguments, description }
|
|
#define emberBinaryCommandEntrySubMenu
|
(
|
|
identifier,
|
|
|
|
|
nestedCommands,
|
|
|
|
|
description
|
|
|
)
|
|
{ { (PGM_P)identifier },
NULL
, description, nestedCommands }
|
|
#define emberCommandEntryAction
|
(
|
|
name,
|
|
|
|
|
command,
|
|
|
|
|
arguments,
|
|
|
|
|
description
|
|
|
)
|
|
{ { name }, command, arguments, description }
|
|
#define emberCommandEntrySubMenu
|
(
|
|
name,
|
|
|
|
|
nestedCommands,
|
|
|
|
|
description
|
|
|
)
|
|
{ { name },
NULL
, (PGM_P)nestedCommands, description }
|
This function copies the EUI64 argument to the given
EmberEui64
destination, reversing the bytes. EUI64's are stored little endian so reversing the bytes means they are big endian in the input command string.
|
#define emberGetKeyArgument
|
(
|
|
index,
|
|
|
|
|
keyDataPointer
|
|
|
)
|
|
|
Value:
emberKeyContents((keyDataPointer)), \
true
))
uint8_t emberGetStringArgument(int8_t argNum, uint8_t *destination, uint8_t maxLength, bool leftPad)
#define EMBER_ENCRYPTION_KEY_SIZE
Size of an encryption key in bytes (16).
Definition:
ember-types.h:43
A convenience macro for copying security key arguments to an
EmberKeyData
pointer.
-
Returns
-
true if an end of line character was read. If the application uses a command line prompt, this indicates it is time to print the prompt.
1
void emberProcessCommandInput(uint8_t port);
|
#define MAX_COMMAND_TABLE_NESTING 16
|
|
typedef void(* CommandAction) (void)
|
If you change this list, ensure you also change the strings that describe these errors in the array emberCommandErrorNames[] in command-interpreter2-error.c.
|
Enumerator
|
|
EMBER_CMD_SUCCESS
|
|
|
EMBER_CMD_ERR_PORT_PROBLEM
|
|
|
EMBER_CMD_ERR_NO_SUCH_COMMAND
|
|
|
EMBER_CMD_ERR_WRONG_NUMBER_OF_ARGUMENTS
|
|
|
EMBER_CMD_ERR_ARGUMENT_OUT_OF_RANGE
|
|
|
EMBER_CMD_ERR_ARGUMENT_SYNTAX_ERROR
|
|
|
EMBER_CMD_ERR_STRING_TOO_LONG
|
|
|
EMBER_CMD_ERR_INVALID_ARGUMENT_TYPE
|
|
|
uint8_t emberCommandArgumentCount
|
(
|
void
|
|
)
|
|
This function returns the number of arguments for the current command.
|
void emberCommandClearBuffer
|
(
|
void
|
|
)
|
|
|
const char* emberCommandName
|
(
|
void
|
|
)
|
|
A convenience macro for copying security key arguments to an
EmberKeyData
pointer.
|
void emberCommandReaderInit
|
(
|
void
|
|
)
|
|
|
void emberCommandReaderSetDefaultBase
|
(
|
uint8_t
|
base
|
)
|
|
|
void emberGetExtendedPanIdArgument
|
(
|
int8_t
|
index,
|
|
|
|
uint8_t *
|
extendedPanId
|
|
|
)
|
|
|
This function copies the extended PAN ID argument to the given destination, reversing the bytes. Extended PAN ids are stored little endian so reversing the bytes means they are big endian in the input command string.
|
bool emberGetIpArgument
|
(
|
uint8_t
|
index,
|
|
|
|
uint8_t *
|
target
|
|
|
)
|
|
|
This function parses and returns, via target, an IP address at the provided index. Returns true if an IP address was successfully parsed Return false otherwise
-
Parameters
-
index
|
An index of the IPv6 address to parse
|
dst
|
the
EmberIpv6Address
a location where the address will be written
|
-
Returns
-
true if the IPv6 address was successfully parsed.
|
bool emberGetIpv6PrefixArgument
|
(
|
uint8_t
|
index,
|
|
|
|
EmberIpv6Address
*
|
dst,
|
|
|
|
uint8_t *
|
dstPrefixBits
|
|
|
)
|
|
|
-
Parameters
-
index
|
An index of the IPv6 prefix to parse
|
dst
|
the
EmberIpv6Address
a location where the address will be written
|
prefixBits
|
the number of prefix bits in the string
|
-
Returns
-
true if the IPv6 prefix was successfully parsed.
|
uint8_t emberGetStringArgument
|
(
|
int8_t
|
argNum,
|
|
|
|
uint8_t *
|
destination,
|
|
|
|
uint8_t
|
maxLength,
|
|
|
|
bool
|
leftPad
|
|
|
)
|
|
|
This function copies the string argument to the given destination up to maxLength. If the argument length is nonzero but less than maxLength and leftPad is true, leading zeroes are prepended to bring the total length of the target up to maxLength. If the argument is longer than the maxLength, it is truncated to maxLength. This function returns the minimum of the argument length and maxLength. ASCII strings are null terminated, but the null terminator is not included in the returned length.
This function is commonly used for reading in hexadecimal strings such as EUI64 or key data and left padding them with zeroes. See
emberGetKeyArgument
and
emberGetEui64Argument
for convenience macros for this purpose.
|
uint8_t* emberLongStringCommandArgument
|
(
|
int8_t
|
argNum,
|
|
|
|
uint16_t *
|
length
|
|
|
)
|
|
|
A convenience macro for copying security key arguments to an
EmberKeyData
pointer.
|
void emberPrintCommandTable
|
(
|
void
|
|
)
|
|
|
void emberPrintCommandUsageNotes
|
(
|
void
|
|
)
|
|
|
bool emberProcessCommandString
|
(
|
const uint8_t *
|
input,
|
|
|
|
uint16_t
|
sizeOrPort
|
|
|
)
|
|
|
|
int32_t emberSignedCommandArgument
|
(
|
uint8_t
|
argNum
|
)
|
|
This function retrieves signed integer arguments.
|
uint8_t* emberStringCommandArgument
|
(
|
int8_t
|
argNum,
|
|
|
|
uint8_t *
|
length
|
|
|
)
|
|
|
This function retrieves quoted string or hexadecimal string arguments. Hexadecimal strings have already been converted into binary. ASCII strings have been null terminated. The null terminator is not included in the returned length argument. To retrieve the name of the command, use an argNum of -1. For example, to retrieve the first character of the command, do: uint8_t firstChar = emberStringCommandArgument(-1, NULL)[0]. If the command is nested, an index of -2, -3, will work to retrieve the higher level command names. Note that [-1] only returns the text entered. If an abbreviated command name is entered, only the text entered will be returned with [-1].
|
uint32_t emberUnsignedCommandArgument
|
(
|
uint8_t
|
argNum
|
)
|
|
This function retrieves unsigned integer arguments.