Microphone Codec MSADPCM Callbacks
Functions |
|
| void | halMicrophoneCodecMsadpcmDataReadyCallback (uint8_t *data, uint8_t length) |
|
A callback called when new microphone data is ready.
|
|
Detailed Description
These callbacks are contributed by the Microphone Codec MSADPCM plugin.
Function Documentation
| void halMicrophoneCodecMsadpcmDataReadyCallback | ( | uint8_t * |
data,
|
| uint8_t |
length
|
||
| ) |
This function is called by the plugin when new data has been processed and is ready to be processed by other parts of the system.
- Parameters
-
dataPointer to the data that is ready lengthLength of the data