EmberUdpConnectionData Struct Reference
Data stored for each connection.
#include <
udp-peer.h
>
Data Fields |
|
EmberUdpConnectionHandle
|
connection |
| uint16_t | flags |
| uint16_t | internal |
| uint8_t | localAddress [16] |
| uint8_t | remoteAddress [16] |
| uint16_t | localPort |
| uint16_t | remotePort |
Field Documentation
EmberUdpConnectionHandle
EmberUdpConnectionData::connection
|
| uint16_t EmberUdpConnectionData::flags |
| uint16_t EmberUdpConnectionData::internal |
| uint8_t EmberUdpConnectionData::localAddress[16] |
| uint16_t EmberUdpConnectionData::localPort |
| uint8_t EmberUdpConnectionData::remoteAddress[16] |
| uint16_t EmberUdpConnectionData::remotePort |
The documentation for this struct was generated from the following file:
-
udp-peer.h