OTA Bootload Client Callbacks
Detailed Description
These callbacks are contributed by the OTA Bootload Client plugin.
Function Documentation
| EmberZclStatus_t emberZclOtaBootloadClientDownloadCompleteCallback | ( | const EmberZclOtaBootloadFileSpec_t * |
fileSpec,
|
| EmberZclStatus_t |
status
|
||
| ) |
An OTA file has been downloaded and verified, or failed to do one of the two.
- Parameters
-
fileSpecThe specification for the OTA file in question. statusThe status of file download and verification.
- Returns
- A status based on the application's analysis of the downloaded file. This is an opportunity for the application to verify the downloaded image and return a related status.
- See also
- emberZclOtaBootloadStorageFind
| bool emberZclOtaBootloadClientGetQueryNextImageParametersCallback | ( | EmberZclOtaBootloadFileSpec_t * |
fileSpec,
|
| EmberZclOtaBootloadHardwareVersion_t * |
hardwareVersion
|
||
| ) |
Get the parameters for a QueryNextImage command.
- Parameters
-
fileSpecThe OTA file specification to include in the query. hardwareVersionThe current hardware version of the device, or EMBER_ZCL_OTA_BOOTLOAD_HARDWARE_VERSION_NULL if this information is to be ignored.
- Returns
-
trueif the device should continue to send a QueryNextImage command, orfalseif it should reschedule the command for a later time.
| void emberZclOtaBootloadClientPreBootloadCallback | ( | const EmberZclOtaBootloadFileSpec_t * |
fileSpec
|
) |
An OTA file is about to be installed.
- Parameters
-
fileSpecThe specification for the OTA file that will be installed.
- See also
- emberZclOtaBootloadStorageFind
| bool emberZclOtaBootloadClientServerDiscoveredCallback | ( | const EmberZclOtaBootloadClientServerInfo_t * |
serverInfo
|
) |
A potential OTA Server has been discovered.
- Parameters
-
serverInfoInformation about the discovered OTA Server device.
- Returns
-
trueif the device should be chosen as the OTA Server,falseotherwise.
- Note
-
If
trueis returned, the OTA Client state machine will move to the next state, which is querying the OTA Server device for a new OTA file to download. Iffalseis returned, the OTA Client will continue to try to discover an OTA Server.
| bool emberZclOtaBootloadClientServerHasDiscByClusterId | ( | const EmberZclClusterSpec_t * |
clusterSpec,
|
| EmberCoapResponseHandler |
responseHandler
|
||
| ) |
Initiate a server discovery
- Parameters
-
clusterSpecserver specifications responseHandlerfunction to handle the response to the CoAP message
- Returns
-
trueif the specification is valid and the request has been sent
- Note
-
If
trueis returned, the OTA Client state machine will wait until the responseHandler is called
References emberZclDiscByClusterId() .
| bool emberZclOtaBootloadClientServerHasDnsNameCallback | ( | EmberZclOtaBootloadClientServerInfo_t * |
serverInfo
|
) |
Start a DNS hostname resolution
- Parameters
-
serverInfoUpdated to the default server parameters
- Returns
-
trueif the device should use the DNS hostname for the OTA Server
- Note
-
If
trueis returned, the OTA Client state machine will wait for the DNS hostname to be resolved.
| bool emberZclOtaBootloadClientServerHasStaticAddressCallback | ( | EmberZclOtaBootloadClientServerInfo_t * |
serverInfo
|
) |
Check to see if a static IP address should be used for the OTA server
- Parameters
-
serverInfoStructure to store the OTA server parameters
- Returns
-
trueif the device should use a static address for the OTA Server
- Note
-
If
trueis returned, the OTA Client state machine will move to the next state, which is querying the OTA Server device for a new OTA file to download. Iffalseis returned, the OTA Client will continue to try to discover an OTA Server.
| bool emberZclOtaBootloadClientSetVersionInfoCallback | ( |
|
) |
This function attempts to set the cluster attribute values to those in the policy parameters. The attributes affected are 'OTA Current File Version', 'Manufacturer ID', and 'Image Type ID'.
- Returns
-
trueif there was an error setting one of the attributes
| bool emberZclOtaBootloadClientStartDownloadCallback | ( | const EmberZclOtaBootloadFileSpec_t * |
fileSpec,
|
| bool |
existingFile
|
||
| ) |
A download of an OTA file can be started.
- Parameters
-
fileSpecThe specification for the OTA file to potentially be downloaded. existingFileA file with this same specification currently exists in OTA storage.
- Returns
-
trueif the device should kick off the download process for this file, orfalseif it should continue to query for new images.
- See also
- emberZclOtaBootloadStorageFind