Sending and receiving ICMP messages.
|
|
|
EmberStatus
|
emberIcmpListen
(const uint8_t *address)
|
|
|
This function sets up a listener for ICMP messages for the given address.
|
|
|
|
bool
|
emberIpPing
(uint8_t *destination, uint16_t id, uint16_t sequence, uint16_t length, uint8_t hopLimit)
|
|
|
This function sends an ICMP ECHO REQUEST message.
|
|
|
|
void
|
emberIncomingIcmpHandler
(
Ipv6Header
*ipHeader)
|
|
|
An application callback for an incoming ICMP message.
|
See
icmp.h
for source code.
|
EmberStatus
emberIcmpListen
|
(
|
const uint8_t *
|
address
|
)
|
|
-
Parameters
-
address
|
The IPv6 address, which is listened to.
|
-
Returns
-
EMBER_SUCCESS if successful EMBER_TABLE_FULL if failed to set up a listener EMBER_ERR_FATAL other fatal failure
|
void emberIncomingIcmpHandler
|
(
|
Ipv6Header
*
|
ipHeader
|
)
|
|
-
Parameters
-
ipHeader
|
Pointer to an IPv6 buffer
|
An application callback for an incoming ICMP message.
-
Parameters
-
ipHeader
|
Pointer to an IPV6 buffer
|
|
bool emberIpPing
|
(
|
uint8_t *
|
destination,
|
|
|
|
uint16_t
|
id,
|
|
|
|
uint16_t
|
sequence,
|
|
|
|
uint16_t
|
length,
|
|
|
|
uint8_t
|
hopLimit
|
|
|
)
|
|
|
-
Parameters
-
destination
|
IPv6 destination address
|
id
|
IPv6 unique ID
|
sequence
|
IPv6 unique sequence
|
length
|
Payload length
|
hopLimit
|
IPv6 hop limit
|
-
Returns
-
Returns true if the ICMP echo request was succesfully submitted to the IP stack and false otherwise.