EmberCommissionData Struct Reference
#include <
network-diagnostics.h
>
Data Fields |
|
| uint32_t | tlvMask |
| const uint8_t * | provisioningUrl |
| const uint8_t * | vendorName |
| const uint8_t * | vendorModel |
| const uint8_t * | swVersion |
| const uint8_t * | vendorData |
| const uint8_t * | vendorStackVersion |
Field Documentation
| const uint8_t* EmberCommissionData::provisioningUrl |
| const uint8_t* EmberCommissionData::swVersion |
| uint32_t EmberCommissionData::tlvMask |
| const uint8_t* EmberCommissionData::vendorData |
| const uint8_t* EmberCommissionData::vendorModel |
| const uint8_t* EmberCommissionData::vendorName |
| const uint8_t* EmberCommissionData::vendorStackVersion |
The documentation for this struct was generated from the following file:
-
network-diagnostics.h