EmberZclGroupEntry_t Struct Reference
#include <
zcl-core-types.h
>
Data Fields |
|
| EmberZclGroupId_t | groupId |
| EmberZclEndpointId_t | endpointId |
| uint8_t | groupNameLength |
| uint8_t | groupName [ EMBER_ZCL_MAX_GROUP_NAME_LENGTH ] |
This structure holds a group entry that represents membership of an endpoint in a group.
Field Documentation
| EmberZclEndpointId_t EmberZclGroupEntry_t::endpointId |
An endpoint identifier of a group entry.
| EmberZclGroupId_t EmberZclGroupEntry_t::groupId |
A group identifier of a group entry.
| uint8_t EmberZclGroupEntry_t::groupName[ EMBER_ZCL_MAX_GROUP_NAME_LENGTH ] |
An array containing group name.
| uint8_t EmberZclGroupEntry_t::groupNameLength |
Length of group name.
The documentation for this struct was generated from the following file:
-
zcl-core-types.h