Button-Press Callbacks
Functions |
|
| void | emberButtonPressIsr (uint8_t button, EmberButtonPress press) |
|
A callback called when a button is pressed. It is sometimes called in ISR context.
|
|
Detailed Description
These callbacks are contributed by the Button-Press plugin.
Function Documentation
| void emberButtonPressIsr | ( | uint8_t |
button,
|
| EmberButtonPress |
press
|
||
| ) |
Must be implemented by the application. This function should contain the functionality to be executed in response to a button press, or callbacks to the appropriate functionality.
- Parameters
-
buttonThe button which was pressed, either BUTTON0 or BUTTON1 as defined in the appropriate BOARD_HEADER. pressEither EMBER_SINGLE_PRESS if it was a single press, or EMBER_DOUBLE_PRESS if it was a double press.