Functions |
|
| void | emberCoapRequestHandler ( EmberCoapCode code, uint8_t *uri, EmberCoapReadOptions *options, const uint8_t *payload, uint16_t payloadLength, const EmberCoapRequestInfo *info) |
|
Callback for incoming requests.
|
|
Detailed Description
These callbacks were contributed by the coap API.
Function Documentation
| void emberCoapRequestHandler | ( | EmberCoapCode |
code,
|
| uint8_t * |
uri,
|
||
| EmberCoapReadOptions * |
options,
|
||
| const uint8_t * |
payload,
|
||
| uint16_t |
payloadLength,
|
||
| const EmberCoapRequestInfo * |
info
|
||
| ) |
For more information, see
stack/include/coap.h
info
can be passed as-is when sending an immediate response from within the call to
emberCoapRequestHandler()
. To send a delayed response, the
info
data must be copied to a more permanent location using
emberSaveRequestInfo()
.