EmberSecurityParameters Struct Reference
Values of security parameters for use in forming or joining a network.
#include <
network-management.h
>
Data Fields |
|
| EmberKeyData * | networkKey |
| uint8_t * | presharedKey |
| uint8_t | presharedKeyLength |
Structure to hold information about pre-shared network security parameters.
Field Documentation
| EmberKeyData * EmberSecurityParameters::networkKey |
| uint8_t* EmberSecurityParameters::presharedKey |
| uint8_t EmberSecurityParameters::presharedKeyLength |
The documentation for this struct was generated from the following file:
-
network-management.h