EmberZclOtaBootloadClientServerInfo_t Struct Reference
#include <
ota-bootload-client.h
>
Data Fields |
|
| EmberZclScheme_t | scheme |
| uint8_t const * | name |
| uint8_t | nameLength |
| EmberIpv6Address | address |
| uint16_t | port |
| EmberZclUid_t | uid |
| EmberZclEndpointId_t | endpointId |
This structure holds information about an OTA Server device.
Field Documentation
| EmberIpv6Address EmberZclOtaBootloadClientServerInfo_t::address |
IPv6 address of the server.
| EmberZclEndpointId_t EmberZclOtaBootloadClientServerInfo_t::endpointId |
Endpoint ID of the server.
| uint8_t const* EmberZclOtaBootloadClientServerInfo_t::name |
| uint8_t EmberZclOtaBootloadClientServerInfo_t::nameLength |
| uint16_t EmberZclOtaBootloadClientServerInfo_t::port |
UDP port of the server.
| EmberZclScheme_t EmberZclOtaBootloadClientServerInfo_t::scheme |
Protocol used to communicate with the server.
| EmberZclUid_t EmberZclOtaBootloadClientServerInfo_t::uid |
UID of the server.
The documentation for this struct was generated from the following file:
-
ota-bootload-client.h