Common bootloader definitions.
Modules |
|
| GPIO | |
|
Bootloader GPIO definitions.
|
|
| Serial | |
|
Common bootloader serial definitions.
|
|
Typedefs |
|
| typedef uint8_t | BL_Status |
|
Define the bootloader status type.
|
|
Enumerations |
|
| enum |
{
COMM_SERIAL = 0x01, COMM_RADIO = 0x02 } |
Bootloader Status Definitions |
|
|
These are numerical definitions for the possible bootloader status codes. |
|
| #define | BL_SUCCESS 0U |
|
Numerical definition for a bootloader status code: Success.
|
|
| #define | BL_CRC_MATCH 2U |
|
Numerical definition for a bootloader status code: CRC match.
|
|
| #define | BL_IMG_FLASHED 3U |
|
Numerical definition for a bootloader status code: Image flashed.
|
|
| #define | BL_ERR 1U |
|
Numerical definition for a bootloader status code: serial error.
|
|
| #define | BL_ERR_MASK 0x40U |
|
Numerical definition for a bootloader status code: Error mask.
|
|
| #define | BL_ERR_HEADER_EXP 0x41U |
|
Numerical definition for a bootloader status code: Failed in header state. Header expected.
|
|
| #define | BL_ERR_HEADER_WRITE_CRC 0x42U |
|
Numerical definition for a bootloader status code: Failed write/CRC of header.
|
|
| #define | BL_ERR_CRC 0x43U |
|
Numerical definition for a bootloader status code: Failed file CRC.
|
|
| #define | BL_ERR_UNKNOWN_TAG 0x44U |
|
Numerical definition for a bootloader status code: Unknown tag.
|
|
| #define | BL_ERR_SIG 0x45U |
|
Numerical definition for a bootloader status code: EBL header error.
|
|
| #define | BL_ERR_ODD_LEN 0x46U |
|
Numerical definition for a bootloader status code: Trying to flash odd length bytes.
|
|
| #define | BL_ERR_BLOCK_INDEX 0x47U |
|
Numerical definition for a bootloader status code: Indexed past end of block buffer.
|
|
| #define | BL_ERR_OVWR_BL 0x48U |
|
Numerical definition for a bootloader status code: Attempt to overwrite bootloader flash.
|
|
| #define | BL_ERR_OVWR_SIMEE 0x49U |
|
Numerical definition for a bootloader status code: Attempt to overwrite Simulated EEPROM flash.
|
|
| #define | BL_ERR_ERASE_FAIL 0x4AU |
|
Numerical definition for a bootloader status code: Flash erase failed.
|
|
| #define | BL_ERR_WRITE_FAIL 0x4BU |
|
Numerical definition for a bootloader status code: Flash write failed.
|
|
| #define | BL_ERR_CRC_LEN 0x4CU |
|
Numerical definition for a bootloader status code: END tag CRC wrong length.
|
|
| #define | BL_ERR_NO_QUERY 0X4DU |
|
Numerical definition for a bootloader status code: Received data before query request/response.
|
|
| #define | BL_ERR_BAD_LEN 0x4EU |
|
Numerical definition for a bootloader status code: Invalid length detected.
|
|
| #define | BL_ERR_TAGBUF 0x4FU |
|
Numerical definition for a bootloader status code: Problem with tagBuf detected.
|
|
| #define | BL_EBL_CONTINUE 0x50U |
|
Numerical definition for a bootloader status code: processEbl deferred, call again to continue.
|
|
| #define | BL_ERR_UNEXPECTED_TAG 0x51U |
|
Numerical definition for a bootloader status code: A known tag was found in an unexpected location (eg. header tag found after data)
|
|
| #define | BL_ERR_UNK_ENC 0x52U |
|
Numerical definition for a bootloader status code: The specified encryption type is unknown to this bootloader.
|
|
| #define | BL_ERR_INV_KEY 0x53U |
|
Numerical definition for a bootloader status code: No valid encryption key found on the device (ie. It's all 0xFF's). Bootloader will not function until this key is set.
|
|
| #define | BL_ERR_ENC 0x54U |
|
Numerical definition for a bootloader status code: Generic error indicating that there was a problem with the encrypted file when decrypting.
|
|
| #define | BL_IBR_ERR_CRC 0x55U |
|
Numerical definition for a bootloader status code: Failed IBR crc.
|
|
| #define | BL_IBR_ERR_VERS 0x56U |
|
Numerical definition for a bootloader status code: Incorrect IBR version.
|
|
| #define | BL_IBR_ERR_ADDR 0x57U |
|
Numerical definition for a bootloader status code: Invalid ebl address in IBR.
|
|
| #define | BL_IBR_ERR_HDR 0x58U |
|
Numerical definition for a bootloader status code: Incorrect IBR header.
|
|
Bootloader State Flags |
|
|
These are numerical flags for the possible bootloader states. These values are used in the bootloader code for making the current state more verbose.
|
|
| #define | TIMEOUT 0x16 |
|
Bootloader state flag.
|
|
| #define | FILEDONE 0x17 |
|
Bootloader state flag.
|
|
| #define | FILEABORT 0x18 |
|
Bootloader state flag.
|
|
| #define | BLOCKOK 0x19 |
|
Bootloader state flag.
|
|
| #define | QUERYFOUND 0x1A |
|
Bootloader state flag.
|
|
| #define | START_TIMEOUT 0x1B |
|
Bootloader state flag.
|
|
| #define | BLOCK_TIMEOUT 0x1C |
|
Bootloader state flag.
|
|
| #define | BLOCKERR_MASK 0x20 |
|
Bootloader state flag.
|
|
| #define | BLOCKERR_SOH 0x21 |
|
Bootloader state flag: Start Of Header not received.
|
|
| #define | BLOCKERR_CHK 0x22 |
|
Bootloader state flag: Sequence of bytes don't match.
|
|
| #define | BLOCKERR_CRCH 0x23 |
|
Bootloader state flag: CRC High byte failure.
|
|
| #define | BLOCKERR_CRCL 0x24 |
|
Bootloader state flag: CRC Low byte failure.
|
|
| #define | BLOCKERR_SEQUENCE 0x25 |
|
Bootloader state flag: Block received out of sequence.
|
|
| #define | BLOCKERR_PARTIAL 0x26 |
|
Bootloader state flag: Partial block received.
|
|
| #define | BLOCKERR_DUPLICATE 0x27 |
|
Bootloader state flag: Duplicate of previous block.
|
|
Detailed Description
See
bootloader-common.h
for source code.
Macro Definition Documentation
| #define BL_CRC_MATCH 2U |
| #define BL_EBL_CONTINUE 0x50U |
| #define BL_ERR 1U |
| #define BL_ERR_BAD_LEN 0x4EU |
| #define BL_ERR_BLOCK_INDEX 0x47U |
| #define BL_ERR_CRC 0x43U |
| #define BL_ERR_CRC_LEN 0x4CU |
| #define BL_ERR_ENC 0x54U |
| #define BL_ERR_ERASE_FAIL 0x4AU |
| #define BL_ERR_HEADER_EXP 0x41U |
| #define BL_ERR_HEADER_WRITE_CRC 0x42U |
| #define BL_ERR_INV_KEY 0x53U |
| #define BL_ERR_MASK 0x40U |
| #define BL_ERR_NO_QUERY 0X4DU |
| #define BL_ERR_ODD_LEN 0x46U |
| #define BL_ERR_OVWR_BL 0x48U |
| #define BL_ERR_OVWR_SIMEE 0x49U |
| #define BL_ERR_SIG 0x45U |
| #define BL_ERR_TAGBUF 0x4FU |
| #define BL_ERR_UNEXPECTED_TAG 0x51U |
| #define BL_ERR_UNK_ENC 0x52U |
| #define BL_ERR_UNKNOWN_TAG 0x44U |
| #define BL_ERR_WRITE_FAIL 0x4BU |
| #define BL_IBR_ERR_ADDR 0x57U |
| #define BL_IBR_ERR_CRC 0x55U |
| #define BL_IBR_ERR_HDR 0x58U |
| #define BL_IBR_ERR_VERS 0x56U |
| #define BL_IMG_FLASHED 3U |
| #define BL_SUCCESS 0U |
| #define BLOCK_TIMEOUT 0x1C |
| #define BLOCKERR_CHK 0x22 |
| #define BLOCKERR_CRCH 0x23 |
| #define BLOCKERR_CRCL 0x24 |
| #define BLOCKERR_DUPLICATE 0x27 |
| #define BLOCKERR_MASK 0x20 |
| #define BLOCKERR_PARTIAL 0x26 |
| #define BLOCKERR_SEQUENCE 0x25 |
| #define BLOCKERR_SOH 0x21 |
| #define BLOCKOK 0x19 |
| #define FILEABORT 0x18 |
| #define FILEDONE 0x17 |
| #define QUERYFOUND 0x1A |
| #define START_TIMEOUT 0x1B |
| #define TIMEOUT 0x16 |
Typedef Documentation
| typedef uint8_t BL_Status |