Color Control Server Callbacks
Functions |
|
| void | emberAfPluginColorControlServerComputePwmFromHsvCallback (uint8_t endpoint) |
|
Compute Pwm from HSV.
|
|
| void | emberAfPluginColorControlServerComputePwmFromXyCallback (uint8_t endpoint) |
|
Compute Pwm from HSV.
|
|
| void | emberAfPluginColorControlServerComputePwmFromTempCallback (uint8_t endpoint) |
|
Compute Pwm from HSV.
|
|
Detailed Description
These callbacks are contributed by the Color Control Server plugin.
Function Documentation
| void emberAfPluginColorControlServerComputePwmFromHsvCallback | ( | uint8_t |
endpoint
|
) |
This function is called from the color server when it is time for the PWMs to be driven with a new value from the HSV values.
- Parameters
-
endpointThe identifying endpoint Ver.: always
| void emberAfPluginColorControlServerComputePwmFromTempCallback | ( | uint8_t |
endpoint
|
) |
This function is called from the color server when it is time for the PWMs to be driven with a new value from the color temperature.
- Parameters
-
endpointThe identifying endpoint Ver.: always
| void emberAfPluginColorControlServerComputePwmFromXyCallback | ( | uint8_t |
endpoint
|
) |
This function is called from the color server when it is time for the PWMs to be driven with a new value from the color X and color Y values.
- Parameters
-
endpointThe identifying endpoint Ver.: always