EmberNetworkParameters Struct Reference
An application structure to hold useful network parameters.
#include <
network-management.h
>
Data Fields |
|
| uint8_t | networkId [ EMBER_NETWORK_ID_SIZE ] |
|
This will only be NUL terminated if the length of the network id is less than EMBER_NETWORK_ID_SIZE.
|
|
| EmberIpv6Prefix | ulaPrefix |
| EmberIpv6Prefix | legacyUla |
| uint8_t | extendedPanId [ EXTENDED_PAN_ID_SIZE ] |
| uint16_t | panId |
| uint8_t | channel |
| EmberNodeType | nodeType |
| int8_t | radioTxPower |
| EmberKeyData | masterKey |
| uint8_t | joinKey [ EMBER_JOIN_KEY_MAX_SIZE ] |
|
This will only be NUL terminated if the length of the key is less than EMBER_JOIN_KEY_MAX_SIZE.
|
|
| uint8_t | joinKeyLength |
Field Documentation
| uint8_t EmberNetworkParameters::channel |
| uint8_t EmberNetworkParameters::extendedPanId[ EXTENDED_PAN_ID_SIZE ] |
| uint8_t EmberNetworkParameters::joinKey[ EMBER_JOIN_KEY_MAX_SIZE ] |
| uint8_t EmberNetworkParameters::joinKeyLength |
| EmberIpv6Prefix EmberNetworkParameters::legacyUla |
| EmberKeyData EmberNetworkParameters::masterKey |
| uint8_t EmberNetworkParameters::networkId[ EMBER_NETWORK_ID_SIZE ] |
| EmberNodeType EmberNetworkParameters::nodeType |
| uint16_t EmberNetworkParameters::panId |
| int8_t EmberNetworkParameters::radioTxPower |
| EmberIpv6Prefix EmberNetworkParameters::ulaPrefix |
The documentation for this struct was generated from the following file:
-
network-management.h