Commands
Data Structures |
|
| struct | EmberZclCommandContext_t |
Macros |
|
| #define | EMBER_ZCL_COMMAND_NULL (( EmberZclCommandId_t )-1) |
Typedefs |
|
| typedef uint8_t | EmberZclCommandId_t |
Functions |
|
| EmberStatus | emberZclSendDefaultResponse (const EmberZclCommandContext_t *context, EmberZclStatus_t status) |
Detailed Description
See
zcl-core-types.h
for source code.
See
zcl-core.h
for source code.
Macro Definition Documentation
| #define EMBER_ZCL_COMMAND_NULL (( EmberZclCommandId_t )-1) |
A distinguished value that represents a null (invalid) command identifier.
Typedef Documentation
| typedef uint8_t EmberZclCommandId_t |
A command identifier.
Function Documentation
| EmberStatus emberZclSendDefaultResponse | ( | const EmberZclCommandContext_t * |
context,
|
| EmberZclStatus_t |
status
|
||
| ) |
This function sends a default response to a command.
- Parameters
-
contextA command context for the response statusA status to respond with
- Returns
-
- EMBER_ZCL_STATUS_SUCCESS if response was sent successfully
- EmberStatus with failure reason otherwise