USB Common
Description
Common parts for both host and device USB stacks.
Data Structures |
|
| struct | USB_Setup_TypeDef |
|
USB Setup request package.
|
|
| struct | USB_DeviceDescriptor_TypeDef |
|
USB Device Descriptor.
|
|
| struct | USB_ConfigurationDescriptor_TypeDef |
|
USB Configuration Descriptor.
|
|
| struct | USB_InterfaceDescriptor_TypeDef |
|
USB Interface Descriptor.
|
|
| struct | USB_EndpointDescriptor_TypeDef |
|
USB Endpoint Descriptor.
|
|
| struct | USB_StringDescriptor_TypeDef |
|
USB String Descriptor.
|
|
Functions |
|
| void | USBTIMER_DelayMs (uint32_t msec) |
|
Active wait millisecond delay function.
|
|
| void | USBTIMER_DelayUs (uint32_t usec) |
|
Active wait microsecond delay function.
|
|
| void | USBTIMER_Init (void) |
|
Activate the hardware timer used to pace the 1 millisecond timer system.
|
|
| void | USBTIMER_Start (uint32_t id, uint32_t timeout, USBTIMER_Callback_TypeDef callback) |
|
Start a timer.
|
|
| void | USBTIMER_Stop (uint32_t id) |
|
Stop a timer.
|
|
| int | USB_PUTCHAR (char c) |
|
Transmit a single char on the debug serial port.
|
|
| void | USB_PUTS (const char *p) |
|
Transmit a zero terminated string on the debug serial port.
|
|
| int | USB_PRINTF (const char *format,...) |
|
Transmit "printf" formated data on the debug serial port.
|
|
| char * | USB_GetErrorMsgString (int error) |
|
Return an error message string for a given error code.
|
|
| void | USB_PrintErrorMsgString (char *pre, int error) |
|
Format and print a text string given an error code, prepends an optional user supplied leader string.
|
|
Macros |
|
| #define | SILABS_USB_VID 0x10C4 |
|
Silicon Labs Vendor ID, supplied by USB-IF.
|
|
| #define | USB_SETUP_DIR_OUT 0 |
|
Setup request data stage OUT direction value.
|
|
| #define | USB_SETUP_DIR_IN 1 |
|
Setup request data stage IN direction value.
|
|
| #define | USB_SETUP_DIR_MASK 0x80 |
|
Setup request data stage direction mask.
|
|
| #define | USB_SETUP_DIR_D2H 0x80 |
|
Setup request data stage IN direction mask.
|
|
| #define | USB_SETUP_DIR_H2D 0x00 |
|
Setup request data stage OUT direction mask.
|
|
| #define | USB_SETUP_TYPE_STANDARD 0 |
|
Standard setup request value.
|
|
| #define | USB_SETUP_TYPE_CLASS 1 |
|
Class setup request value.
|
|
| #define | USB_SETUP_TYPE_VENDOR 2 |
|
Vendor setup request value.
|
|
| #define | USB_SETUP_TYPE_STANDARD_MASK 0x00 |
|
Standard setup request mask.
|
|
| #define | USB_SETUP_TYPE_CLASS_MASK 0x20 |
|
Class setup request mask.
|
|
| #define | USB_SETUP_TYPE_VENDOR_MASK 0x40 |
|
Vendor setup request mask.
|
|
| #define | USB_SETUP_RECIPIENT_DEVICE 0 |
|
Setup request device recipient value.
|
|
| #define | USB_SETUP_RECIPIENT_INTERFACE 1 |
|
Setup request interface recipient value.
|
|
| #define | USB_SETUP_RECIPIENT_ENDPOINT 2 |
|
Setup request endpoint recipient value.
|
|
| #define | USB_SETUP_RECIPIENT_OTHER 3 |
|
Setup request other recipient value.
|
|
| #define | GET_STATUS 0 |
|
Standard setup request GET_STATUS.
|
|
| #define | CLEAR_FEATURE 1 |
|
Standard setup request CLEAR_FEATURE.
|
|
| #define | SET_FEATURE 3 |
|
Standard setup request SET_FEATURE.
|
|
| #define | SET_ADDRESS 5 |
|
Standard setup request SET_ADDRESS.
|
|
| #define | GET_DESCRIPTOR 6 |
|
Standard setup request GET_DESCRIPTOR.
|
|
| #define | SET_DESCRIPTOR 7 |
|
Standard setup request SET_DESCRIPTOR.
|
|
| #define | GET_CONFIGURATION 8 |
|
Standard setup request GET_CONFIGURATION.
|
|
| #define | SET_CONFIGURATION 9 |
|
Standard setup request SET_CONFIGURATION.
|
|
| #define | GET_INTERFACE 10 |
|
Standard setup request GET_INTERFACE.
|
|
| #define | SET_INTERFACE 11 |
|
Standard setup request SET_INTERFACE.
|
|
| #define | SYNCH_FRAME 12 |
|
Standard setup request SYNCH_FRAME.
|
|
| #define | USB_HID_GET_REPORT 0x01 |
|
HID class setup request GET_REPORT.
|
|
| #define | USB_HID_GET_IDLE 0x02 |
|
HID class setup request GET_IDLE.
|
|
| #define | USB_HID_SET_REPORT 0x09 |
|
HID class setup request SET_REPORT.
|
|
| #define | USB_HID_SET_IDLE 0x0A |
|
HID class setup request SET_IDLE.
|
|
| #define | USB_HID_SET_PROTOCOL 0x0B |
|
HID class setup request SET_PROTOCOL.
|
|
| #define | USB_CDC_SETLINECODING 0x20 |
|
CDC class setup request SET_LINE_CODING.
|
|
| #define | USB_CDC_GETLINECODING 0x21 |
|
CDC class setup request GET_LINE_CODING.
|
|
| #define | USB_CDC_SETCTRLLINESTATE 0x22 |
|
CDC class setup request SET_CONTROL_LINE_STATE.
|
|
| #define | USB_MSD_BOTRESET 0xFF |
|
MSD class setup request Bulk only transfer reset.
|
|
| #define | USB_MSD_GETMAXLUN 0xFE |
|
MSD class setup request Get Max LUN.
|
|
| #define | USB_AUDIO_GET_CUR 0x81 |
|
Audio class setup request GET_CUR.
|
|
| #define | USB_AUDIO_GET_CUR 0x81 |
|
Audio class setup request GET_CUR.
|
|
| #define | USB_AUDIO_SET_CUR 0x01 |
|
Audio class setup request SET_CUR.
|
|
| #define | USB_AUDIO_SET_MIN 0x02 |
|
Audio class setup request SET_MIN.
|
|
| #define | USB_AUDIO_GET_MIN 0x82 |
|
Audio class setup request GET_MIN.
|
|
| #define | USB_AUDIO_SET_MAX 0x03 |
|
Audio class setup request SET_MAX.
|
|
| #define | USB_AUDIO_GET_MAX 0x83 |
|
Audio class setup request GET_MAX.
|
|
| #define | USB_AUDIO_SET_RES 0x04 |
|
Audio class setup request SET_RES.
|
|
| #define | USB_AUDIO_GET_RES 0x84 |
|
Audio class setup request GET_RES.
|
|
| #define | USB_AUDIO_SET_MEM 0x05 |
|
Audio class setup request SET_MEM.
|
|
| #define | USB_AUDIO_GET_MEM 0x85 |
|
Audio class setup request GET_MEM.
|
|
| #define | USB_AUDIO_GET_STAT 0xFF |
|
Audio class setup request GET_STAT.
|
|
| #define | USB_DEVICE_DESCRIPTOR 1 |
|
DEVICE descriptor value.
|
|
| #define | USB_CONFIG_DESCRIPTOR 2 |
|
CONFIGURATION descriptor value.
|
|
| #define | USB_STRING_DESCRIPTOR 3 |
|
STRING descriptor value.
|
|
| #define | USB_MAX_STRING_DESCRIPTOR_CHARS 126 |
|
Maximum STRING descriptor bString length.
|
|
| #define | USB_INTERFACE_DESCRIPTOR 4 |
|
INTERFACE descriptor value.
|
|
| #define | USB_ENDPOINT_DESCRIPTOR 5 |
|
ENDPOINT descriptor value.
|
|
| #define | USB_DEVICE_QUALIFIER_DESCRIPTOR 6 |
|
DEVICE_QUALIFIER descriptor value.
|
|
| #define | USB_OTHER_SPEED_CONFIG_DESCRIPTOR 7 |
|
OTHER_SPEED_CONFIGURATION descriptor value.
|
|
| #define | USB_INTERFACE_POWER_DESCRIPTOR 8 |
|
INTERFACE_POWER descriptor value.
|
|
| #define | USB_INTERFACE_ASSOCIATION_DESCRIPTOR 11 |
|
INTERFACE_ASSOCIATION descriptor value.
|
|
| #define | USB_HID_DESCRIPTOR 0x21 |
|
HID descriptor value.
|
|
| #define | USB_SMARTCARD_DESCRIPTOR 0x21 |
|
Smartcard usb-ccid-specific Descriptor Type.
|
|
| #define | USB_HID_REPORT_DESCRIPTOR 0x22 |
|
HID REPORT descriptor value.
|
|
| #define | USB_CS_INTERFACE_DESCRIPTOR 0x24 |
|
Audio Class-specific interface Descriptor Type.
|
|
| #define | USB_CS_ENDPOINT_DESCRIPTOR 0x25 |
|
Audio Class-specific endpoint Descriptor Type.
|
|
| #define | USB_HUB_DESCRIPTOR 0x29 |
|
HUB descriptor value.
|
|
| #define | USB_CA_HEADER_DESCRIPTOR 1 |
|
Audio Class-Specific AC Interface Header descriptor.
|
|
| #define | USB_CA_INPUT_TERMINAL_DESCRIPTOR 2 |
|
Audio Class-Specific AC Interface Input Terminal desc.
|
|
| #define | USB_CA_OUTPUT_TERMINAL_DESCRIPTOR 3 |
|
Audio Class-Specific AC Interface Output Terminal desc.
|
|
| #define | USB_CA_MIXER_UNIT_DESCRIPTOR 4 |
|
Audio Class-Specific AC Interface Mixer descriptor.
|
|
| #define | USB_CA_SELECTOR_UNIT_DESCRIPTOR 5 |
|
Audio Class-Specific AC Interface Selector desc.
|
|
| #define | USB_CA_FEATURE_UNIT_DESCRIPTOR 6 |
|
Audio Class-Specific AC Interface Feature desc.
|
|
| #define | USB_CA_PROCESSING_UNIT_DESCRIPTOR 7 |
|
Audio Class-Specific AC Interface Processing desc.
|
|
| #define | USB_CA_EXTENSION_UNIT_DESCRIPTOR 8 |
|
Audio Class-Specific AC Interface Extension desc.
|
|
| #define | USB_CA_EP_GENERAL_DESCRIPTOR 1 |
|
Audio Class-Specific general descriptor subtype code.
|
|
| #define | USB_CA_AS_GENERAL_DESCRIPTOR 1 |
|
Audio Class-Specific AS Interface General descriptor.
|
|
| #define | USB_CA_FORMAT_TYPE_DESCRIPTOR 2 |
|
Audio Class-Specific AS Interface Format Type desc.
|
|
| #define | USB_DEVICE_DESCSIZE 18 |
|
Device descriptor size.
|
|
| #define | USB_CONFIG_DESCSIZE 9 |
|
Configuration descriptor size.
|
|
| #define | USB_INTERFACE_DESCSIZE 9 |
|
Interface descriptor size.
|
|
| #define | USB_ENDPOINT_DESCSIZE 7 |
|
Endpoint descriptor size.
|
|
| #define | USB_DEVICE_QUALIFIER_DESCSIZE 10 |
|
Device qualifier descriptor size.
|
|
| #define | USB_OTHER_SPEED_CONFIG_DESCSIZE 9 |
|
Device other speed configuration descriptor size.
|
|
| #define | USB_INTERFACE_ASSOCIATION_DESCSIZE 8 |
|
INTERFACE_ASSOCIATION descriptor size.
|
|
| #define | USB_HID_DESCSIZE 9 |
|
HID descriptor size.
|
|
| #define | USB_SMARTCARD_DESCSIZE 54 |
|
CCID descriptor size.
|
|
| #define | USB_CDC_HEADER_FND_DESCSIZE 5 |
|
CDC Header functional descriptor size.
|
|
| #define | USB_CDC_CALLMNG_FND_DESCSIZE 5 |
|
CDC Call Management functional descriptor size.
|
|
| #define | USB_CDC_ACM_FND_DESCSIZE 4 |
|
CDC Abstract Control Management functional descriptor size.
|
|
| #define | USB_CA_INPUT_TERMINAL_DESCSIZE 12 |
|
Audio Input Terminal descriptor size.
|
|
| #define | USB_CA_OUTPUT_TERMINAL_DESCSIZE 9 |
|
Audio Output Terminal descriptor size.
|
|
| #define | USB_CA_EP_GENERAL_DESCSIZE 7 |
|
Audio Class-Specific general descriptor subtype size.
|
|
| #define | USB_CA_AS_GENERAL_DESCSIZE 7 |
|
Audio Class-Specific AS Interface General desc size.
|
|
| #define | USB_CA_STD_AS_ENDPOINT_DESCSZIE 9 |
|
Audio-class standard audio stream descriptor size.
|
|
| #define | USB_LS_CTRL_EP_MAXSIZE 8 |
|
The max size of low speed control endpoints.
|
|
| #define | USB_LS_INTR_EP_MAXSIZE 8 |
|
The max size of low speed interrupt endpoints.
|
|
| #define | USB_FS_CTRL_EP_MAXSIZE 64 |
|
The max size of full speed control endpoints.
|
|
| #define | USB_FS_INTR_EP_MAXSIZE 64 |
|
The max size of full speed interrupt endpoints.
|
|
| #define | USB_FS_BULK_EP_MAXSIZE 64 |
|
The max size of full speed bulk endpoints.
|
|
| #define | USB_FS_ISOC_EP_MAXSIZE 1023 |
|
The max size of full speed isochronous endpoints.
|
|
| #define | USB_EPTYPE_CTRL 0 |
|
Endpoint type control.
|
|
| #define | USB_EPTYPE_ISOC 1 |
|
Endpoint type isochron.
|
|
| #define | USB_EPTYPE_BULK 2 |
|
Endpoint type bulk.
|
|
| #define | USB_EPTYPE_INTR 3 |
|
Endpoint type interrupt.
|
|
| #define | USB_EPSYNC_NO (0 << 2) |
|
Endpoint synchronization type, none.
|
|
| #define | USB_EPSYNC_ASYNC (1 << 2) |
|
Endpoint synchronization type, asynchronous.
|
|
| #define | USB_EPSYNC_ADAPTIVE (2 << 2) |
|
Endpoint synchronization type, adaptive.
|
|
| #define | USB_EPSYNC_SYNC (3 << 2) |
|
Endpoint synchronization type, synchronous.
|
|
| #define | USB_EP_DIR_IN 0x80 |
|
Endpoint direction mask.
|
|
| #define | USB_SETUP_PKT_SIZE 8 |
|
Setup request packet size.
|
|
| #define | USB_EPNUM_MASK 0x0F |
|
Endpoint number mask.
|
|
| #define | USB_LANGID_ENUS 0x0409 |
|
English-United States language id.
|
|
| #define | USB_MAX_DEVICE_ADDRESS 127 |
|
Maximum allowable device address.
|
|
| #define | CONFIG_DESC_BM_REMOTEWAKEUP 0x20 |
|
Configuration descriptor attribute macro.
|
|
| #define | CONFIG_DESC_BM_SELFPOWERED 0x40 |
|
Configuration descriptor attribute macro.
|
|
| #define | CONFIG_DESC_BM_RESERVED_D7 0x80 |
|
Configuration descriptor attribute macro.
|
|
| #define | CONFIG_DESC_BM_TRANSFERTYPE 0x03 |
|
Configuration descriptor transfer type bitmask.
|
|
| #define | CONFIG_DESC_MAXPOWER_mA (x) (((x) + 1) / 2) |
|
Configuration descriptor power macro.
|
|
| #define | DEVICE_IS_SELFPOWERED 0x0001 |
|
Standard request GET_STATUS bitmask.
|
|
| #define | REMOTE_WAKEUP_ENABLED 0x0002 |
|
Standard request GET_STATUS bitmask.
|
|
| #define | USB_FEATURE_ENDPOINT_HALT 0 |
|
Standard request CLEAR/SET_FEATURE bitmask.
|
|
| #define | USB_FEATURE_DEVICE_REMOTE_WAKEUP 1 |
|
Standard request CLEAR/SET_FEATURE bitmask.
|
|
| #define | HUB_FEATURE_PORT_RESET 4 |
|
HUB class request CLEAR/SET_PORT_FEATURE feature selector.
|
|
| #define | HUB_FEATURE_PORT_POWER 8 |
|
HUB class request CLEAR/SET_PORT_FEATURE feature selector.
|
|
| #define | HUB_FEATURE_C_PORT_CONNECTION 16 |
|
HUB class request CLEAR/SET_PORT_FEATURE feature selector.
|
|
| #define | HUB_FEATURE_C_PORT_RESET 20 |
|
HUB class request CLEAR/SET_PORT_FEATURE feature selector.
|
|
| #define | HUB_FEATURE_PORT_INDICATOR 22 |
|
HUB class request CLEAR/SET_PORT_FEATURE feature selector.
|
|
| #define | USB_CLASS_CDC 2 |
|
CDC device/interface class code.
|
|
| #define | USB_CLASS_CDC_DATA 0x0A |
|
CDC Data interface class code.
|
|
| #define | USB_CLASS_CDC_ACM 2 |
|
CDC Abstract Control Model interface subclass code.
|
|
| #define | USB_CLASS_CDC_HFN 0 |
|
CDC class Header Functional Descriptor subtype.
|
|
| #define | USB_CLASS_CDC_CMNGFN 1 |
|
CDC class Call Management Functional Descriptor subtype.
|
|
| #define | USB_CLASS_CDC_ACMFN 2 |
|
CDC class Abstract Control Management Functional Descriptor subtype.
|
|
| #define | USB_CLASS_CDC_UNIONFN 6 |
|
CDC class Union Functional Descriptor subtype.
|
|
| #define | USB_CLASS_HID 3 |
|
HID device/interface class code.
|
|
| #define | USB_CLASS_HID_KEYBOARD 1 |
|
HID keyboard interface protocol code.
|
|
| #define | USB_CLASS_HID_MOUSE 2 |
|
HID mouse interface protocol code.
|
|
| #define | USB_CLASS_HUB 9 |
|
HUB device/interface class code.
|
|
| #define | USB_CLASS_MSD 8 |
|
MSD device/interface class code.
|
|
| #define | USB_CLASS_MSD_BOT_TRANSPORT 0x50 |
|
MSD Bulk Only Transport protocol.
|
|
| #define | USB_CLASS_MSD_SCSI_CMDSET 6 |
|
MSD Subclass SCSI transparent command set.
|
|
| #define | USB_CLASS_MSD_CSW_CMDPASSED 0 |
|
MSD BOT Command status wrapper command passed code.
|
|
| #define | USB_CLASS_MSD_CSW_CMDFAILED 1 |
|
MSD BOT Command status wrapper command failed code.
|
|
| #define | USB_CLASS_MSD_CSW_PHASEERROR 2 |
|
MSD BOT Command status wrapper cmd phase error code.
|
|
| #define | USB_CLASS_AUDIO 1 |
|
Audio interface class code.
|
|
| #define | USB_CLASS_AUDIO_CONTROL 1 |
|
Audio subclass code for control interface.
|
|
| #define | USB_CLASS_AUDIO_STREAMING 2 |
|
Audio subclass code for streaming interface.
|
|
| #define | USB_CLASS_AUDIO_MIDISTREAMING 3 |
|
Audio subclass code for midi streaming interface.
|
|
| #define | USB_CLASS_MISCELLANEOUS 0xEF |
|
MISCELLANEOUS device class code.
|
|
| #define | USB_CLASS_MISC_COMMON_SUBCLASS 2 |
|
MISCELLANEOUS Common sub class code.
|
|
| #define | USB_CLASS_MISC_IAD_PROTOCOL 1 |
|
MISCELLANEOUS Interface Association Descriptor protocol code.
|
|
| #define | PORT_FULL_SPEED 1 |
|
Full speed return value for
USBH_GetPortSpeed()
.
|
|
| #define | PORT_LOW_SPEED 2 |
|
Low speed return value for
USBH_GetPortSpeed()
.
|
|
| #define | USB_DPLL_SRC_LFXO 1 |
|
Use LFXO as DPLL clock source.
|
|
| #define | USB_DPLL_SRC_HFXO 2 |
|
Use HFXO as DPLL clock source.
|
|
| #define | STATIC_CONST_STRING_DESC (_name, ...) |
|
Macro for creating USB compliant UTF-16LE UNICODE string descriptors.
|
|
| #define | STATIC_CONST_STRING_DESC_LANGID (_name, x, y) |
|
Macro for creating USB compliant language string descriptors.
|
|
| #define | UBUF (x, y) SL_ALIGN(4) uint8_t x[((y) + 3) & ~3] SL_ATTRIBUTE_ALIGN(4) |
|
Macro for creating WORD (4 byte) aligned uint8_t array with size which is a multiple of WORD size.
|
|
| #define | STATIC_UBUF (x, y) SL_ALIGN(4) static uint8_t x[((y) + 3) & ~3] SL_ATTRIBUTE_ALIGN(4) |
|
Macro for creating WORD (4 byte) aligned static uint8_t arrays with size which is a multiple of WORD size.
|
|
Typedefs |
|
| typedef unsigned short | char16_t |
|
Data type used for UTF-16LE formatted USB string descriptors.
|
|
| typedef int(* | USB_XferCompleteCb_TypeDef ) ( USB_Status_TypeDef status, uint32_t xferred, uint32_t remaining) |
|
USB transfer callback function.
|
|
| typedef void(* | USBTIMER_Callback_TypeDef ) (void) |
|
USBTIMER callback function.
|
|
Enumerations |
|
| enum |
USB_Status_TypeDef
{
USB_STATUS_OK = 0, USB_STATUS_REQ_ERR = -1, USB_STATUS_EP_BUSY = -2, USB_STATUS_REQ_UNHANDLED = -3, USB_STATUS_ILLEGAL = -4, USB_STATUS_EP_STALLED = -5, USB_STATUS_EP_ABORTED = -6, USB_STATUS_EP_ERROR = -7, USB_STATUS_EP_NAK = -8, USB_STATUS_DEVICE_UNCONFIGURED = -9, USB_STATUS_DEVICE_SUSPENDED = -10, USB_STATUS_DEVICE_RESET = -11, USB_STATUS_TIMEOUT = -12, USB_STATUS_DEVICE_REMOVED = -13, USB_STATUS_HC_BUSY = -14, USB_STATUS_DEVICE_MALFUNCTION = -15, USB_STATUS_PORT_OVERCURRENT = -16 } |
|
USB transfer status enumerator.
|
|
Function Documentation
◆ USBTIMER_DelayMs()
| void USBTIMER_DelayMs | ( | uint32_t |
msec
|
) |
Active wait millisecond delay function.
Can also be used inside interrupt handlers.
- Parameters
-
[in] msecNumber of milliseconds to wait.
◆ USBTIMER_DelayUs()
| void USBTIMER_DelayUs | ( | uint32_t |
usec
|
) |
Active wait microsecond delay function.
Can also be used inside interrupt handlers.
- Parameters
-
[in] usecNumber of microseconds to wait.
◆ USBTIMER_Init()
| void USBTIMER_Init | ( | void |
|
) |
Activate the hardware timer used to pace the 1 millisecond timer system.
Call this function whenever the HFPERCLK frequency is changed. This function is initially called by HOST and DEVICE stack xxxx_Init() functions.
◆ USBTIMER_Start()
| void USBTIMER_Start | ( | uint32_t |
id,
|
| uint32_t |
timeout,
|
||
| USBTIMER_Callback_TypeDef |
callback
|
||
| ) |
Start a timer.
If the timer is already running, it will be restarted with new timeout.
- Parameters
-
[in] idTimer id (0..). [in] timeoutNumber of milliseconds before timer will elapse. [in] callbackFunction to be called on timer elapse, ref. USBTIMER_Callback_TypeDef .
◆ USBTIMER_Stop()
| void USBTIMER_Stop | ( | uint32_t |
id
|
) |
Stop a timer.
- Parameters
-
[in] idTimer id (0..).
◆ USB_PUTCHAR()
| int USB_PUTCHAR | ( | char |
c
|
) |
Transmit a single char on the debug serial port.
- Note
- This function is enabled with #define DEBUG_USB_API when configuring the protocol stack in "usbconfig.h". This is convenient when debugging code, no need to remove use of this function when debugging has completed.
- Parameters
-
[in] cChar to transmit.
- Returns
- The char transmitted.
◆ USB_PUTS()
| void USB_PUTS | ( | const char * |
p
|
) |
Transmit a zero terminated string on the debug serial port.
- Note
- This function is enabled with #define DEBUG_USB_API when configuring the protocol stack in "usbconfig.h". This is convenient when debugging code, no need to remove use of this function when debugging has completed.
- Parameters
-
[in] pPointer to string to transmit.
◆ USB_PRINTF()
| int USB_PRINTF | ( | const char * |
format,
|
...
|
|||
| ) |
Transmit "printf" formated data on the debug serial port.
- Note
- This function is enabled with #define USB_USE_PRINTF when configuring the protocol stack in "usbconfig.h". This is convenient when debugging code, no need to remove use of this function when debugging has completed.
- Parameters
-
[in] formatFormat string (as in printf). No floating point format support.
- Returns
- Number of chars transmitted.
◆ USB_GetErrorMsgString()
| char* USB_GetErrorMsgString | ( | int |
error
|
) |
Return an error message string for a given error code.
- Parameters
-
[in] errorError code, see USB_Status_TypeDef .
- Returns
- Error message string pointer.
◆ USB_PrintErrorMsgString()
| void USB_PrintErrorMsgString | ( | char * |
pre,
|
| int |
error
|
||
| ) |
Format and print a text string given an error code, prepends an optional user supplied leader string.
- Parameters
-
[in] preOptional leader string to prepend to error message string. [in] errorError code, see USB_Status_TypeDef .
Macro Definition Documentation
◆ SILABS_USB_VID
| #define SILABS_USB_VID 0x10C4 |
Silicon Labs Vendor ID, supplied by USB-IF.
◆ USB_SETUP_DIR_OUT
| #define USB_SETUP_DIR_OUT 0 |
Setup request data stage OUT direction value.
◆ USB_SETUP_DIR_IN
| #define USB_SETUP_DIR_IN 1 |
Setup request data stage IN direction value.
◆ USB_SETUP_DIR_MASK
| #define USB_SETUP_DIR_MASK 0x80 |
Setup request data stage direction mask.
◆ USB_SETUP_DIR_D2H
| #define USB_SETUP_DIR_D2H 0x80 |
Setup request data stage IN direction mask.
◆ USB_SETUP_DIR_H2D
| #define USB_SETUP_DIR_H2D 0x00 |
Setup request data stage OUT direction mask.
◆ USB_SETUP_TYPE_STANDARD
| #define USB_SETUP_TYPE_STANDARD 0 |
Standard setup request value.
◆ USB_SETUP_TYPE_CLASS
| #define USB_SETUP_TYPE_CLASS 1 |
Class setup request value.
◆ USB_SETUP_TYPE_VENDOR
| #define USB_SETUP_TYPE_VENDOR 2 |
Vendor setup request value.
◆ USB_SETUP_TYPE_STANDARD_MASK
| #define USB_SETUP_TYPE_STANDARD_MASK 0x00 |
Standard setup request mask.
◆ USB_SETUP_TYPE_CLASS_MASK
| #define USB_SETUP_TYPE_CLASS_MASK 0x20 |
Class setup request mask.
◆ USB_SETUP_TYPE_VENDOR_MASK
| #define USB_SETUP_TYPE_VENDOR_MASK 0x40 |
Vendor setup request mask.
◆ USB_SETUP_RECIPIENT_DEVICE
| #define USB_SETUP_RECIPIENT_DEVICE 0 |
Setup request device recipient value.
◆ USB_SETUP_RECIPIENT_INTERFACE
| #define USB_SETUP_RECIPIENT_INTERFACE 1 |
Setup request interface recipient value.
◆ USB_SETUP_RECIPIENT_ENDPOINT
| #define USB_SETUP_RECIPIENT_ENDPOINT 2 |
Setup request endpoint recipient value.
◆ USB_SETUP_RECIPIENT_OTHER
| #define USB_SETUP_RECIPIENT_OTHER 3 |
Setup request other recipient value.
◆ GET_STATUS
| #define GET_STATUS 0 |
Standard setup request GET_STATUS.
◆ CLEAR_FEATURE
| #define CLEAR_FEATURE 1 |
Standard setup request CLEAR_FEATURE.
◆ SET_FEATURE
| #define SET_FEATURE 3 |
Standard setup request SET_FEATURE.
◆ SET_ADDRESS
| #define SET_ADDRESS 5 |
Standard setup request SET_ADDRESS.
◆ GET_DESCRIPTOR
| #define GET_DESCRIPTOR 6 |
Standard setup request GET_DESCRIPTOR.
◆ SET_DESCRIPTOR
| #define SET_DESCRIPTOR 7 |
Standard setup request SET_DESCRIPTOR.
◆ GET_CONFIGURATION
| #define GET_CONFIGURATION 8 |
Standard setup request GET_CONFIGURATION.
◆ SET_CONFIGURATION
| #define SET_CONFIGURATION 9 |
Standard setup request SET_CONFIGURATION.
◆ GET_INTERFACE
| #define GET_INTERFACE 10 |
Standard setup request GET_INTERFACE.
◆ SET_INTERFACE
| #define SET_INTERFACE 11 |
Standard setup request SET_INTERFACE.
◆ SYNCH_FRAME
| #define SYNCH_FRAME 12 |
Standard setup request SYNCH_FRAME.
◆ USB_HID_GET_REPORT
| #define USB_HID_GET_REPORT 0x01 |
HID class setup request GET_REPORT.
◆ USB_HID_GET_IDLE
| #define USB_HID_GET_IDLE 0x02 |
HID class setup request GET_IDLE.
◆ USB_HID_SET_REPORT
| #define USB_HID_SET_REPORT 0x09 |
HID class setup request SET_REPORT.
◆ USB_HID_SET_IDLE
| #define USB_HID_SET_IDLE 0x0A |
HID class setup request SET_IDLE.
◆ USB_HID_SET_PROTOCOL
| #define USB_HID_SET_PROTOCOL 0x0B |
HID class setup request SET_PROTOCOL.
◆ USB_CDC_SETLINECODING
| #define USB_CDC_SETLINECODING 0x20 |
CDC class setup request SET_LINE_CODING.
◆ USB_CDC_GETLINECODING
| #define USB_CDC_GETLINECODING 0x21 |
CDC class setup request GET_LINE_CODING.
◆ USB_CDC_SETCTRLLINESTATE
| #define USB_CDC_SETCTRLLINESTATE 0x22 |
CDC class setup request SET_CONTROL_LINE_STATE.
◆ USB_MSD_BOTRESET
| #define USB_MSD_BOTRESET 0xFF |
MSD class setup request Bulk only transfer reset.
◆ USB_MSD_GETMAXLUN
| #define USB_MSD_GETMAXLUN 0xFE |
MSD class setup request Get Max LUN.
◆ USB_AUDIO_GET_CUR [1/2]
| #define USB_AUDIO_GET_CUR 0x81 |
Audio class setup request GET_CUR.
◆ USB_AUDIO_GET_CUR [2/2]
| #define USB_AUDIO_GET_CUR 0x81 |
Audio class setup request GET_CUR.
◆ USB_AUDIO_SET_CUR
| #define USB_AUDIO_SET_CUR 0x01 |
Audio class setup request SET_CUR.
◆ USB_AUDIO_SET_MIN
| #define USB_AUDIO_SET_MIN 0x02 |
Audio class setup request SET_MIN.
◆ USB_AUDIO_GET_MIN
| #define USB_AUDIO_GET_MIN 0x82 |
Audio class setup request GET_MIN.
◆ USB_AUDIO_SET_MAX
| #define USB_AUDIO_SET_MAX 0x03 |
Audio class setup request SET_MAX.
◆ USB_AUDIO_GET_MAX
| #define USB_AUDIO_GET_MAX 0x83 |
Audio class setup request GET_MAX.
◆ USB_AUDIO_SET_RES
| #define USB_AUDIO_SET_RES 0x04 |
Audio class setup request SET_RES.
◆ USB_AUDIO_GET_RES
| #define USB_AUDIO_GET_RES 0x84 |
Audio class setup request GET_RES.
◆ USB_AUDIO_SET_MEM
| #define USB_AUDIO_SET_MEM 0x05 |
Audio class setup request SET_MEM.
◆ USB_AUDIO_GET_MEM
| #define USB_AUDIO_GET_MEM 0x85 |
Audio class setup request GET_MEM.
◆ USB_AUDIO_GET_STAT
| #define USB_AUDIO_GET_STAT 0xFF |
Audio class setup request GET_STAT.
◆ USB_DEVICE_DESCRIPTOR
| #define USB_DEVICE_DESCRIPTOR 1 |
DEVICE descriptor value.
◆ USB_CONFIG_DESCRIPTOR
| #define USB_CONFIG_DESCRIPTOR 2 |
CONFIGURATION descriptor value.
◆ USB_STRING_DESCRIPTOR
| #define USB_STRING_DESCRIPTOR 3 |
STRING descriptor value.
◆ USB_MAX_STRING_DESCRIPTOR_CHARS
| #define USB_MAX_STRING_DESCRIPTOR_CHARS 126 |
Maximum STRING descriptor bString length.
◆ USB_INTERFACE_DESCRIPTOR
| #define USB_INTERFACE_DESCRIPTOR 4 |
INTERFACE descriptor value.
◆ USB_ENDPOINT_DESCRIPTOR
| #define USB_ENDPOINT_DESCRIPTOR 5 |
ENDPOINT descriptor value.
◆ USB_DEVICE_QUALIFIER_DESCRIPTOR
| #define USB_DEVICE_QUALIFIER_DESCRIPTOR 6 |
DEVICE_QUALIFIER descriptor value.
◆ USB_OTHER_SPEED_CONFIG_DESCRIPTOR
| #define USB_OTHER_SPEED_CONFIG_DESCRIPTOR 7 |
OTHER_SPEED_CONFIGURATION descriptor value.
◆ USB_INTERFACE_POWER_DESCRIPTOR
| #define USB_INTERFACE_POWER_DESCRIPTOR 8 |
INTERFACE_POWER descriptor value.
◆ USB_INTERFACE_ASSOCIATION_DESCRIPTOR
| #define USB_INTERFACE_ASSOCIATION_DESCRIPTOR 11 |
INTERFACE_ASSOCIATION descriptor value.
◆ USB_HID_DESCRIPTOR
| #define USB_HID_DESCRIPTOR 0x21 |
HID descriptor value.
◆ USB_SMARTCARD_DESCRIPTOR
| #define USB_SMARTCARD_DESCRIPTOR 0x21 |
Smartcard usb-ccid-specific Descriptor Type.
◆ USB_HID_REPORT_DESCRIPTOR
| #define USB_HID_REPORT_DESCRIPTOR 0x22 |
HID REPORT descriptor value.
◆ USB_CS_INTERFACE_DESCRIPTOR
| #define USB_CS_INTERFACE_DESCRIPTOR 0x24 |
Audio Class-specific interface Descriptor Type.
◆ USB_CS_ENDPOINT_DESCRIPTOR
| #define USB_CS_ENDPOINT_DESCRIPTOR 0x25 |
Audio Class-specific endpoint Descriptor Type.
◆ USB_HUB_DESCRIPTOR
| #define USB_HUB_DESCRIPTOR 0x29 |
HUB descriptor value.
◆ USB_CA_HEADER_DESCRIPTOR
| #define USB_CA_HEADER_DESCRIPTOR 1 |
Audio Class-Specific AC Interface Header descriptor.
◆ USB_CA_INPUT_TERMINAL_DESCRIPTOR
| #define USB_CA_INPUT_TERMINAL_DESCRIPTOR 2 |
Audio Class-Specific AC Interface Input Terminal desc.
◆ USB_CA_OUTPUT_TERMINAL_DESCRIPTOR
| #define USB_CA_OUTPUT_TERMINAL_DESCRIPTOR 3 |
Audio Class-Specific AC Interface Output Terminal desc.
◆ USB_CA_MIXER_UNIT_DESCRIPTOR
| #define USB_CA_MIXER_UNIT_DESCRIPTOR 4 |
Audio Class-Specific AC Interface Mixer descriptor.
◆ USB_CA_SELECTOR_UNIT_DESCRIPTOR
| #define USB_CA_SELECTOR_UNIT_DESCRIPTOR 5 |
Audio Class-Specific AC Interface Selector desc.
◆ USB_CA_FEATURE_UNIT_DESCRIPTOR
| #define USB_CA_FEATURE_UNIT_DESCRIPTOR 6 |
Audio Class-Specific AC Interface Feature desc.
◆ USB_CA_PROCESSING_UNIT_DESCRIPTOR
| #define USB_CA_PROCESSING_UNIT_DESCRIPTOR 7 |
Audio Class-Specific AC Interface Processing desc.
◆ USB_CA_EXTENSION_UNIT_DESCRIPTOR
| #define USB_CA_EXTENSION_UNIT_DESCRIPTOR 8 |
Audio Class-Specific AC Interface Extension desc.
◆ USB_CA_EP_GENERAL_DESCRIPTOR
| #define USB_CA_EP_GENERAL_DESCRIPTOR 1 |
Audio Class-Specific general descriptor subtype code.
◆ USB_CA_AS_GENERAL_DESCRIPTOR
| #define USB_CA_AS_GENERAL_DESCRIPTOR 1 |
Audio Class-Specific AS Interface General descriptor.
◆ USB_CA_FORMAT_TYPE_DESCRIPTOR
| #define USB_CA_FORMAT_TYPE_DESCRIPTOR 2 |
Audio Class-Specific AS Interface Format Type desc.
◆ USB_DEVICE_DESCSIZE
| #define USB_DEVICE_DESCSIZE 18 |
Device descriptor size.
◆ USB_CONFIG_DESCSIZE
| #define USB_CONFIG_DESCSIZE 9 |
Configuration descriptor size.
◆ USB_INTERFACE_DESCSIZE
| #define USB_INTERFACE_DESCSIZE 9 |
Interface descriptor size.
◆ USB_ENDPOINT_DESCSIZE
| #define USB_ENDPOINT_DESCSIZE 7 |
Endpoint descriptor size.
◆ USB_DEVICE_QUALIFIER_DESCSIZE
| #define USB_DEVICE_QUALIFIER_DESCSIZE 10 |
Device qualifier descriptor size.
◆ USB_OTHER_SPEED_CONFIG_DESCSIZE
| #define USB_OTHER_SPEED_CONFIG_DESCSIZE 9 |
Device other speed configuration descriptor size.
◆ USB_INTERFACE_ASSOCIATION_DESCSIZE
| #define USB_INTERFACE_ASSOCIATION_DESCSIZE 8 |
INTERFACE_ASSOCIATION descriptor size.
◆ USB_HID_DESCSIZE
| #define USB_HID_DESCSIZE 9 |
HID descriptor size.
◆ USB_SMARTCARD_DESCSIZE
| #define USB_SMARTCARD_DESCSIZE 54 |
CCID descriptor size.
◆ USB_CDC_HEADER_FND_DESCSIZE
| #define USB_CDC_HEADER_FND_DESCSIZE 5 |
CDC Header functional descriptor size.
◆ USB_CDC_CALLMNG_FND_DESCSIZE
| #define USB_CDC_CALLMNG_FND_DESCSIZE 5 |
CDC Call Management functional descriptor size.
◆ USB_CDC_ACM_FND_DESCSIZE
| #define USB_CDC_ACM_FND_DESCSIZE 4 |
CDC Abstract Control Management functional descriptor size.
◆ USB_CA_INPUT_TERMINAL_DESCSIZE
| #define USB_CA_INPUT_TERMINAL_DESCSIZE 12 |
Audio Input Terminal descriptor size.
◆ USB_CA_OUTPUT_TERMINAL_DESCSIZE
| #define USB_CA_OUTPUT_TERMINAL_DESCSIZE 9 |
Audio Output Terminal descriptor size.
◆ USB_CA_EP_GENERAL_DESCSIZE
| #define USB_CA_EP_GENERAL_DESCSIZE 7 |
Audio Class-Specific general descriptor subtype size.
◆ USB_CA_AS_GENERAL_DESCSIZE
| #define USB_CA_AS_GENERAL_DESCSIZE 7 |
Audio Class-Specific AS Interface General desc size.
◆ USB_CA_STD_AS_ENDPOINT_DESCSZIE
| #define USB_CA_STD_AS_ENDPOINT_DESCSZIE 9 |
Audio-class standard audio stream descriptor size.
◆ USB_LS_CTRL_EP_MAXSIZE
| #define USB_LS_CTRL_EP_MAXSIZE 8 |
The max size of low speed control endpoints.
◆ USB_LS_INTR_EP_MAXSIZE
| #define USB_LS_INTR_EP_MAXSIZE 8 |
The max size of low speed interrupt endpoints.
◆ USB_FS_CTRL_EP_MAXSIZE
| #define USB_FS_CTRL_EP_MAXSIZE 64 |
The max size of full speed control endpoints.
◆ USB_FS_INTR_EP_MAXSIZE
| #define USB_FS_INTR_EP_MAXSIZE 64 |
The max size of full speed interrupt endpoints.
◆ USB_FS_BULK_EP_MAXSIZE
| #define USB_FS_BULK_EP_MAXSIZE 64 |
The max size of full speed bulk endpoints.
◆ USB_FS_ISOC_EP_MAXSIZE
| #define USB_FS_ISOC_EP_MAXSIZE 1023 |
The max size of full speed isochronous endpoints.
◆ USB_EPTYPE_CTRL
| #define USB_EPTYPE_CTRL 0 |
Endpoint type control.
◆ USB_EPTYPE_ISOC
| #define USB_EPTYPE_ISOC 1 |
Endpoint type isochron.
◆ USB_EPTYPE_BULK
| #define USB_EPTYPE_BULK 2 |
Endpoint type bulk.
◆ USB_EPTYPE_INTR
| #define USB_EPTYPE_INTR 3 |
Endpoint type interrupt.
◆ USB_EPSYNC_NO
| #define USB_EPSYNC_NO (0 << 2) |
Endpoint synchronization type, none.
◆ USB_EPSYNC_ASYNC
| #define USB_EPSYNC_ASYNC (1 << 2) |
Endpoint synchronization type, asynchronous.
◆ USB_EPSYNC_ADAPTIVE
| #define USB_EPSYNC_ADAPTIVE (2 << 2) |
Endpoint synchronization type, adaptive.
◆ USB_EPSYNC_SYNC
| #define USB_EPSYNC_SYNC (3 << 2) |
Endpoint synchronization type, synchronous.
◆ USB_EP_DIR_IN
| #define USB_EP_DIR_IN 0x80 |
Endpoint direction mask.
◆ USB_SETUP_PKT_SIZE
| #define USB_SETUP_PKT_SIZE 8 |
Setup request packet size.
◆ USB_EPNUM_MASK
| #define USB_EPNUM_MASK 0x0F |
Endpoint number mask.
◆ USB_LANGID_ENUS
| #define USB_LANGID_ENUS 0x0409 |
English-United States language id.
◆ USB_MAX_DEVICE_ADDRESS
| #define USB_MAX_DEVICE_ADDRESS 127 |
Maximum allowable device address.
◆ CONFIG_DESC_BM_REMOTEWAKEUP
| #define CONFIG_DESC_BM_REMOTEWAKEUP 0x20 |
Configuration descriptor attribute macro.
◆ CONFIG_DESC_BM_SELFPOWERED
| #define CONFIG_DESC_BM_SELFPOWERED 0x40 |
Configuration descriptor attribute macro.
◆ CONFIG_DESC_BM_RESERVED_D7
| #define CONFIG_DESC_BM_RESERVED_D7 0x80 |
Configuration descriptor attribute macro.
◆ CONFIG_DESC_BM_TRANSFERTYPE
| #define CONFIG_DESC_BM_TRANSFERTYPE 0x03 |
Configuration descriptor transfer type bitmask.
◆ CONFIG_DESC_MAXPOWER_mA
| #define CONFIG_DESC_MAXPOWER_mA | ( |
x
|
) | (((x) + 1) / 2) |
Configuration descriptor power macro.
◆ DEVICE_IS_SELFPOWERED
| #define DEVICE_IS_SELFPOWERED 0x0001 |
Standard request GET_STATUS bitmask.
◆ REMOTE_WAKEUP_ENABLED
| #define REMOTE_WAKEUP_ENABLED 0x0002 |
Standard request GET_STATUS bitmask.
◆ USB_FEATURE_ENDPOINT_HALT
| #define USB_FEATURE_ENDPOINT_HALT 0 |
Standard request CLEAR/SET_FEATURE bitmask.
◆ USB_FEATURE_DEVICE_REMOTE_WAKEUP
| #define USB_FEATURE_DEVICE_REMOTE_WAKEUP 1 |
Standard request CLEAR/SET_FEATURE bitmask.
◆ HUB_FEATURE_PORT_RESET
| #define HUB_FEATURE_PORT_RESET 4 |
HUB class request CLEAR/SET_PORT_FEATURE feature selector.
◆ HUB_FEATURE_PORT_POWER
| #define HUB_FEATURE_PORT_POWER 8 |
HUB class request CLEAR/SET_PORT_FEATURE feature selector.
◆ HUB_FEATURE_C_PORT_CONNECTION
| #define HUB_FEATURE_C_PORT_CONNECTION 16 |
HUB class request CLEAR/SET_PORT_FEATURE feature selector.
◆ HUB_FEATURE_C_PORT_RESET
| #define HUB_FEATURE_C_PORT_RESET 20 |
HUB class request CLEAR/SET_PORT_FEATURE feature selector.
◆ HUB_FEATURE_PORT_INDICATOR
| #define HUB_FEATURE_PORT_INDICATOR 22 |
HUB class request CLEAR/SET_PORT_FEATURE feature selector.
◆ USB_CLASS_CDC
| #define USB_CLASS_CDC 2 |
CDC device/interface class code.
◆ USB_CLASS_CDC_DATA
| #define USB_CLASS_CDC_DATA 0x0A |
CDC Data interface class code.
◆ USB_CLASS_CDC_ACM
| #define USB_CLASS_CDC_ACM 2 |
CDC Abstract Control Model interface subclass code.
◆ USB_CLASS_CDC_HFN
| #define USB_CLASS_CDC_HFN 0 |
CDC class Header Functional Descriptor subtype.
◆ USB_CLASS_CDC_CMNGFN
| #define USB_CLASS_CDC_CMNGFN 1 |
CDC class Call Management Functional Descriptor subtype.
◆ USB_CLASS_CDC_ACMFN
| #define USB_CLASS_CDC_ACMFN 2 |
CDC class Abstract Control Management Functional Descriptor subtype.
◆ USB_CLASS_CDC_UNIONFN
| #define USB_CLASS_CDC_UNIONFN 6 |
CDC class Union Functional Descriptor subtype.
◆ USB_CLASS_HID
| #define USB_CLASS_HID 3 |
HID device/interface class code.
◆ USB_CLASS_HID_KEYBOARD
| #define USB_CLASS_HID_KEYBOARD 1 |
HID keyboard interface protocol code.
◆ USB_CLASS_HID_MOUSE
| #define USB_CLASS_HID_MOUSE 2 |
HID mouse interface protocol code.
◆ USB_CLASS_HUB
| #define USB_CLASS_HUB 9 |
HUB device/interface class code.
◆ USB_CLASS_MSD
| #define USB_CLASS_MSD 8 |
MSD device/interface class code.
◆ USB_CLASS_MSD_BOT_TRANSPORT
| #define USB_CLASS_MSD_BOT_TRANSPORT 0x50 |
MSD Bulk Only Transport protocol.
◆ USB_CLASS_MSD_SCSI_CMDSET
| #define USB_CLASS_MSD_SCSI_CMDSET 6 |
MSD Subclass SCSI transparent command set.
◆ USB_CLASS_MSD_CSW_CMDPASSED
| #define USB_CLASS_MSD_CSW_CMDPASSED 0 |
MSD BOT Command status wrapper command passed code.
◆ USB_CLASS_MSD_CSW_CMDFAILED
| #define USB_CLASS_MSD_CSW_CMDFAILED 1 |
MSD BOT Command status wrapper command failed code.
◆ USB_CLASS_MSD_CSW_PHASEERROR
| #define USB_CLASS_MSD_CSW_PHASEERROR 2 |
MSD BOT Command status wrapper cmd phase error code.
◆ USB_CLASS_AUDIO
| #define USB_CLASS_AUDIO 1 |
Audio interface class code.
◆ USB_CLASS_AUDIO_CONTROL
| #define USB_CLASS_AUDIO_CONTROL 1 |
Audio subclass code for control interface.
◆ USB_CLASS_AUDIO_STREAMING
| #define USB_CLASS_AUDIO_STREAMING 2 |
Audio subclass code for streaming interface.
◆ USB_CLASS_AUDIO_MIDISTREAMING
| #define USB_CLASS_AUDIO_MIDISTREAMING 3 |
Audio subclass code for midi streaming interface.
◆ USB_CLASS_MISCELLANEOUS
| #define USB_CLASS_MISCELLANEOUS 0xEF |
MISCELLANEOUS device class code.
◆ USB_CLASS_MISC_COMMON_SUBCLASS
| #define USB_CLASS_MISC_COMMON_SUBCLASS 2 |
MISCELLANEOUS Common sub class code.
◆ USB_CLASS_MISC_IAD_PROTOCOL
| #define USB_CLASS_MISC_IAD_PROTOCOL 1 |
MISCELLANEOUS Interface Association Descriptor protocol code.
◆ PORT_FULL_SPEED
| #define PORT_FULL_SPEED 1 |
Full speed return value for USBH_GetPortSpeed() .
◆ PORT_LOW_SPEED
| #define PORT_LOW_SPEED 2 |
Low speed return value for USBH_GetPortSpeed() .
◆ USB_DPLL_SRC_LFXO
| #define USB_DPLL_SRC_LFXO 1 |
Use LFXO as DPLL clock source.
◆ USB_DPLL_SRC_HFXO
| #define USB_DPLL_SRC_HFXO 2 |
Use HFXO as DPLL clock source.
◆ STATIC_CONST_STRING_DESC
| #define STATIC_CONST_STRING_DESC | ( |
_name,
|
|
...
|
|||
| ) |
Macro for creating USB compliant UTF-16LE UNICODE string descriptors.
Example: STATIC_CONST_STRING_DESC(iManufacturer, 'E','n','e','r','g','y',' ','M','i','c','r','o',' ','A','S');
- Note
- The size of the resulting struct will be two byte larger than a USB string descriptor. This is to accommodate a terminating null char for the string. The value assigned to the 'len' member does not take this into account and is therefore correct usb wise.
◆ STATIC_CONST_STRING_DESC_LANGID
| #define STATIC_CONST_STRING_DESC_LANGID | ( |
_name,
|
|
x,
|
|||
y
|
|||
| ) |
Macro for creating USB compliant language string descriptors.
Example:
STATIC_CONST_STRING_DESC_LANGID(langID, 0x04, 0x09)
;
◆ UBUF
| #define UBUF | ( |
x,
|
|
y
|
|||
| ) | SL_ALIGN(4) uint8_t x[((y) + 3) & ~3] SL_ATTRIBUTE_ALIGN(4) |
Macro for creating WORD (4 byte) aligned uint8_t array with size which is a multiple of WORD size.
Example:
UBUF(rxBuffer, 37)
; => uint8_t rxBuffer[40];
◆ STATIC_UBUF
| #define STATIC_UBUF | ( |
x,
|
|
y
|
|||
| ) | SL_ALIGN(4) static uint8_t x[((y) + 3) & ~3] SL_ATTRIBUTE_ALIGN(4) |
Macro for creating WORD (4 byte) aligned static uint8_t arrays with size which is a multiple of WORD size.
Example:
STATIC_UBUF(rxBuffer, 37)
; => static uint8_t rxBuffer[40];
Typedef Documentation
◆ char16_t
| typedef unsigned short char16_t |
Data type used for UTF-16LE formatted USB string descriptors.
◆ USB_XferCompleteCb_TypeDef
| typedef int(* USB_XferCompleteCb_TypeDef) ( USB_Status_TypeDef status, uint32_t xferred, uint32_t remaining) |
USB transfer callback function.
The callback function is called when a transfer has completed. An application should check the status, xferred and optionally the remaining parameters before deciding if the transfer is usable. In the case where the transfer is part of a control request data stage, the callback function should return an appropriate USB_Status_TypeDef status.
- Parameters
-
[in] statusThe transfer status. See USB_Status_TypeDef . [in] xferredNumber of bytes actually transferred. [in] remainingNumber of bytes not transferred.
- Returns
- USB_STATUS_OK on success, else an appropriate error code.
◆ USBTIMER_Callback_TypeDef
| typedef void(* USBTIMER_Callback_TypeDef) (void) |
USBTIMER callback function.
The callback function is called when an USBTIMER has expired. The callback is done with interrupts disabled.
Enumeration Type Documentation
◆ USB_Status_TypeDef
| enum USB_Status_TypeDef |
USB transfer status enumerator.