Key policies

Description

Macros

#define PSA_KEY_USAGE_EXPORT (( psa_key_usage_t )0x00000001)
Whether the key may be exported.
#define PSA_KEY_USAGE_COPY (( psa_key_usage_t )0x00000002)
Whether the key may be copied.
#define PSA_KEY_USAGE_ENCRYPT (( psa_key_usage_t )0x00000100)
Whether the key may be used to encrypt a message.
#define PSA_KEY_USAGE_DECRYPT (( psa_key_usage_t )0x00000200)
Whether the key may be used to decrypt a message.
#define PSA_KEY_USAGE_SIGN_MESSAGE (( psa_key_usage_t )0x00000400)
Whether the key may be used to sign a message.
#define PSA_KEY_USAGE_VERIFY_MESSAGE (( psa_key_usage_t )0x00000800)
Whether the key may be used to verify a message.
#define PSA_KEY_USAGE_SIGN_HASH (( psa_key_usage_t )0x00001000)
Whether the key may be used to sign a message.
#define PSA_KEY_USAGE_VERIFY_HASH (( psa_key_usage_t )0x00002000)
Whether the key may be used to verify a message signature.
#define PSA_KEY_USAGE_DERIVE (( psa_key_usage_t )0x00004000)
Whether the key may be used to derive other keys or produce a password hash.
#define PSA_KEY_USAGE_VERIFY_DERIVATION (( psa_key_usage_t )0x00008000)
Whether the key may be used to verify the result of a key derivation, including password hashing.

Typedefs

typedef uint32_t psa_key_usage_t
Encoding of permitted usage on a key.

Macro Definition Documentation

◆ PSA_KEY_USAGE_EXPORT

#define PSA_KEY_USAGE_EXPORT   (( psa_key_usage_t )0x00000001)

Whether the key may be exported.

A public key or the public part of a key pair may always be exported regardless of the value of this permission flag.

If a key does not have export permission, implementations shall not allow the key to be exported in plain form from the cryptoprocessor, whether through psa_export_key() or through a proprietary interface. The key may however be exportable in a wrapped form, i.e. in a form where it is encrypted by another key.

◆ PSA_KEY_USAGE_COPY

#define PSA_KEY_USAGE_COPY   (( psa_key_usage_t )0x00000002)

Whether the key may be copied.

This flag allows the use of psa_copy_key() to make a copy of the key with the same policy or a more restrictive policy.

For lifetimes for which the key is located in a secure element which enforce the non-exportability of keys, copying a key outside the secure element also requires the usage flag PSA_KEY_USAGE_EXPORT . Copying the key inside the secure element is permitted with just PSA_KEY_USAGE_COPY if the secure element supports it. For keys with the lifetime PSA_KEY_LIFETIME_VOLATILE or PSA_KEY_LIFETIME_PERSISTENT , the usage flag PSA_KEY_USAGE_COPY is sufficient to permit the copy.

◆ PSA_KEY_USAGE_ENCRYPT

#define PSA_KEY_USAGE_ENCRYPT   (( psa_key_usage_t )0x00000100)

Whether the key may be used to encrypt a message.

This flag allows the key to be used for a symmetric encryption operation, for an AEAD encryption-and-authentication operation, or for an asymmetric encryption operation, if otherwise permitted by the key's type and policy.

For a key pair, this concerns the public key.

◆ PSA_KEY_USAGE_DECRYPT

#define PSA_KEY_USAGE_DECRYPT   (( psa_key_usage_t )0x00000200)

Whether the key may be used to decrypt a message.

This flag allows the key to be used for a symmetric decryption operation, for an AEAD decryption-and-verification operation, or for an asymmetric decryption operation, if otherwise permitted by the key's type and policy.

For a key pair, this concerns the private key.

◆ PSA_KEY_USAGE_SIGN_MESSAGE

#define PSA_KEY_USAGE_SIGN_MESSAGE   (( psa_key_usage_t )0x00000400)

Whether the key may be used to sign a message.

This flag allows the key to be used for a MAC calculation operation or for an asymmetric message signature operation, if otherwise permitted by the key’s type and policy.

For a key pair, this concerns the private key.

◆ PSA_KEY_USAGE_VERIFY_MESSAGE

#define PSA_KEY_USAGE_VERIFY_MESSAGE   (( psa_key_usage_t )0x00000800)

Whether the key may be used to verify a message.

This flag allows the key to be used for a MAC verification operation or for an asymmetric message signature verification operation, if otherwise permitted by the key’s type and policy.

For a key pair, this concerns the public key.

◆ PSA_KEY_USAGE_SIGN_HASH

#define PSA_KEY_USAGE_SIGN_HASH   (( psa_key_usage_t )0x00001000)

Whether the key may be used to sign a message.

This flag allows the key to be used for a MAC calculation operation or for an asymmetric signature operation, if otherwise permitted by the key's type and policy.

For a key pair, this concerns the private key.

◆ PSA_KEY_USAGE_VERIFY_HASH

#define PSA_KEY_USAGE_VERIFY_HASH   (( psa_key_usage_t )0x00002000)

Whether the key may be used to verify a message signature.

This flag allows the key to be used for a MAC verification operation or for an asymmetric signature verification operation, if otherwise permitted by by the key's type and policy.

For a key pair, this concerns the public key.

◆ PSA_KEY_USAGE_DERIVE

#define PSA_KEY_USAGE_DERIVE   (( psa_key_usage_t )0x00004000)

Whether the key may be used to derive other keys or produce a password hash.

This flag allows the key to be used for a key derivation operation or for a key agreement operation, if otherwise permitted by by the key's type and policy.

If this flag is present on all keys used in calls to psa_key_derivation_input_key() for a key derivation operation, then it permits calling psa_key_derivation_output_bytes() or psa_key_derivation_output_key() at the end of the operation.

◆ PSA_KEY_USAGE_VERIFY_DERIVATION

#define PSA_KEY_USAGE_VERIFY_DERIVATION   (( psa_key_usage_t )0x00008000)

Whether the key may be used to verify the result of a key derivation, including password hashing.

This flag allows the key to be used:

This flag allows the key to be used in a key derivation operation, if otherwise permitted by by the key's type and policy.

If this flag is present on all keys used in calls to psa_key_derivation_input_key() for a key derivation operation, then it permits calling psa_key_derivation_verify_bytes() or psa_key_derivation_verify_key() at the end of the operation.

Typedef Documentation

◆ psa_key_usage_t

typedef uint32_t psa_key_usage_t

Encoding of permitted usage on a key.

Values of this type are generally constructed as bitwise-ors of macros called PSA_KEY_USAGE_xxx .

Note
Values of this type are encoded in the persistent key store. Any changes to existing values will require bumping the storage format version and providing a translation when reading the old format.