Asymmetric cryptography

Description

Functions

psa_status_t psa_sign_message ( mbedtls_svc_key_id_t key, psa_algorithm_t alg, const uint8_t *input, size_t input_length, uint8_t *signature, size_t signature_size, size_t *signature_length)
Sign a message with a private key.
psa_status_t psa_verify_message ( mbedtls_svc_key_id_t key, psa_algorithm_t alg, const uint8_t *input, size_t input_length, const uint8_t *signature, size_t signature_length)
Verify the signature of a message with a public key, using a hash-and-sign verification algorithm.
psa_status_t psa_sign_hash ( mbedtls_svc_key_id_t key, psa_algorithm_t alg, const uint8_t *hash, size_t hash_length, uint8_t *signature, size_t signature_size, size_t *signature_length)
Sign a hash or short message with a private key.
psa_status_t psa_verify_hash ( mbedtls_svc_key_id_t key, psa_algorithm_t alg, const uint8_t *hash, size_t hash_length, const uint8_t *signature, size_t signature_length)
Verify the signature of a hash or short message using a public key.
psa_status_t psa_asymmetric_encrypt ( mbedtls_svc_key_id_t key, psa_algorithm_t alg, const uint8_t *input, size_t input_length, const uint8_t *salt, size_t salt_length, uint8_t *output, size_t output_size, size_t *output_length)
Encrypt a short message with a public key.
psa_status_t psa_asymmetric_decrypt ( mbedtls_svc_key_id_t key, psa_algorithm_t alg, const uint8_t *input, size_t input_length, const uint8_t *salt, size_t salt_length, uint8_t *output, size_t output_size, size_t *output_length)
Decrypt a short message with a private key.

Function Documentation

◆ psa_sign_message()

psa_status_t psa_sign_message ( mbedtls_svc_key_id_t key,
psa_algorithm_t alg,
const uint8_t * input,
size_t input_length,
uint8_t * signature,
size_t signature_size,
size_t * signature_length
)

Sign a message with a private key.

For hash-and-sign algorithms, this includes the hashing step.

Note
To perform a multi-part hash-and-sign signature algorithm, first use a multi-part hash operation and then pass the resulting hash to psa_sign_hash() . PSA_ALG_GET_HASH( alg ) can be used to determine the hash algorithm to use.
Parameters
[in] key Identifier of the key to use for the operation. It must be an asymmetric key pair. The key must allow the usage PSA_KEY_USAGE_SIGN_MESSAGE .
[in] alg An asymmetric signature algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_SIGN_MESSAGE ( alg ) is true), that is compatible with the type of key .
[in] input The input message to sign.
[in] input_length Size of the input buffer in bytes.
[out] signature Buffer where the signature is to be written.
[in] signature_size Size of the signature buffer in bytes. This must be appropriate for the selected algorithm and key:
  • The required signature size is #PSA_SIGN_OUTPUT_SIZE( key_type , key_bits , alg ) where key_type and key_bits are the type and bit-size respectively of key.
  • #PSA_SIGNATURE_MAX_SIZE evaluates to the maximum signature size of any supported signature algorithm.
[out] signature_length On success, the number of bytes that make up the returned signature value.
Return values
PSA_SUCCESS
PSA_ERROR_INVALID_HANDLE
PSA_ERROR_NOT_PERMITTED The key does not have the PSA_KEY_USAGE_SIGN_MESSAGE flag, or it does not permit the requested algorithm.
PSA_ERROR_BUFFER_TOO_SMALL The size of the signature buffer is too small. You can determine a sufficient buffer size by calling #PSA_SIGN_OUTPUT_SIZE( key_type , key_bits , alg ) where key_type and key_bits are the type and bit-size respectively of key .
PSA_ERROR_NOT_SUPPORTED
PSA_ERROR_INVALID_ARGUMENT
PSA_ERROR_INSUFFICIENT_MEMORY
PSA_ERROR_COMMUNICATION_FAILURE
PSA_ERROR_HARDWARE_FAILURE
PSA_ERROR_CORRUPTION_DETECTED
PSA_ERROR_STORAGE_FAILURE
PSA_ERROR_DATA_CORRUPT
PSA_ERROR_DATA_INVALID
PSA_ERROR_INSUFFICIENT_ENTROPY
PSA_ERROR_BAD_STATE The library has not been previously initialized by psa_crypto_init() . It is implementation-dependent whether a failure to initialize results in this error code.

◆ psa_verify_message()

psa_status_t psa_verify_message ( mbedtls_svc_key_id_t key,
psa_algorithm_t alg,
const uint8_t * input,
size_t input_length,
const uint8_t * signature,
size_t signature_length
)

Verify the signature of a message with a public key, using a hash-and-sign verification algorithm.

Note
To perform a multi-part hash-and-sign signature verification algorithm, first use a multi-part hash operation to hash the message and then pass the resulting hash to psa_verify_hash() . PSA_ALG_GET_HASH( alg ) can be used to determine the hash algorithm to use.
Parameters
[in] key Identifier of the key to use for the operation. It must be a public key or an asymmetric key pair. The key must allow the usage PSA_KEY_USAGE_VERIFY_MESSAGE .
[in] alg An asymmetric signature algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_SIGN_MESSAGE ( alg ) is true), that is compatible with the type of key .
[in] input The message whose signature is to be verified.
[in] input_length Size of the input buffer in bytes.
[out] signature Buffer containing the signature to verify.
[in] signature_length Size of the signature buffer in bytes.
Return values
PSA_SUCCESS
PSA_ERROR_INVALID_HANDLE
PSA_ERROR_NOT_PERMITTED The key does not have the PSA_KEY_USAGE_SIGN_MESSAGE flag, or it does not permit the requested algorithm.
PSA_ERROR_INVALID_SIGNATURE The calculation was performed successfully, but the passed signature is not a valid signature.
PSA_ERROR_NOT_SUPPORTED
PSA_ERROR_INVALID_ARGUMENT
PSA_ERROR_INSUFFICIENT_MEMORY
PSA_ERROR_COMMUNICATION_FAILURE
PSA_ERROR_HARDWARE_FAILURE
PSA_ERROR_CORRUPTION_DETECTED
PSA_ERROR_STORAGE_FAILURE
PSA_ERROR_DATA_CORRUPT
PSA_ERROR_DATA_INVALID
PSA_ERROR_BAD_STATE The library has not been previously initialized by psa_crypto_init() . It is implementation-dependent whether a failure to initialize results in this error code.

◆ psa_sign_hash()

psa_status_t psa_sign_hash ( mbedtls_svc_key_id_t key,
psa_algorithm_t alg,
const uint8_t * hash,
size_t hash_length,
uint8_t * signature,
size_t signature_size,
size_t * signature_length
)

Sign a hash or short message with a private key.

Note that to perform a hash-and-sign signature algorithm, you must first calculate the hash by calling psa_hash_setup() , psa_hash_update() and psa_hash_finish() , or alternatively by calling psa_hash_compute() . Then pass the resulting hash as the hash parameter to this function. You can use PSA_ALG_SIGN_GET_HASH ( alg ) to determine the hash algorithm to use.

Parameters
key Identifier of the key to use for the operation. It must be an asymmetric key pair. The key must allow the usage PSA_KEY_USAGE_SIGN_HASH .
alg A signature algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_SIGN_HASH ( alg ) is true), that is compatible with the type of key .
[in] hash The hash or message to sign.
hash_length Size of the hash buffer in bytes.
[out] signature Buffer where the signature is to be written.
signature_size Size of the signature buffer in bytes.
[out] signature_length On success, the number of bytes that make up the returned signature value.
Return values
PSA_SUCCESS
PSA_ERROR_INVALID_HANDLE
PSA_ERROR_NOT_PERMITTED
PSA_ERROR_BUFFER_TOO_SMALL The size of the signature buffer is too small. You can determine a sufficient buffer size by calling #PSA_SIGN_OUTPUT_SIZE( key_type , key_bits , alg ) where key_type and key_bits are the type and bit-size respectively of key .
PSA_ERROR_NOT_SUPPORTED
PSA_ERROR_INVALID_ARGUMENT
PSA_ERROR_INSUFFICIENT_MEMORY
PSA_ERROR_COMMUNICATION_FAILURE
PSA_ERROR_HARDWARE_FAILURE
PSA_ERROR_CORRUPTION_DETECTED
PSA_ERROR_STORAGE_FAILURE
PSA_ERROR_INSUFFICIENT_ENTROPY
PSA_ERROR_BAD_STATE The library has not been previously initialized by psa_crypto_init() . It is implementation-dependent whether a failure to initialize results in this error code.

◆ psa_verify_hash()

psa_status_t psa_verify_hash ( mbedtls_svc_key_id_t key,
psa_algorithm_t alg,
const uint8_t * hash,
size_t hash_length,
const uint8_t * signature,
size_t signature_length
)

Verify the signature of a hash or short message using a public key.

Note that to perform a hash-and-sign signature algorithm, you must first calculate the hash by calling psa_hash_setup() , psa_hash_update() and psa_hash_finish() , or alternatively by calling psa_hash_compute() . Then pass the resulting hash as the hash parameter to this function. You can use PSA_ALG_SIGN_GET_HASH ( alg ) to determine the hash algorithm to use.

Parameters
key Identifier of the key to use for the operation. It must be a public key or an asymmetric key pair. The key must allow the usage PSA_KEY_USAGE_VERIFY_HASH .
alg A signature algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_SIGN_HASH ( alg ) is true), that is compatible with the type of key .
[in] hash The hash or message whose signature is to be verified.
hash_length Size of the hash buffer in bytes.
[in] signature Buffer containing the signature to verify.
signature_length Size of the signature buffer in bytes.
Return values
PSA_SUCCESS The signature is valid.
PSA_ERROR_INVALID_HANDLE
PSA_ERROR_NOT_PERMITTED
PSA_ERROR_INVALID_SIGNATURE The calculation was performed successfully, but the passed signature is not a valid signature.
PSA_ERROR_NOT_SUPPORTED
PSA_ERROR_INVALID_ARGUMENT
PSA_ERROR_INSUFFICIENT_MEMORY
PSA_ERROR_COMMUNICATION_FAILURE
PSA_ERROR_HARDWARE_FAILURE
PSA_ERROR_CORRUPTION_DETECTED
PSA_ERROR_STORAGE_FAILURE
PSA_ERROR_BAD_STATE The library has not been previously initialized by psa_crypto_init() . It is implementation-dependent whether a failure to initialize results in this error code.

◆ psa_asymmetric_encrypt()

psa_status_t psa_asymmetric_encrypt ( mbedtls_svc_key_id_t key,
psa_algorithm_t alg,
const uint8_t * input,
size_t input_length,
const uint8_t * salt,
size_t salt_length,
uint8_t * output,
size_t output_size,
size_t * output_length
)

Encrypt a short message with a public key.

Parameters
key Identifier of the key to use for the operation. It must be a public key or an asymmetric key pair. It must allow the usage PSA_KEY_USAGE_ENCRYPT .
alg An asymmetric encryption algorithm that is compatible with the type of key .
[in] input The message to encrypt.
input_length Size of the input buffer in bytes.
[in] salt A salt or label, if supported by the encryption algorithm. If the algorithm does not support a salt, pass NULL . If the algorithm supports an optional salt and you do not want to pass a salt, pass NULL .
  • For PSA_ALG_RSA_PKCS1V15_CRYPT , no salt is supported.
    Parameters
    salt_length Size of the salt buffer in bytes. If salt is NULL , pass 0.
    [out] output Buffer where the encrypted message is to be written.
    output_size Size of the output buffer in bytes.
    [out] output_length On success, the number of bytes that make up the returned output.
    Return values
    PSA_SUCCESS
    PSA_ERROR_INVALID_HANDLE
    PSA_ERROR_NOT_PERMITTED
    PSA_ERROR_BUFFER_TOO_SMALL The size of the output buffer is too small. You can determine a sufficient buffer size by calling #PSA_ASYMMETRIC_ENCRYPT_OUTPUT_SIZE( key_type , key_bits , alg ) where key_type and key_bits are the type and bit-size respectively of key .
    PSA_ERROR_NOT_SUPPORTED
    PSA_ERROR_INVALID_ARGUMENT
    PSA_ERROR_INSUFFICIENT_MEMORY
    PSA_ERROR_COMMUNICATION_FAILURE
    PSA_ERROR_HARDWARE_FAILURE
    PSA_ERROR_CORRUPTION_DETECTED
    PSA_ERROR_STORAGE_FAILURE
    PSA_ERROR_INSUFFICIENT_ENTROPY
    PSA_ERROR_BAD_STATE The library has not been previously initialized by psa_crypto_init() . It is implementation-dependent whether a failure to initialize results in this error code.

◆ psa_asymmetric_decrypt()

psa_status_t psa_asymmetric_decrypt ( mbedtls_svc_key_id_t key,
psa_algorithm_t alg,
const uint8_t * input,
size_t input_length,
const uint8_t * salt,
size_t salt_length,
uint8_t * output,
size_t output_size,
size_t * output_length
)

Decrypt a short message with a private key.

Parameters
key Identifier of the key to use for the operation. It must be an asymmetric key pair. It must allow the usage PSA_KEY_USAGE_DECRYPT .
alg An asymmetric encryption algorithm that is compatible with the type of key .
[in] input The message to decrypt.
input_length Size of the input buffer in bytes.
[in] salt A salt or label, if supported by the encryption algorithm. If the algorithm does not support a salt, pass NULL . If the algorithm supports an optional salt and you do not want to pass a salt, pass NULL .
  • For PSA_ALG_RSA_PKCS1V15_CRYPT , no salt is supported.
    Parameters
    salt_length Size of the salt buffer in bytes. If salt is NULL , pass 0.
    [out] output Buffer where the decrypted message is to be written.
    output_size Size of the output buffer in bytes.
    [out] output_length On success, the number of bytes that make up the returned output.
    Return values
    PSA_SUCCESS
    PSA_ERROR_INVALID_HANDLE
    PSA_ERROR_NOT_PERMITTED
    PSA_ERROR_BUFFER_TOO_SMALL The size of the output buffer is too small. You can determine a sufficient buffer size by calling #PSA_ASYMMETRIC_DECRYPT_OUTPUT_SIZE( key_type , key_bits , alg ) where key_type and key_bits are the type and bit-size respectively of key .
    PSA_ERROR_NOT_SUPPORTED
    PSA_ERROR_INVALID_ARGUMENT
    PSA_ERROR_INSUFFICIENT_MEMORY
    PSA_ERROR_COMMUNICATION_FAILURE
    PSA_ERROR_HARDWARE_FAILURE
    PSA_ERROR_CORRUPTION_DETECTED
    PSA_ERROR_STORAGE_FAILURE
    PSA_ERROR_INSUFFICIENT_ENTROPY
    PSA_ERROR_INVALID_PADDING
    PSA_ERROR_BAD_STATE The library has not been previously initialized by psa_crypto_init() . It is implementation-dependent whether a failure to initialize results in this error code.